ResultCoordinateSystem Enumeration¶
NXOpen.CAE.Result.CoordinateSystem is an alias for NXOpen.CAE.ResultCoordinateSystem
-
class
NXOpen.CAE.
ResultCoordinateSystem
¶ Bases:
object
Coordinate systems
Enum Members
such coordinate systems are defined in the results model; if no material coordinate system is defined
NXOpen.CAE.ResultCoordinateSystem.AbsoluteRectangular
will be used”“SelectRectangular”, ” - ” “SelectCylindrical”, ” - ” “SelectSpherical”, ” - “-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-