ResultVelocityParameters_Struct Struct¶
NXOpen.CAE.Result.VelocityParameters is an alias for NXOpen.CAE.ResultVelocityParameters_Struct
-
class
NXOpen.CAE.
ResultVelocityParameters_Struct
¶ Bases:
object
Velociy parameter structure to specify result state for the velocity field used in streamline extraction
Fields¶
Field | Description |
---|---|
LoadCaseIndex | load case number starting from 0 |
IterationIndex | iteration number starting from 0 |
Type |
LoadCaseIndex¶
-
ResultVelocityParameters_Struct.
LoadCaseIndex
¶ load case number starting from 0
-------------------------------------
Getter Method Signature
LoadCaseIndex()
Returns: Return type: int -------------------------------------
Setter Method
Signature
LoadCaseIndex(value)
Parameters: value (int) –
IterationIndex¶
-
ResultVelocityParameters_Struct.
IterationIndex
¶ iteration number starting from 0
-------------------------------------
Getter Method Signature
IterationIndex()
Returns: Return type: int -------------------------------------
Setter Method
Signature
IterationIndex(value)
Parameters: value (int) –
Type¶
-
ResultVelocityParameters_Struct.
Type
¶ -------------------------------------
Getter Method Signature
Type()
Returns: Return type: NXOpen.CAE.ResultType_Struct
-------------------------------------
Setter Method
Signature
Type(value)
Parameters: value ( NXOpen.CAE.ResultType_Struct
) –