AfuZHeaderInfo Class¶
-
class
NXOpen.CAE.
AfuZHeaderInfo
¶ Bases:
NXOpen.TransientObject
Represents the Z axis header information for an afu record
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
GeneralValue | Returns or sets the value of general field |
OrderValue | Returns or sets the value of order field |
RpmValue | Returns or sets the value of RPM field |
TimeValue | Returns or sets the value of time field |
Unit | Returns or sets the unit type of Z axis |
Property Detail¶
GeneralValue¶
-
AfuZHeaderInfo.
GeneralValue
¶ Returns or sets the value of general field
-------------------------------------
Getter Method
Signature
GeneralValue()
Returns: the value of general field Return type: float New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
-------------------------------------
Setter Method
Signature
GeneralValue(generalValue)
Parameters: generalValue (float) – the value of general field New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
OrderValue¶
-
AfuZHeaderInfo.
OrderValue
¶ Returns or sets the value of order field
-------------------------------------
Getter Method
Signature
OrderValue()
Returns: the value of order field Return type: float New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
-------------------------------------
Setter Method
Signature
OrderValue(orderValue)
Parameters: orderValue (float) – the value of order field New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
RpmValue¶
-
AfuZHeaderInfo.
RpmValue
¶ Returns or sets the value of RPM field
-------------------------------------
Getter Method
Signature
RpmValue()
Returns: the value of RPM field Return type: float New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
-------------------------------------
Setter Method
Signature
RpmValue(rpmValue)
Parameters: rpmValue (float) – the value of RPM field New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
TimeValue¶
-
AfuZHeaderInfo.
TimeValue
¶ Returns or sets the value of time field
-------------------------------------
Getter Method
Signature
TimeValue()
Returns: the value of time field Return type: float New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
-------------------------------------
Setter Method
Signature
TimeValue(timeValue)
Parameters: timeValue (float) – the value of time field New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
Unit¶
-
AfuZHeaderInfo.
Unit
¶ Returns or sets the unit type of Z axis
-------------------------------------
Getter Method
Signature
Unit()
Returns: the unit type of Z axis Return type: NXOpen.CAE.XyFunctionUnit
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
-------------------------------------
Setter Method
Signature
Unit(unit)
Parameters: unit ( NXOpen.CAE.XyFunctionUnit
) – the unit type of Z axisNew in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)