MeshFromBoundaryBuilder Class¶
-
class
NXOpen.CAE.
MeshFromBoundaryBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.MeshFromBoundaryBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateMeshFromBoundaryBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CollectorName | Returns or sets the mesh collector name |
ElementType | Returns the element type |
Layers | Returns or sets the layers |
LoopType | Returns or sets the type of loop |
NumElementsOnRail1 | Returns or sets the number of elements along rail1 |
NumElementsOnRail2 | Returns or sets the number of elements along rail2 |
RailType | Returns or sets the type of rail mesh |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetSourceElementEdgePathMethod | Set the source element path of the selection |
SetTargetElementEdgePathMethod | Set the target elemnt path of the selection |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MeshFromBoundaryBuilderLoopOption Enumeration | Type of loop |
MeshFromBoundaryBuilderRailOption Enumeration | Type of rail |
Property Detail¶
CollectorName¶
-
MeshFromBoundaryBuilder.
CollectorName
¶ Returns or sets the mesh collector name
-------------------------------------
Getter Method
Signature
CollectorName()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CollectorName(collectorName)
Parameters: collectorName (str) – New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ElementType¶
-
MeshFromBoundaryBuilder.
ElementType
¶ Returns the element type
-------------------------------------
Getter Method
Signature
ElementType()
Returns: Return type: NXOpen.CAE.ElementTypeBuilder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Layers¶
-
MeshFromBoundaryBuilder.
Layers
¶ Returns or sets the layers
-------------------------------------
Getter Method
Signature
Layers()
Returns: Return type: int New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
Layers(layers)
Parameters: layers (int) – New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
LoopType¶
-
MeshFromBoundaryBuilder.
LoopType
¶ Returns or sets the type of loop
-------------------------------------
Getter Method
Signature
LoopType()
Returns: Return type: NXOpen.CAE.MeshFromBoundaryBuilderLoopOption
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
LoopType(loopoption)
Parameters: loopoption ( NXOpen.CAE.MeshFromBoundaryBuilderLoopOption
) –New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NumElementsOnRail1¶
-
MeshFromBoundaryBuilder.
NumElementsOnRail1
¶ Returns or sets the number of elements along rail1
-------------------------------------
Getter Method
Signature
NumElementsOnRail1()
Returns: Return type: int New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
NumElementsOnRail1(layers)
Parameters: layers (int) – New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NumElementsOnRail2¶
-
MeshFromBoundaryBuilder.
NumElementsOnRail2
¶ Returns or sets the number of elements along rail2
-------------------------------------
Getter Method
Signature
NumElementsOnRail2()
Returns: Return type: int New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
NumElementsOnRail2(layers)
Parameters: layers (int) – New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
RailType¶
-
MeshFromBoundaryBuilder.
RailType
¶ Returns or sets the type of rail mesh
-------------------------------------
Getter Method
Signature
RailType()
Returns: Return type: NXOpen.CAE.MeshFromBoundaryBuilderRailOption
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
RailType(option)
Parameters: option ( NXOpen.CAE.MeshFromBoundaryBuilderRailOption
) –New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
SetSourceElementEdgePathMethod¶
-
MeshFromBoundaryBuilder.
SetSourceElementEdgePathMethod
¶ Set the source element path of the selection
Signature
SetSourceElementEdgePathMethod(sourceElementEdgePathMethod)
Parameters: sourceElementEdgePathMethod ( NXOpen.CAE.ElemEdgePathMethod
) –New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetTargetElementEdgePathMethod¶
-
MeshFromBoundaryBuilder.
SetTargetElementEdgePathMethod
¶ Set the target elemnt path of the selection
Signature
SetTargetElementEdgePathMethod(targetElementEdgePathMethod)
Parameters: targetElementEdgePathMethod ( NXOpen.CAE.ElemEdgePathMethod
) –New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Validate¶
-
MeshFromBoundaryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.