LaminateRelabelPliesBuilder Class¶
-
class
NXOpen.CAE.
LaminateRelabelPliesBuilder
¶ Bases:
NXOpen.Builder
Represents a
CAE.LaminateDynamicEvent
builderTo create a new instance of this class, use
NXOpen.CAE.LaminateGlobalLayupMgr.CreateRelabelPliesBuilder
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Increment | Returns or sets the increment value for the label and increment option |
MinLabel | Returns or sets the start label for the label and increment option |
Offset | Returns or sets the offset value for the label offset option |
RelabelOption | Returns or sets the relabeling option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddGlobalLayup | Adds a layup to the list of layups that will have their plies relabeled. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LaminateRelabelPliesBuilderRelabelOptionEnum Enumeration | the relabeling option enum. |
Property Detail¶
Increment¶
-
LaminateRelabelPliesBuilder.
Increment
¶ Returns or sets the increment value for the label and increment option
-------------------------------------
Getter Method
Signature
Increment()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Increment(increment)
Parameters: increment (int) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
MinLabel¶
-
LaminateRelabelPliesBuilder.
MinLabel
¶ Returns or sets the start label for the label and increment option
-------------------------------------
Getter Method
Signature
MinLabel()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinLabel(minLabel)
Parameters: minLabel (int) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Offset¶
-
LaminateRelabelPliesBuilder.
Offset
¶ Returns or sets the offset value for the label offset option
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Offset(offset)
Parameters: offset (int) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
RelabelOption¶
-
LaminateRelabelPliesBuilder.
RelabelOption
¶ Returns or sets the relabeling option
-------------------------------------
Getter Method
Signature
RelabelOption()
Returns: Return type: NXOpen.CAE.LaminateRelabelPliesBuilderRelabelOptionEnum
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RelabelOption(relabelOption)
Parameters: relabelOption ( NXOpen.CAE.LaminateRelabelPliesBuilderRelabelOptionEnum
) –New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Method Detail¶
AddGlobalLayup¶
-
LaminateRelabelPliesBuilder.
AddGlobalLayup
¶ Adds a layup to the list of layups that will have their plies relabeled.
Signature
AddGlobalLayup(layup)
Parameters: layup ( NXOpen.CAE.LaminateGlobalLayup
) –New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Validate¶
-
LaminateRelabelPliesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.