LaminatePlyFilterBuilder Class¶
-
class
NXOpen.CAE.
LaminatePlyFilterBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.LaminatePlyFilterBuilder
There is no kf creator.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
SelectAllPlies | Returns or sets the select all plies option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetSelectedPlyNames | Returns the selected plies |
SetSelectedPlyNames | Sets the selected plies |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SelectAllPlies¶
-
LaminatePlyFilterBuilder.
SelectAllPlies
¶ Returns or sets the select all plies option
-------------------------------------
Getter Method
Signature
SelectAllPlies()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
-------------------------------------
Setter Method
Signature
SelectAllPlies(selectAllPlies)
Parameters: selectAllPlies (bool) – New in version NX8.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
Method Detail¶
GetSelectedPlyNames¶
-
LaminatePlyFilterBuilder.
GetSelectedPlyNames
¶ Returns the selected plies
Signature
GetSelectedPlyNames()
Returns: Return type: list of str New in version NX8.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
SetSelectedPlyNames¶
-
LaminatePlyFilterBuilder.
SetSelectedPlyNames
¶ Sets the selected plies
Signature
SetSelectedPlyNames(selectedPlies)
Parameters: selectedPlies (list of str) – New in version NX8.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
Validate¶
-
LaminatePlyFilterBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.