SimMotionLoadsListItemBuilder Class¶
-
class
NXOpen.CAE.
SimMotionLoadsListItemBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.CAE.SimMotionLoadsListItemBuilder
To create a new instance of this class, use
NXOpen.CAE.SimSimulation.CreateMotionLoadsListItemBuilder
New in version NX5.0.1.
Properties¶
Property | Description |
---|---|
LinkName | Returns or sets the link name |
SolutionName | Returns or sets the solution name |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
LinkName¶
-
SimMotionLoadsListItemBuilder.
LinkName
¶ Returns or sets the link name
-------------------------------------
Getter Method
Signature
LinkName()
Returns: Return type: str New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinkName(linkName)
Parameters: linkName (str) – New in version NX5.0.1.
License requirements: None.
SolutionName¶
-
SimMotionLoadsListItemBuilder.
SolutionName
¶ Returns or sets the solution name
-------------------------------------
Getter Method
Signature
SolutionName()
Returns: Return type: str New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
SolutionName(solutionName)
Parameters: solutionName (str) – New in version NX5.0.1.
License requirements: None.
Method Detail¶
Validate¶
-
SimMotionLoadsListItemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.