DurabilityRandomFatigueBuilder Class¶
-
class
NXOpen.CAE.
DurabilityRandomFatigueBuilder
¶ Bases:
NXOpen.Builder
Represents a builder class for the event fatigue settings.
The fatigue settings help the user control the fatigue/durability parameters in the event. To create a new instance of this class, use
NXOpen.CAE.DurabilityRandomFatigueCollection.CreateRandomfatigueBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
EventDamage | Returns or sets the event damage. |
EventLife | Returns or sets the event life. |
Name | Returns or sets the name. |
RandomEventDuration | Returns the random event duration. |
RandomFatigueMethod | Returns or sets the random fatigue method. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DurabilityRandomFatigueBuilderRandomFatigueMethodEnum Enumeration | the random method. |
Property Detail¶
EventDamage¶
-
DurabilityRandomFatigueBuilder.
EventDamage
¶ Returns or sets the event damage.
-------------------------------------
Getter Method
Signature
EventDamage()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EventDamage(eventDamage)
Parameters: eventDamage (bool) – New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
EventLife¶
-
DurabilityRandomFatigueBuilder.
EventLife
¶ Returns or sets the event life.
-------------------------------------
Getter Method
Signature
EventLife()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EventLife(eventLife)
Parameters: eventLife (bool) – New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Name¶
-
DurabilityRandomFatigueBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(title)
Parameters: title (str) – New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
RandomEventDuration¶
-
DurabilityRandomFatigueBuilder.
RandomEventDuration
¶ Returns the random event duration.
-------------------------------------
Getter Method
Signature
RandomEventDuration()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RandomFatigueMethod¶
-
DurabilityRandomFatigueBuilder.
RandomFatigueMethod
¶ Returns or sets the random fatigue method.
-------------------------------------
Getter Method
Signature
RandomFatigueMethod()
Returns: Return type: NXOpen.CAE.DurabilityRandomFatigueBuilderRandomFatigueMethodEnum
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RandomFatigueMethod(numberOfElementsInHysterisisLoop)
Parameters: numberOfElementsInHysterisisLoop ( NXOpen.CAE.DurabilityRandomFatigueBuilderRandomFatigueMethodEnum
) –New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Method Detail¶
Validate¶
-
DurabilityRandomFatigueBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.