LaminateFillSetupBuilder Class¶
-
class
NXOpen.CAE.
LaminateFillSetupBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.LaminateFillSetupBuilder
builderTo create a new instance of this class, use
NXOpen.CAE.LaminateGlobalLayupMgr.CreateLaminateFillSetupBuilder
New in version NX7.5.2.
Properties¶
Property | Description |
---|---|
FillName | Returns or sets the name of the laminate fill setup |
HomogeneousPlies | Returns or sets the option to (de)activate homogeneous ply meshes |
LimitThicknessVariation | Returns or sets the layup thickness variation control option |
SamcefSolidShells | Returns or sets the option to use SAMCEF solid shells |
Selection | Returns the face(s) on which to perform the fill |
SinglePlyPerLayer | Returns or sets the option to group plies into single layer(s) of extruded elements |
Tag | Returns the Tag for this object. |
ThicknessVariationDownLimit | Returns or sets the global maximum allowed relative thickness reduction variation, in percentage |
ThicknessVariationUpLimit | Returns or sets the global maximum allowed relative thickness increase variation, in percentage |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FillName¶
-
LaminateFillSetupBuilder.
FillName
¶ Returns or sets the name of the laminate fill setup
-------------------------------------
Getter Method
Signature
FillName()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FillName(fillName)
Parameters: fillName (str) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
HomogeneousPlies¶
-
LaminateFillSetupBuilder.
HomogeneousPlies
¶ Returns or sets the option to (de)activate homogeneous ply meshes
-------------------------------------
Getter Method
Signature
HomogeneousPlies()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HomogeneousPlies(homogeneousPlies)
Parameters: homogeneousPlies (bool) – New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
LimitThicknessVariation¶
-
LaminateFillSetupBuilder.
LimitThicknessVariation
¶ Returns or sets the layup thickness variation control option
-------------------------------------
Getter Method
Signature
LimitThicknessVariation()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitThicknessVariation(limitThicknessVariation)
Parameters: limitThicknessVariation (bool) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SamcefSolidShells¶
-
LaminateFillSetupBuilder.
SamcefSolidShells
¶ Returns or sets the option to use SAMCEF solid shells
-------------------------------------
Getter Method
Signature
SamcefSolidShells()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SamcefSolidShells(samcefSolidShells)
Parameters: samcefSolidShells (bool) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Selection¶
-
LaminateFillSetupBuilder.
Selection
¶ Returns the face(s) on which to perform the fill
-------------------------------------
Getter Method
Signature
Selection()
Returns: Return type: NXOpen.CAE.LaminateSelectEntitiesBuilder
New in version NX7.5.2.
License requirements: None.
SinglePlyPerLayer¶
-
LaminateFillSetupBuilder.
SinglePlyPerLayer
¶ Returns or sets the option to group plies into single layer(s) of extruded elements
-------------------------------------
Getter Method
Signature
SinglePlyPerLayer()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SinglePlyPerLayer(singlePlyPerLayer)
Parameters: singlePlyPerLayer (bool) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ThicknessVariationDownLimit¶
-
LaminateFillSetupBuilder.
ThicknessVariationDownLimit
¶ Returns or sets the global maximum allowed relative thickness reduction variation, in percentage
-------------------------------------
Getter Method
Signature
ThicknessVariationDownLimit()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThicknessVariationDownLimit(thicknessVariationDownLimit)
Parameters: thicknessVariationDownLimit (float) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ThicknessVariationUpLimit¶
-
LaminateFillSetupBuilder.
ThicknessVariationUpLimit
¶ Returns or sets the global maximum allowed relative thickness increase variation, in percentage
-------------------------------------
Getter Method
Signature
ThicknessVariationUpLimit()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThicknessVariationUpLimit(thicknessVariationUpLimit)
Parameters: thicknessVariationUpLimit (float) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Method Detail¶
Validate¶
-
LaminateFillSetupBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.