SetObject Struct¶
-
class
NXOpen.CAE.
SetObject
¶ Bases:
object
Structure used to pass objects into SetManager and CAESet
Fields¶
Field | Description |
---|---|
Obj | the object |
SubType | object sub_component type |
SubId | object sub_component identifier |
Obj¶
-
SetObject.
Obj
¶ the object
-------------------------------------
Getter Method Signature
Obj()
Returns: Return type: NXOpen.TaggedObject
-------------------------------------
Setter Method
Signature
Obj(value)
Parameters: value ( NXOpen.TaggedObject
) –
SubType¶
-
SetObject.
SubType
¶ object sub_component type
-------------------------------------
Getter Method Signature
SubType()
Returns: Return type: NXOpen.CAE.CaeSetObjectSubType
-------------------------------------
Setter Method
Signature
SubType(value)
Parameters: value ( NXOpen.CAE.CaeSetObjectSubType
) –