ElementConnectivityBuilderTypes Enumeration¶
NXOpen.CAE.ElementConnectivityBuilder.Types is an alias for NXOpen.CAE.ElementConnectivityBuilderTypes
-
class
NXOpen.CAE.
ElementConnectivityBuilderTypes
¶ Bases:
object
Modify connectivity types
Enum Members
Enum Member Enum Member Description SingleElement Modify connectivity of selected element. AllElementsAttachedToNode Modify connectivities of all attached elements to nodes. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-