MeshPointMultipleOnCurveBuilder Class¶
-
class
NXOpen.CAE.
MeshPointMultipleOnCurveBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.MeshPointMultipleOnCurveBuilder
To create a new instance of this class, use
NXOpen.CAE.MeshPointCollection.CreateMeshpointMultipleOnCurveBuilder
New in version NX5.0.2.
Properties¶
Property | Description |
---|---|
CreateOption | Returns or sets the create option |
Distance | Returns the distance |
Edge | Returns the node |
NumMeshpoints | Returns or sets the number of meshpoints |
PlacementOption | Returns or sets the placement option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MeshPointMultipleOnCurveBuilderPlacementType Enumeration | the placement type types |
Property Detail¶
CreateOption¶
-
MeshPointMultipleOnCurveBuilder.
CreateOption
¶ Returns or sets the create option
-------------------------------------
Getter Method
Signature
CreateOption()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateOption(createOption)
Parameters: createOption (bool) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Distance¶
-
MeshPointMultipleOnCurveBuilder.
Distance
¶ Returns the distance
-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: None.
Edge¶
-
MeshPointMultipleOnCurveBuilder.
Edge
¶ Returns the node
-------------------------------------
Getter Method
Signature
Edge()
Returns: Return type: NXOpen.SelectIBaseCurveList
New in version NX5.0.2.
License requirements: None.
NumMeshpoints¶
-
MeshPointMultipleOnCurveBuilder.
NumMeshpoints
¶ Returns or sets the number of meshpoints
-------------------------------------
Getter Method
Signature
NumMeshpoints()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumMeshpoints(numMeshpoints)
Parameters: numMeshpoints (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PlacementOption¶
-
MeshPointMultipleOnCurveBuilder.
PlacementOption
¶ Returns or sets the placement option
-------------------------------------
Getter Method
Signature
PlacementOption()
Returns: Return type: NXOpen.CAE.MeshPointMultipleOnCurveBuilderPlacementType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlacementOption(placementOption)
Parameters: placementOption ( NXOpen.CAE.MeshPointMultipleOnCurveBuilderPlacementType
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
MeshPointMultipleOnCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.