ResultsManipulationBuilder Class¶
-
class
NXOpen.CAE.
ResultsManipulationBuilder
¶ Bases:
NXOpen.Builder
Represents an abstract
NXOpen.CAE.ResultsManipulationBuilder
This is an abstract class and cannot be instantiated
New in version NX7.5.2.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAction | The action |
SetAppendMethod | The append method if action is NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult |
SetCompanionResultName | The companion result name if action is NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult |
SetCompanionResultReference | The companion Result Reference if action is NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult |
SetCompanionSolution | The companion solution if action is NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult |
SetCreateSolution | Specifies whether to create an imported solution |
SetImportResult | Import the result immediately |
SetImportedSolutionName | The imported solution name if action is NXOpen.CAE.ResultsManipulationBuilderAction.CreateImportedSolution |
SetIncludeModel | Include nodes and elements |
SetLoadcaseName | The load case name |
SetOutputFile | The output file |
SetOutputName | The output name |
SetOutputQuantity | The output quantity |
SetOutputResultType | The result output type |
SetUnitsSystem | The units system |
SetUnitsSystemResult | The result to copy the units system from |
SetUserDefinedUnitsSystem | The user-defined units system |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ResultsManipulationBuilderAction Enumeration | Action options |
ResultsManipulationBuilderElementValueAtNode Enumeration | Value at Nodes for element nodal values |
ResultsManipulationBuilderOutputResultType Enumeration | Output result types |
ResultsManipulationBuilderResultAppendMethod Enumeration | Result Append Method options |
ResultsManipulationBuilderUnitsSystem Enumeration | Units system options |
Method Detail¶
SetAction¶
-
ResultsManipulationBuilder.
SetAction
¶ The action
Signature
SetAction(action)
Parameters: action ( NXOpen.CAE.ResultsManipulationBuilderAction
) – set actionNew in version NX7.5.2.
Deprecated since version NX9.0.0: Use
NXOpen.CAE.ResultsManipulationBuilder.SetOutputResultType
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetAppendMethod¶
-
ResultsManipulationBuilder.
SetAppendMethod
¶ The append method if action is
NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult
Signature
SetAppendMethod(appendMethod)
Parameters: appendMethod ( NXOpen.CAE.ResultsManipulationBuilderResultAppendMethod
) – set append methodNew in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetCompanionResultName¶
-
ResultsManipulationBuilder.
SetCompanionResultName
¶ The companion result name if action is
NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult
Signature
SetCompanionResultName(companionResultName)
Parameters: companionResultName (str) – set companion result name NOTE: The full Unicode character set is not supported for this parameter. New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetCompanionResultReference¶
-
ResultsManipulationBuilder.
SetCompanionResultReference
¶ The companion Result Reference if action is
NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult
Signature
SetCompanionResultReference(tResultRef)
Parameters: tResultRef ( NXOpen.CAE.SimResultReference
) – set companion result referenceNew in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetCompanionSolution¶
-
ResultsManipulationBuilder.
SetCompanionSolution
¶ The companion solution if action is
NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult
Signature
SetCompanionSolution(solution)
Parameters: solution ( NXOpen.CAE.SimSolution
) – set companion solutionNew in version NX7.5.2.
Deprecated since version NX10.0.0: Use
SetCompanionResultReference
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetCreateSolution¶
-
ResultsManipulationBuilder.
SetCreateSolution
¶ Specifies whether to create an imported solution
Signature
SetCreateSolution(createSolution)
Parameters: createSolution (bool) – New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetImportResult¶
-
ResultsManipulationBuilder.
SetImportResult
¶ Import the result immediately
Signature
SetImportResult(importResult)
Parameters: importResult (bool) – nodes and elements will be included New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetImportedSolutionName¶
-
ResultsManipulationBuilder.
SetImportedSolutionName
¶ The imported solution name if action is
NXOpen.CAE.ResultsManipulationBuilderAction.CreateImportedSolution
Signature
SetImportedSolutionName(importedSolutionName)
Parameters: importedSolutionName (str) – set imported solution name NOTE: The full Unicode character set is not supported for this parameter. New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetIncludeModel¶
-
ResultsManipulationBuilder.
SetIncludeModel
¶ Include nodes and elements
Signature
SetIncludeModel(includeModel)
Parameters: includeModel (bool) – nodes and elements will be included New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetLoadcaseName¶
-
ResultsManipulationBuilder.
SetLoadcaseName
¶ The load case name
Signature
SetLoadcaseName(loadcaseName)
Parameters: loadcaseName (str) – set load case name NOTE: The full Unicode character set is not supported for this parameter. New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetOutputFile¶
-
ResultsManipulationBuilder.
SetOutputFile
¶ The output file
Signature
SetOutputFile(outputFile)
Parameters: outputFile (str) – set output file NOTE: The full Unicode character set is not supported for this parameter. New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetOutputName¶
-
ResultsManipulationBuilder.
SetOutputName
¶ The output name
Signature
SetOutputName(outputName)
Parameters: outputName (str) – set output name NOTE: The full Unicode character set is not supported for this parameter. New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetOutputQuantity¶
-
ResultsManipulationBuilder.
SetOutputQuantity
¶ The output quantity
Signature
SetOutputQuantity(quantity)
Parameters: quantity ( NXOpen.CAE.ResultQuantity
) – not all values may be validNew in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetOutputResultType¶
-
ResultsManipulationBuilder.
SetOutputResultType
¶ The result output type
Signature
SetOutputResultType(type)
Parameters: type ( NXOpen.CAE.ResultsManipulationBuilderOutputResultType
) –New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetUnitsSystem¶
-
ResultsManipulationBuilder.
SetUnitsSystem
¶ The units system
Signature
SetUnitsSystem(unitsSystem)
Parameters: unitsSystem ( NXOpen.CAE.ResultsManipulationBuilderUnitsSystem
) – set units systemNew in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetUnitsSystemResult¶
-
ResultsManipulationBuilder.
SetUnitsSystemResult
¶ The result to copy the units system from
Signature
SetUnitsSystemResult(result)
Parameters: result ( NXOpen.CAE.Result
) – set the result for the units systemNew in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetUserDefinedUnitsSystem¶
-
ResultsManipulationBuilder.
SetUserDefinedUnitsSystem
¶ The user-defined units system
Signature
SetUserDefinedUnitsSystem(unitsSystem)
Parameters: unitsSystem ( NXOpen.CAE.ResultResultBasicUnit_Struct
) – set user-defined units systemNew in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Validate¶
-
ResultsManipulationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.