DurabilitySolveOptionsCollection Class¶
-
class
NXOpen.CAE.
DurabilitySolveOptionsCollection
¶ Bases:
object
Represents a collection of correl meta solution.
To obtain an instance of this class, refer to
NXOpen.CAE.DurabilityManager
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
CloneSolveoptions | Clones a durability event override. |
CreateEventoverridesBuilder | Creates the builder object of durability event overrides. |
DeleteSolveoptions | Delete a durability event overrides. |
FindObject | Finds an event override with a specified name. |
Method Detail¶
CloneSolveoptions¶
-
DurabilitySolveOptionsCollection.
CloneSolveoptions
¶ Clones a durability event override.
Signature
CloneSolveoptions(source)
Parameters: source ( NXOpen.CAE.DurabilitySolveOptions
) – Source event overridesReturns: Cloned event overrides Return type: NXOpen.CAE.DurabilitySolveOptions
New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
CreateEventoverridesBuilder¶
-
DurabilitySolveOptionsCollection.
CreateEventoverridesBuilder
¶ Creates the builder object of durability event overrides.
Signature
CreateEventoverridesBuilder(eventoverrides)
Parameters: eventoverrides ( NXOpen.CAE.DurabilitySolveOptions
) –Returns: Return type: NXOpen.CAE.DurabilityEventOverridesBuilder
New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
DeleteSolveoptions¶
-
DurabilitySolveOptionsCollection.
DeleteSolveoptions
¶ Delete a durability event overrides.
Signature
DeleteSolveoptions(eventoverrides)
Parameters: eventoverrides ( NXOpen.CAE.DurabilitySolveOptions
) – The durability event overrides to be deletedNew in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
FindObject¶
-
DurabilitySolveOptionsCollection.
FindObject
¶ Finds an event override with a specified name.
Signature
FindObject(name)
Parameters: name (str) – name of the durability event override Returns: The durability event override Return type: NXOpen.CAE.DurabilitySolveOptions
New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)