SimSimulationObjectCollection Class¶
-
class
NXOpen.CAE.
SimSimulationObjectCollection
¶ Bases:
object
Provides methods for managing simulation objects
NXOpen.CAE.SimSimulationObject
in a sim partTo obtain an instance of this class, refer to
NXOpen.CAE.SimSimulation
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateSimulationObject | Creates a Simulation object for the simulation object descriptor passed @return simulation object created |
FindObject | Finds the NXOpen.CAE.SimSimulationObject with the given identifier as recorded in a journal. |
Method Detail¶
CreateSimulationObject¶
-
SimSimulationObjectCollection.
CreateSimulationObject
¶ Creates a Simulation object for the simulation object descriptor passed
Signature
CreateSimulationObject(descriptorName, name)
Parameters: - descriptorName (str) – name of the simulation object descriptor NOTE: The full Unicode character set is not supported for this parameter.
- name (str) – name of the simulation object to be created
Returns: simulation object created
Return type: New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
SimSimulationObjectCollection.
FindObject
¶ Finds the
NXOpen.CAE.SimSimulationObject
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: simulation object found Return type: NXOpen.CAE.SimSimulationObject
New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)