DeformationParameters Class¶
-
class
NXOpen.CAE.
DeformationParameters
¶ Bases:
NXOpen.TaggedObject
This class is worked as a packet of information that can be be used to deform
NXOpen.CAE.Post
objects.<br/>Use
NXOpen.CAE.ResultManager
to create anNXOpen.CAE.DeformationParameters
<br/>You can modifiy these values but validation of correctness will only be performed when this object is set to a
NXOpen.CAE.Post
objectTo obtain an instance of this class use
NXOpen.Session.ResultManager
.New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
ComplexCriterion | Returns or sets the complexity criterion. |
Component | Returns or sets the result component that is used for deforming the model. |
DeformationType | Returns or sets the type of scale used for deforming the model |
GenericType | Returns or sets the result type that will be used for deforming the model |
IsReferenceNode | Returns or sets a value of true means the reference node will be used |
PhaseAngle | Returns or sets the phase angle at which result will be evaluated and used for deformation. |
ReferenceNodeLabel | Returns or sets the node label which identifies the reference node used when deforming the model if NXOpen.CAE.DeformationParameters.IsReferenceNode is set to true |
Scale | Returns or sets the scale to be applied to the deformation value |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
ComplexCriterion¶
-
DeformationParameters.
ComplexCriterion
¶ Returns or sets the complexity criterion.
If the result type is complex
NXOpen.CAE.BaseResultType.Complex
the complexity criterion defines which value is used for deformation(likeNXOpen.CAE.ResultComplex.Real
orNXOpen.CAE.ResultComplex.Imaginary
)-------------------------------------
Getter Method
Signature
ComplexCriterion()
Returns: Return type: NXOpen.CAE.ResultComplex
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
ComplexCriterion(complex)
Parameters: complex ( NXOpen.CAE.ResultComplex
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Component¶
-
DeformationParameters.
Component
¶ Returns or sets the result component that is used for deforming the model.
-------------------------------------
Getter Method
Signature
Component()
Returns: Return type: NXOpen.CAE.ResultComponent
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Component(component)
Parameters: component ( NXOpen.CAE.ResultComponent
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeformationType¶
-
DeformationParameters.
DeformationType
¶ Returns or sets the type of scale used for deforming the model
-------------------------------------
Getter Method
Signature
DeformationType()
Returns: Return type: NXOpen.CAE.ResultDeformationScale
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
DeformationType(unit)
Parameters: unit ( NXOpen.CAE.ResultDeformationScale
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GenericType¶
-
DeformationParameters.
GenericType
¶ Returns or sets the result type that will be used for deforming the model
-------------------------------------
Getter Method
Signature
GenericType()
Returns: Return type: NXOpen.CAE.BaseResultType
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
GenericType(type)
Parameters: type ( NXOpen.CAE.BaseResultType
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsReferenceNode¶
-
DeformationParameters.
IsReferenceNode
¶ Returns or sets a value of true means the reference node will be used
-------------------------------------
Getter Method
Signature
IsReferenceNode()
Returns: Return type: bool New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
IsReferenceNode(isReferenceNode)
Parameters: isReferenceNode (bool) – New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PhaseAngle¶
-
DeformationParameters.
PhaseAngle
¶ Returns or sets the phase angle at which result will be evaluated and used for deformation.
If the result type is complex
NXOpen.CAE.BaseResultType.Complex
and theNXOpen.CAE.DeformationParameters.ComplexCriterion`
is set toNXOpen.CAE.ResultComplex.PhaseAngle
, the Phaseangle will be used to evaluate the value of the complex result-------------------------------------
Getter Method
Signature
PhaseAngle()
Returns: Return type: float New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
PhaseAngle(angle)
Parameters: angle (float) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ReferenceNodeLabel¶
-
DeformationParameters.
ReferenceNodeLabel
¶ Returns or sets the node label which identifies the reference node used when deforming the model if
NXOpen.CAE.DeformationParameters.IsReferenceNode
is set to true-------------------------------------
Getter Method
Signature
ReferenceNodeLabel()
Returns: Return type: int New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
ReferenceNodeLabel(referenceNodeLabel)
Parameters: referenceNodeLabel (int) – New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Scale¶
-
DeformationParameters.
Scale
¶ Returns or sets the scale to be applied to the deformation value
-------------------------------------
Getter Method
Signature
Scale()
Returns: Return type: float New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Scale(scale)
Parameters: scale (float) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)