ResultManager Class¶
-
class
NXOpen.CAE.
ResultManager
¶ Bases:
object
Manages results
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX6.0.2.
Methods¶
Method | Description |
---|---|
ConvertOdbFile | Convert older version of ODB file to currently supported version |
Create3dGraphBuilder | Returns a builder used for creating 3d graphs across iterations. |
CreateClippingParameters | Creates a clipping parameter object. |
CreateCrossSectionParameters | Creates a cross-section parameter object. |
CreateDaoOptimizationSolutionResult | Creates a solution result object given a NXOpen.CAE.Optimization.DAOSolution It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult , in order to free up system resources @return |
CreateDeformationParameters | Creates a deformation parameter object. |
CreateDurabilityEventResult | Creates a solution result object given a NXOpen.CAE.DurabilityEvent It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult , in order to free up system resources @return |
CreateFreeBodyResultsBuilder | Creates a free body results builder. |
CreateGraphAcrossIterationsBuilder | Returns a builder used for creating graphs of postview result values across iterations. |
CreateGraphAlongPathBuilder | Returns a builder used for creating the graph of result values of postview result defined by series of entities or path object. |
CreateGraphOrbitBuilder | Returns a builder used for creating the orbit graph from postview. |
CreateImportedResult | Creates a imported result object given a solver results file and the unit systems that these results are defined in. |
CreateJtBuilder | Creates a builder for exporting a component or result type JT @return |
CreateLaminateDynamicEventResult | Creates a solution result object given a NXOpen.CAE.LaminateDynamicEvent It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult , in order to free up system resources @return Created solution result given the input dynamic event |
CreateLaminateGraphicalReportResult | Creates a solution result object given a NXOpen.CAE.LaminateGraphicalReport It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult , in order to free up system resources @return Created solution result given the input laminate graphical report specifications |
CreatePostJtBuilder | Creates a builder for exporting a component or result type JT @return |
CreateReferenceResult | Creates a reference result object given a NXOpen.CAE.SimResultReference It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult , in order to free up system resources @return |
CreateResponseEventResult | Creates a solution result object given a NXOpen.CAE.ResponseSimulation.RSEvent It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult , in order to free up system resources @return |
CreateResponseSolutionResult | Creates a solution result object given a NXOpen.CAE.ResponseSimulation.Solution It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult , in order to free up system resources @return |
CreateResultAccess | Creates a result access object It is user’s responsibility to destroy the result access object once done using NXOpen.CAE.ResultManager.DeleteResultAccess , in order to free up system resources @return |
CreateResultAccessReferenceField | Creates a result access reference field object. |
CreateResultParameters | Creates a result parameter object. |
CreateResultParametersWithProbe | Creates a result parameter object for given Result Probe. |
CreateResultsCombinationBuilder | Creates a results combination builder. |
CreateResultsEnvelopeBuilder | Creates a results envelope builder. |
CreateResultsModelExportBuilder | Creates a model export builder. |
CreateResultsReductionBuilder | Creates a results reduction builder. |
CreateResultvariable | Creates Result Variable object @return |
CreateSeResult | Creates a result object given a seid within an existing NXOpen.CAE.Result . |
CreateSolutionResult | Creates a solution result object given a NXOpen.CAE.SimSolution It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult , in order to free up system resources @return |
CreateTableFieldFromProbe | Creates a field from the lists of independent, dependent variables along with a given Result Probe. |
CreateTbsOptimizationSolutionResult | Creates a solution result object given a NXOpen.CAE.Optimization.TBSOptimizationSolution It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult , in order to free up system resources @return |
CreateTransientResultsReductionBuilder | Creates a transient results reduction builder. |
DeleteClippingParameters | Delete a NXOpen.CAE.ClippingParameters object. |
DeleteCrossSectionParameters | Delete a NXOpen.CAE.CrossSectionParameters object. |
DeleteDeformationParameters | Delete a NXOpen.CAE.DeformationParameters object. |
DeleteFreeBodyResultsBuilder | Delete a NXOpen.CAE.FreeBodyResultsBuilder object. |
DeletePostJtBuilder | Delete a NXOpen.CAE.PostJtExportBuilder object. |
DeleteResult | Delete a NXOpen.CAE.Result object. |
DeleteResultAccess | Delete a NXOpen.CAE.ResultAccess object. |
DeleteResultParameters | Delete a NXOpen.CAE.ResultParameters object. |
DeleteResultParametersWithProbe | Delete a NXOpen.CAE.ResultParametersWithProbe object. |
FindObject | Returns a NXOpen.CAE.Result @return |
Method Detail¶
ConvertOdbFile¶
-
ResultManager.
ConvertOdbFile
¶ Convert older version of ODB file to currently supported version
Signature
ConvertOdbFile(inputFileName, outputFileName)
Parameters: - inputFileName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- outputFileName (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX6.0.2.
License requirements: None.
Create3dGraphBuilder¶
-
ResultManager.
Create3dGraphBuilder
¶ Returns a builder used for creating 3d graphs across iterations.
It is user’s responsibility to destroy the builder object once done using
Builder.Destroy
, in order to free up system resourcesSignature
Create3dGraphBuilder(parameter)
Parameters: parameter ( NXOpen.CAE.ResultProbe
) –Returns: Return type: NXOpen.CAE.Post3DGraphBuilder
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateClippingParameters¶
-
ResultManager.
CreateClippingParameters
¶ Creates a clipping parameter object.
It is user’s responsibility to destroy the clipping parameters object once done using
NXOpen.CAE.ResultManager.DeleteClippingParameters
, in order to free up system resourcesSignature
CreateClippingParameters()
Returns: Return type: NXOpen.CAE.ClippingParameters
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateCrossSectionParameters¶
-
ResultManager.
CreateCrossSectionParameters
¶ Creates a cross-section parameter object.
It is user’s responsibility to destroy the crosss-section parameters object once done using
NXOpen.CAE.ResultManager.DeleteCrossSectionParameters
, in order to free up system resourcesSignature
CreateCrossSectionParameters()
Returns: Return type: NXOpen.CAE.CrossSectionParameters
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateDaoOptimizationSolutionResult¶
-
ResultManager.
CreateDaoOptimizationSolutionResult
¶ Creates a solution result object given a
NXOpen.CAE.Optimization.DAOSolution
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult
, in order to free up system resourcesSignature
CreateDaoOptimizationSolutionResult(daoOptimizationSolution)
Parameters: daoOptimizationSolution ( NXOpen.CAE.Optimization.DAOSolution
) –Returns: Return type: NXOpen.CAE.SolutionResult
New in version NX8.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateDeformationParameters¶
-
ResultManager.
CreateDeformationParameters
¶ Creates a deformation parameter object.
It is user’s responsibility to destroy the deformation parameters object once done using
NXOpen.CAE.ResultManager.DeleteDeformationParameters
, in order to free up system resourcesSignature
CreateDeformationParameters()
Returns: Return type: NXOpen.CAE.DeformationParameters
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateDurabilityEventResult¶
-
ResultManager.
CreateDurabilityEventResult
¶ Creates a solution result object given a
NXOpen.CAE.DurabilityEvent
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult
, in order to free up system resourcesSignature
CreateDurabilityEventResult(durablityEvent)
Parameters: durablityEvent ( NXOpen.CAE.DurabilityEvent
) –Returns: Return type: NXOpen.CAE.SolutionResult
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateFreeBodyResultsBuilder¶
-
ResultManager.
CreateFreeBodyResultsBuilder
¶ Creates a free body results builder.
It is user’s responsibility to destroy the builder object once done using
NXOpen.CAE.ResultManager.DeleteFreeBodyResultsBuilder
, in order to free up system resourcesSignature
CreateFreeBodyResultsBuilder()
Returns: Return type: NXOpen.CAE.FreeBodyResultsBuilder
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateGraphAcrossIterationsBuilder¶
-
ResultManager.
CreateGraphAcrossIterationsBuilder
¶ Overloaded method CreateGraphAcrossIterationsBuilder
CreateGraphAcrossIterationsBuilder(pvid)
CreateGraphAcrossIterationsBuilder(firstpvid, secondpvid)
CreateGraphAcrossIterationsBuilder(result, parameter)
CreateGraphAcrossIterationsBuilder(parameter)
CreateGraphAcrossIterationsBuilder(result, parameter1, parameter2)
CreateGraphAcrossIterationsBuilder(result, parameters, names, formula)
-------------------------------------
Returns a builder used for creating graphs of postview result values across iterations. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy
, in order to free up system resourcesSignature
CreateGraphAcrossIterationsBuilder(pvid)
Parameters: pvid (int) – Returns: Return type: NXOpen.CAE.PostGraphAcrossIterationsBuilder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Returns a builder used for creating graphs of two postview result values across iterations. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy
, in order to free up system resourcesSignature
CreateGraphAcrossIterationsBuilder(firstpvid, secondpvid)
Parameters: - firstpvid (int) –
- secondpvid (int) –
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Returns a builder used for creating graphs across iterations of result values of result parameter. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy
, in order to free up system resourcesSignature
CreateGraphAcrossIterationsBuilder(result, parameter)
Parameters: - result (
NXOpen.CAE.Result
) – set result - parameter (
NXOpen.CAE.ResultParameters
) –
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Returns a builder used for creating graphs across iterations of result values of result parameter. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy
, in order to free up system resourcesSignature
CreateGraphAcrossIterationsBuilder(parameter)
Parameters: parameter ( NXOpen.CAE.ResultProbe
) –Returns: Return type: NXOpen.CAE.PostGraphAcrossIterationsBuilder
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Returns a builder used for creating graphs across iterations of result values two result parameters. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy
, in order to free up system resourcesSignature
CreateGraphAcrossIterationsBuilder(result, parameter1, parameter2)
Parameters: - result (
NXOpen.CAE.Result
) – set result - parameter1 (
NXOpen.CAE.ResultParameters
) – - parameter2 (
NXOpen.CAE.ResultParameters
) –
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Returns a builder used for creating graphs across iterations of result values of expression. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy
, in order to free up system resourcesSignature
CreateGraphAcrossIterationsBuilder(result, parameters, names, formula)
Parameters: - result (
NXOpen.CAE.Result
) – set result - parameters (list of
NXOpen.CAE.ResultParameters
) – set result parameters - names (list of str) – set result names NOTE: The full Unicode character set is not supported for this parameter.
- formula (str) – set formula NOTE: The full Unicode character set is not supported for this parameter.
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
CreateGraphAlongPathBuilder¶
-
ResultManager.
CreateGraphAlongPathBuilder
¶ Overloaded method CreateGraphAlongPathBuilder
CreateGraphAlongPathBuilder(pvid)
CreateGraphAlongPathBuilder(firstpvid, secondpvid)
CreateGraphAlongPathBuilder(result, parameter)
CreateGraphAlongPathBuilder(parameter)
CreateGraphAlongPathBuilder(result, parameter1, parameter2)
-------------------------------------
Returns a builder used for creating the graph of result values of postview result defined by series of entities or path object. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy
, in order to free up system resourcesSignature
CreateGraphAlongPathBuilder(pvid)
Parameters: pvid (int) – Returns: Return type: NXOpen.CAE.PostGraphAlongPathBuilder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Returns a builder used for creating the graph of result values of two postviews defined by series of entities or path object. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy
, in order to free up system resourcesSignature
CreateGraphAlongPathBuilder(firstpvid, secondpvid)
Parameters: - firstpvid (int) –
- secondpvid (int) –
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Returns a builder used for creating the graph of result values series of entities or path object defined by result parameter. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy
, in order to free up system resourcesSignature
CreateGraphAlongPathBuilder(result, parameter)
Parameters: - result (
NXOpen.CAE.Result
) – set result - parameter (
NXOpen.CAE.ResultParameters
) –
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Returns a builder used for creating the graph of result values series of entities or path object defined by result parameter. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy
, in order to free up system resourcesSignature
CreateGraphAlongPathBuilder(parameter)
Parameters: parameter ( NXOpen.CAE.ResultProbe
) –Returns: Return type: NXOpen.CAE.PostGraphAlongPathBuilder
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Returns a builder used for creating the graph of result values of series of entities or path object defined by two result parameter. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy
, in order to free up system resourcesSignature
CreateGraphAlongPathBuilder(result, parameter1, parameter2)
Parameters: - result (
NXOpen.CAE.Result
) – set result - parameter1 (
NXOpen.CAE.ResultParameters
) – - parameter2 (
NXOpen.CAE.ResultParameters
) –
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
CreateGraphOrbitBuilder¶
-
ResultManager.
CreateGraphOrbitBuilder
¶ Overloaded method CreateGraphOrbitBuilder
CreateGraphOrbitBuilder(pvid)
CreateGraphOrbitBuilder(result, parameter)
-------------------------------------
Returns a builder used for creating the orbit graph from postview. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy
, in order to free up system resourcesSignature
CreateGraphOrbitBuilder(pvid)
Parameters: pvid (int) – Returns: Return type: NXOpen.CAE.PostGraphOrbitBuilder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Returns a builder used for creating the orbit graph from result defined by result parameter. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy
, in order to free up system resourcesSignature
CreateGraphOrbitBuilder(result, parameter)
Parameters: - result (
NXOpen.CAE.Result
) – set result - parameter (
NXOpen.CAE.ResultParameters
) –
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
CreateImportedResult¶
-
ResultManager.
CreateImportedResult
¶ Overloaded method CreateImportedResult
CreateImportedResult(filename, unitsystem)
CreateImportedResult(filename, resultname, unitsystem)
CreateImportedResult(filename, resultname)
-------------------------------------
Creates a imported result object given a solver results file and the unit systems that these results are defined in. It is user’s responsibility to destroy the result object once done using
NXOpen.CAE.ResultManager.DeleteResult
, in order to free up system resourcesSignature
CreateImportedResult(filename, unitsystem)
Parameters: - filename (str) – NOTE: The full Unicode character set is not supported for this parameter.
- unitsystem (
NXOpen.CAE.ResultResultBasicUnit_Struct
) –
Returns: Return type: New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Creates a imported result object given a solver results file and the unit systems that these results are defined in. It is user’s responsibility to destroy the result object once done using
NXOpen.CAE.ResultManager.DeleteResult
, in order to free up system resourcesSignature
CreateImportedResult(filename, resultname, unitsystem)
Parameters: - filename (str) – NOTE: The full Unicode character set is not supported for this parameter.
- resultname (str) – NOTE: The full Unicode character set is not supported for this parameter.
- unitsystem (
NXOpen.CAE.ResultResultBasicUnit_Struct
) –
Returns: Return type: New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Creates a imported result object given a solver results file. The unit systems is infered from the result file and Part. It is user’s responsibility to destroy the result object once done using
NXOpen.CAE.ResultManager.DeleteResult
, in order to free up system resourcesSignature
CreateImportedResult(filename, resultname)
Parameters: - filename (str) – NOTE: The full Unicode character set is not supported for this parameter.
- resultname (str) – NOTE: The full Unicode character set is not supported for this parameter.
Returns: Return type: New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
CreateJtBuilder¶
-
ResultManager.
CreateJtBuilder
¶ Creates a builder for exporting a component or result type JT
Signature
CreateJtBuilder()
Returns: Return type: NXOpen.CAE.CreateJtBuilder
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateLaminateDynamicEventResult¶
-
ResultManager.
CreateLaminateDynamicEventResult
¶ Creates a solution result object given a
NXOpen.CAE.LaminateDynamicEvent
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult
, in order to free up system resourcesSignature
CreateLaminateDynamicEventResult(dynEvent)
Parameters: dynEvent ( NXOpen.CAE.LaminateDynamicEvent
) – The dynamic eventReturns: Created solution result given the input dynamic event Return type: NXOpen.CAE.SolutionResult
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateLaminateGraphicalReportResult¶
-
ResultManager.
CreateLaminateGraphicalReportResult
¶ Creates a solution result object given a
NXOpen.CAE.LaminateGraphicalReport
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult
, in order to free up system resourcesSignature
CreateLaminateGraphicalReportResult(lamGraphReport)
Parameters: lamGraphReport ( NXOpen.CAE.LaminateGraphicalReport
) – The laminate graphical report specificationsReturns: Created solution result given the input laminate graphical report specifications Return type: NXOpen.CAE.SolutionResult
New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreatePostJtBuilder¶
-
ResultManager.
CreatePostJtBuilder
¶ Creates a builder for exporting a component or result type JT
Signature
CreatePostJtBuilder()
Returns: Return type: NXOpen.CAE.PostJtExportBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateReferenceResult¶
-
ResultManager.
CreateReferenceResult
¶ Creates a reference result object given a
NXOpen.CAE.SimResultReference
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult
, in order to free up system resourcesSignature
CreateReferenceResult(solution)
Parameters: solution ( NXOpen.CAE.SimResultReference
) –Returns: Return type: NXOpen.CAE.SolutionResult
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateResponseEventResult¶
-
ResultManager.
CreateResponseEventResult
¶ Creates a solution result object given a
NXOpen.CAE.ResponseSimulation.RSEvent
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult
, in order to free up system resourcesSignature
CreateResponseEventResult(responseSolution)
Parameters: responseSolution ( NXOpen.CAE.ResponseSimulation.RSEvent
) –Returns: Return type: NXOpen.CAE.SolutionResult
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateResponseSolutionResult¶
-
ResultManager.
CreateResponseSolutionResult
¶ Creates a solution result object given a
NXOpen.CAE.ResponseSimulation.Solution
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult
, in order to free up system resourcesSignature
CreateResponseSolutionResult(responseSolution)
Parameters: responseSolution ( NXOpen.CAE.ResponseSimulation.Solution
) –Returns: Return type: NXOpen.CAE.SolutionResult
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateResultAccess¶
-
ResultManager.
CreateResultAccess
¶ Overloaded method CreateResultAccess
CreateResultAccess(result, parameters)
CreateResultAccess(postViewID)
-------------------------------------
Creates a result access object It is user’s responsibility to destroy the result access object once done using
NXOpen.CAE.ResultManager.DeleteResultAccess
, in order to free up system resourcesSignature
CreateResultAccess(result, parameters)
Parameters: - result (
NXOpen.CAE.Result
) – analysis results for which you want to access information - parameters (
NXOpen.CAE.ResultParameters
) – defines the specific results state you wish to access
Returns: Return type: New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Creates a result access object based on an existing Post View It is user’s responsibility to destroy the result access object once done using
NXOpen.CAE.ResultManager.DeleteResultAccess
, in order to free up system resourcesSignature
CreateResultAccess(postViewID)
Parameters: postViewID (int) – an existing PostView Id Returns: Return type: NXOpen.CAE.ResultAccess
New in version NX8.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
CreateResultAccessReferenceField¶
-
ResultManager.
CreateResultAccessReferenceField
¶ Creates a result access reference field object.
The created field is automatically made persistent and stored in the collection of fields for the part.
Signature
CreateResultAccessReferenceField(fieldManager, result, parameters, depDemainName, fieldName)
Parameters: - fieldManager (
NXOpen.Fields.FieldManager
) – field manager in part - result (
NXOpen.CAE.Result
) – analysis results for which you want to access information - parameters (
NXOpen.CAE.ResultParameters
) – defines the specific results state you wish to access - depDemainName (str) – alphanumeric string; it must match with existing domain names NOTE: The full Unicode character set is not supported for this parameter.
- fieldName (str) – field name NOTE: The full Unicode character set is not supported for this parameter.
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- fieldManager (
CreateResultParameters¶
-
ResultManager.
CreateResultParameters
¶ Creates a result parameter object.
It is user’s responsibility to destroy the result parameters object once done using
NXOpen.CAE.ResultManager.DeleteResultParameters
, in order to free up system resourcesSignature
CreateResultParameters()
Returns: Return type: NXOpen.CAE.ResultParameters
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateResultParametersWithProbe¶
-
ResultManager.
CreateResultParametersWithProbe
¶ Creates a result parameter object for given Result Probe.
It is user’s responsibility to destroy the result parameters object once done using
NXOpen.CAE.ResultManager.DeleteResultParametersWithProbe
, in order to free up system resourcesSignature
CreateResultParametersWithProbe(resultProbe)
Parameters: resultProbe ( NXOpen.CAE.ResultProbe
) –Returns: Return type: NXOpen.CAE.ResultParametersWithProbe
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateResultsCombinationBuilder¶
-
ResultManager.
CreateResultsCombinationBuilder
¶ Creates a results combination builder.
It is user’s responsibility to destroy the builder object once done
Signature
CreateResultsCombinationBuilder()
Returns: Return type: NXOpen.CAE.ResultsCombinationBuilder
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateResultsEnvelopeBuilder¶
-
ResultManager.
CreateResultsEnvelopeBuilder
¶ Creates a results envelope builder.
It is user’s responsibility to destroy the builder object once done
Signature
CreateResultsEnvelopeBuilder()
Returns: Return type: NXOpen.CAE.ResultsEnvelopeBuilder
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateResultsModelExportBuilder¶
-
ResultManager.
CreateResultsModelExportBuilder
¶ Creates a model export builder.
It is user’s responsibility to destroy the builder object once done
Signature
CreateResultsModelExportBuilder()
Returns: Return type: NXOpen.CAE.ResultsModelExportBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateResultsReductionBuilder¶
-
ResultManager.
CreateResultsReductionBuilder
¶ Creates a results reduction builder.
It is user’s responsibility to destroy the builder object once done
Signature
CreateResultsReductionBuilder()
Returns: Return type: NXOpen.CAE.ResultsReductionBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateResultvariable¶
-
ResultManager.
CreateResultvariable
¶ Creates Result Variable object
Signature
CreateResultvariable(sim, quan, loc, comp, restypename, name)
Parameters: - sim (
NXOpen.CAE.SimSimulation
) – Simulation - quan (
NXOpen.CAE.ResultQuantity
) – - loc (
NXOpen.CAE.ResultLocation
) – - comp (
NXOpen.CAE.ResultComponent
) – - restypename (str) – Result Type UserName, If not sure pass empty string NOTE: The full Unicode character set is not supported for this parameter.
- name (str) – Result Variable name NOTE: The full Unicode character set is not supported for this parameter.
Returns: Return type: New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- sim (
CreateSeResult¶
-
ResultManager.
CreateSeResult
¶ Creates a result object given a seid within an existing
NXOpen.CAE.Result
.It is user’s responsibility to destroy the result object once done using
NXOpen.CAE.ResultManager.DeleteResult
, in order to free up system resourcesSignature
CreateSeResult(parentResult, seid)
Parameters: - parentResult (
NXOpen.CAE.Result
) – - seid (int) –
Returns: Return type: New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- parentResult (
CreateSolutionResult¶
-
ResultManager.
CreateSolutionResult
¶ Creates a solution result object given a
NXOpen.CAE.SimSolution
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult
, in order to free up system resourcesSignature
CreateSolutionResult(solution)
Parameters: solution ( NXOpen.CAE.SimSolution
) –Returns: Return type: NXOpen.CAE.SolutionResult
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateTableFieldFromProbe¶
-
ResultManager.
CreateTableFieldFromProbe
¶ Creates a field from the lists of independent, dependent variables along with a given Result Probe.
Signature
CreateTableFieldFromProbe(fieldName, indepVarArray, depVarArray, resultProbe, createTableOfFields)
Parameters: - fieldName (str) – field name NOTE: The full Unicode character set is not supported for this parameter.
- indepVarArray (list of
NXOpen.Fields.FieldVariable
) – independent variables to be associated with the table field - depVarArray (list of
NXOpen.Fields.FieldVariable
) – dependent variables to be associated with the table field - resultProbe (
NXOpen.CAE.ResultProbe
) – - createTableOfFields (bool) – When output field is both time/frequency and space varying, it is possble to create a table of fields
Returns: field
Return type: New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateTbsOptimizationSolutionResult¶
-
ResultManager.
CreateTbsOptimizationSolutionResult
¶ Creates a solution result object given a
NXOpen.CAE.Optimization.TBSOptimizationSolution
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult
, in order to free up system resourcesSignature
CreateTbsOptimizationSolutionResult(tbsOptimizationSolution)
Parameters: tbsOptimizationSolution ( NXOpen.CAE.Optimization.TBSOptimizationSolution
) –Returns: Return type: NXOpen.CAE.SolutionResult
New in version NX8.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateTransientResultsReductionBuilder¶
-
ResultManager.
CreateTransientResultsReductionBuilder
¶ Creates a transient results reduction builder.
It is user’s responsibility to destroy the builder object once done
Signature
CreateTransientResultsReductionBuilder()
Returns: Return type: NXOpen.CAE.TransientResultsReductionBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteClippingParameters¶
-
ResultManager.
DeleteClippingParameters
¶ Delete a
NXOpen.CAE.ClippingParameters
object.Signature
DeleteClippingParameters(result)
Parameters: result ( NXOpen.CAE.ClippingParameters
) –New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteCrossSectionParameters¶
-
ResultManager.
DeleteCrossSectionParameters
¶ Delete a
NXOpen.CAE.CrossSectionParameters
object.Signature
DeleteCrossSectionParameters(crossSection)
Parameters: crossSection ( NXOpen.CAE.CrossSectionParameters
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteDeformationParameters¶
-
ResultManager.
DeleteDeformationParameters
¶ Delete a
NXOpen.CAE.DeformationParameters
object.Signature
DeleteDeformationParameters(result)
Parameters: result ( NXOpen.CAE.DeformationParameters
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteFreeBodyResultsBuilder¶
-
ResultManager.
DeleteFreeBodyResultsBuilder
¶ Delete a
NXOpen.CAE.FreeBodyResultsBuilder
object.Signature
DeleteFreeBodyResultsBuilder(builder)
Parameters: builder ( NXOpen.CAE.FreeBodyResultsBuilder
) –New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeletePostJtBuilder¶
-
ResultManager.
DeletePostJtBuilder
¶ Delete a
NXOpen.CAE.PostJtExportBuilder
object.Signature
DeletePostJtBuilder(builder)
Parameters: builder ( NXOpen.CAE.PostJtExportBuilder
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteResult¶
-
ResultManager.
DeleteResult
¶ Delete a
NXOpen.CAE.Result
object.If a
NXOpen.CAE.ResultAccess
object referencing it, that will also be deletedSignature
DeleteResult(result)
Parameters: result ( NXOpen.CAE.Result
) –New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteResultAccess¶
-
ResultManager.
DeleteResultAccess
¶ Delete a
NXOpen.CAE.ResultAccess
object.Signature
DeleteResultAccess(result)
Parameters: result ( NXOpen.CAE.ResultAccess
) –New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteResultParameters¶
-
ResultManager.
DeleteResultParameters
¶ Delete a
NXOpen.CAE.ResultParameters
object.Signature
DeleteResultParameters(result)
Parameters: result ( NXOpen.CAE.ResultParameters
) –New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteResultParametersWithProbe¶
-
ResultManager.
DeleteResultParametersWithProbe
¶ Delete a
NXOpen.CAE.ResultParametersWithProbe
object.Signature
DeleteResultParametersWithProbe(result)
Parameters: result ( NXOpen.CAE.ResultParametersWithProbe
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
ResultManager.
FindObject
¶ Returns a
NXOpen.CAE.Result
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.TaggedObject
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)