FreeBodyResultsBuilder Class¶
-
class
NXOpen.CAE.
FreeBodyResultsBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.FreeBodyResultsBuilder
To obtain an instance of this class use
NXOpen.Session.ResultManager
.New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDisplayForce | Display Force @return Ask Display |
GetDisplayMoment | Display Moment @return Ask Moment |
GetElements | The free body elements @return Ask Elements |
GetForceColor | Force Color @return Ask Color |
GetForceVectorDisplay | Force vector display @return Ask force vector display |
GetIteration | The iteration containing the grid point force results @return Ask Iteration |
GetLocationCoords | The location definition method by coordinates @return Ask Coordinates |
GetLocationCsys | The location definition method by coordinate system origin @return Ask Coordinate System |
GetLocationCsysSource | The source for the location coordinate system @return Ask Source |
GetLocationId | The location definition method by node id @return Ask Node ID |
GetLocationMethod | The location definition method @return Ask Method |
GetMomentColor | Moment Color @return Ask Color |
GetMomentVectorDisplay | Moment vector display @return Ask moment vector display |
GetNodes | The interface nodes @return Ask Nodes |
GetObject | Returns the object currently being edited by this builder. |
GetOutputUnits | Output Units @return Ask Units |
GetPostview | The view where graphics will be displayed @return Ask View |
GetPrintOutput | Print Output @return Ask Print |
GetReferenceCsys | The reference coordinate system @return Ask Coordinate System |
GetSelectedReferenceCsys | The selected reference coordinate system @return Ask Coordinate System |
GetSelectedReferenceCsysSource | The source for the selected reference coordinate system @return Ask Source |
SetDisplayForce | Display Force |
SetDisplayMoment | Display Moment |
SetElements | The free body elements |
SetForceColor | Force Color |
SetForceVectorDisplay | Force vector display |
SetIteration | The iteration containing the grid point force results |
SetLocationCoords | The location definition method by coordinates |
SetLocationCsys | The location definition method by coordinate system origin |
SetLocationCsysSource | The source for the location coordinate system |
SetLocationId | The location definition method by node id |
SetLocationMethod | The location definition method |
SetMomentColor | Moment Color |
SetMomentVectorDisplay | Moment vector display |
SetNodes | The interface nodes |
SetOutputUnits | Output Units |
SetPostview | The view where graphics will be displayed |
SetPrintOutput | Print Output |
SetReferenceCsys | The reference coordinate system |
SetSelectedReferenceCsys | The selected reference coordinate system |
SetSelectedReferenceCsysSource | The source for the selected reference coordinate system |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FreeBodyResultsBuilderLocationMethod Enumeration | Location definition method |
FreeBodyResultsBuilderOutputUnits Enumeration | User Specified output units |
FreeBodyResultsBuilderVectorDisplay Enumeration | Vector display option |
Method Detail¶
GetDisplayForce¶
-
FreeBodyResultsBuilder.
GetDisplayForce
¶ Display Force
Signature
GetDisplayForce()
Returns: Ask Display Return type: bool New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetDisplayMoment¶
-
FreeBodyResultsBuilder.
GetDisplayMoment
¶ Display Moment
Signature
GetDisplayMoment()
Returns: Ask Moment Return type: bool New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetElements¶
-
FreeBodyResultsBuilder.
GetElements
¶ The free body elements
Signature
GetElements()
Returns: Ask Elements Return type: list of int New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetForceColor¶
-
FreeBodyResultsBuilder.
GetForceColor
¶ Force Color
Signature
GetForceColor()
Returns: Ask Color Return type: Id New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetForceVectorDisplay¶
-
FreeBodyResultsBuilder.
GetForceVectorDisplay
¶ Force vector display
Signature
GetForceVectorDisplay()
Returns: Ask force vector display Return type: NXOpen.CAE.FreeBodyResultsBuilderVectorDisplay
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetIteration¶
-
FreeBodyResultsBuilder.
GetIteration
¶ The iteration containing the grid point force results
Signature
GetIteration()
Returns: Ask Iteration Return type: NXOpen.CAE.BaseIteration
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetLocationCoords¶
-
FreeBodyResultsBuilder.
GetLocationCoords
¶ The location definition method by coordinates
Signature
GetLocationCoords()
Returns: Ask Coordinates Return type: NXOpen.Point3d
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetLocationCsys¶
-
FreeBodyResultsBuilder.
GetLocationCsys
¶ The location definition method by coordinate system origin
Signature
GetLocationCsys()
Returns: Ask Coordinate System Return type: int New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetLocationCsysSource¶
-
FreeBodyResultsBuilder.
GetLocationCsysSource
¶ The source for the location coordinate system
Signature
GetLocationCsysSource()
Returns: Ask Source Return type: NXOpen.CAE.ResultCoordinateSystemSource
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetLocationId¶
-
FreeBodyResultsBuilder.
GetLocationId
¶ The location definition method by node id
Signature
GetLocationId()
Returns: Ask Node ID Return type: int New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetLocationMethod¶
-
FreeBodyResultsBuilder.
GetLocationMethod
¶ The location definition method
Signature
GetLocationMethod()
Returns: Ask Method Return type: NXOpen.CAE.FreeBodyResultsBuilderLocationMethod
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetMomentColor¶
-
FreeBodyResultsBuilder.
GetMomentColor
¶ Moment Color
Signature
GetMomentColor()
Returns: Ask Color Return type: Id New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetMomentVectorDisplay¶
-
FreeBodyResultsBuilder.
GetMomentVectorDisplay
¶ Moment vector display
Signature
GetMomentVectorDisplay()
Returns: Ask moment vector display Return type: NXOpen.CAE.FreeBodyResultsBuilderVectorDisplay
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetNodes¶
-
FreeBodyResultsBuilder.
GetNodes
¶ The interface nodes
Signature
GetNodes()
Returns: Ask Nodes Return type: list of int New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetOutputUnits¶
-
FreeBodyResultsBuilder.
GetOutputUnits
¶ Output Units
Signature
GetOutputUnits()
Returns: Ask Units Return type: NXOpen.CAE.FreeBodyResultsBuilderOutputUnits
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetPostview¶
-
FreeBodyResultsBuilder.
GetPostview
¶ The view where graphics will be displayed
Signature
GetPostview()
Returns: Ask View Return type: int New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetPrintOutput¶
-
FreeBodyResultsBuilder.
GetPrintOutput
¶ Print Output
Signature
GetPrintOutput()
Returns: Ask Print Return type: bool New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetReferenceCsys¶
-
FreeBodyResultsBuilder.
GetReferenceCsys
¶ The reference coordinate system
Signature
GetReferenceCsys()
Returns: Ask Coordinate System Return type: NXOpen.CAE.ResultCoordinateSystem
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetSelectedReferenceCsys¶
-
FreeBodyResultsBuilder.
GetSelectedReferenceCsys
¶ The selected reference coordinate system
Signature
GetSelectedReferenceCsys()
Returns: Ask Coordinate System Return type: int New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetSelectedReferenceCsysSource¶
-
FreeBodyResultsBuilder.
GetSelectedReferenceCsysSource
¶ The source for the selected reference coordinate system
Signature
GetSelectedReferenceCsysSource()
Returns: Ask Source Return type: NXOpen.CAE.ResultCoordinateSystemSource
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetDisplayForce¶
-
FreeBodyResultsBuilder.
SetDisplayForce
¶ Display Force
Signature
SetDisplayForce(display)
Parameters: display (bool) – Set Display New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetDisplayMoment¶
-
FreeBodyResultsBuilder.
SetDisplayMoment
¶ Display Moment
Signature
SetDisplayMoment(display)
Parameters: display (bool) – Set Moment New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetElements¶
-
FreeBodyResultsBuilder.
SetElements
¶ The free body elements
Signature
SetElements(elements)
Parameters: elements (list of int) – Set Elements New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetForceColor¶
-
FreeBodyResultsBuilder.
SetForceColor
¶ Force Color
Signature
SetForceColor(display)
Parameters: display (Id) – Set Color New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetForceVectorDisplay¶
-
FreeBodyResultsBuilder.
SetForceVectorDisplay
¶ Force vector display
Signature
SetForceVectorDisplay(vectorDisplay)
Parameters: vectorDisplay ( NXOpen.CAE.FreeBodyResultsBuilderVectorDisplay
) – Set force vector displayNew in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetIteration¶
-
FreeBodyResultsBuilder.
SetIteration
¶ The iteration containing the grid point force results
Signature
SetIteration(iteration)
Parameters: iteration ( NXOpen.CAE.BaseIteration
) – Set IterationNew in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetLocationCoords¶
-
FreeBodyResultsBuilder.
SetLocationCoords
¶ The location definition method by coordinates
Signature
SetLocationCoords(coordinates)
Parameters: coordinates ( NXOpen.Point3d
) – Set CoordinatesNew in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetLocationCsys¶
-
FreeBodyResultsBuilder.
SetLocationCsys
¶ The location definition method by coordinate system origin
Signature
SetLocationCsys(id)
Parameters: id (int) – Set Node Coordinate System New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetLocationCsysSource¶
-
FreeBodyResultsBuilder.
SetLocationCsysSource
¶ The source for the location coordinate system
Signature
SetLocationCsysSource(source)
Parameters: source ( NXOpen.CAE.ResultCoordinateSystemSource
) – Set SourceNew in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetLocationId¶
-
FreeBodyResultsBuilder.
SetLocationId
¶ The location definition method by node id
Signature
SetLocationId(nodeId)
Parameters: nodeId (int) – Set Node ID New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetLocationMethod¶
-
FreeBodyResultsBuilder.
SetLocationMethod
¶ The location definition method
Signature
SetLocationMethod(method)
Parameters: method ( NXOpen.CAE.FreeBodyResultsBuilderLocationMethod
) – Set MethodNew in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetMomentColor¶
-
FreeBodyResultsBuilder.
SetMomentColor
¶ Moment Color
Signature
SetMomentColor(color)
Parameters: color (Id) – Set Color New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetMomentVectorDisplay¶
-
FreeBodyResultsBuilder.
SetMomentVectorDisplay
¶ Moment vector display
Signature
SetMomentVectorDisplay(vectorDisplay)
Parameters: vectorDisplay ( NXOpen.CAE.FreeBodyResultsBuilderVectorDisplay
) – Set moment vector displayNew in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetNodes¶
-
FreeBodyResultsBuilder.
SetNodes
¶ The interface nodes
Signature
SetNodes(nodes)
Parameters: nodes (list of int) – Set Nodes New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetOutputUnits¶
-
FreeBodyResultsBuilder.
SetOutputUnits
¶ Output Units
Signature
SetOutputUnits(units)
Parameters: units ( NXOpen.CAE.FreeBodyResultsBuilderOutputUnits
) – Set UnitsNew in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetPostview¶
-
FreeBodyResultsBuilder.
SetPostview
¶ The view where graphics will be displayed
Signature
SetPostview(postviewId)
Parameters: postviewId (int) – Set View New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetPrintOutput¶
-
FreeBodyResultsBuilder.
SetPrintOutput
¶ Print Output
Signature
SetPrintOutput(print)
Parameters: print (bool) – Set Print New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetReferenceCsys¶
-
FreeBodyResultsBuilder.
SetReferenceCsys
¶ The reference coordinate system
Signature
SetReferenceCsys(csys)
Parameters: csys ( NXOpen.CAE.ResultCoordinateSystem
) – Set Coordinate SystemNew in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetSelectedReferenceCsys¶
-
FreeBodyResultsBuilder.
SetSelectedReferenceCsys
¶ The selected reference coordinate system
Signature
SetSelectedReferenceCsys(id)
Parameters: id (int) – Set Coordinate System New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetSelectedReferenceCsysSource¶
-
FreeBodyResultsBuilder.
SetSelectedReferenceCsysSource
¶ The source for the selected reference coordinate system
Signature
SetSelectedReferenceCsysSource(source)
Parameters: source ( NXOpen.CAE.ResultCoordinateSystemSource
) – Set SourceNew in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Validate¶
-
FreeBodyResultsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.