BaseIteration Class¶
-
class
NXOpen.CAE.
BaseIteration
¶ Bases:
NXOpen.TaggedObject
This class provides interfaces to query iteration attributes
An instance of this class can not be obtained
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Name | Returns the name of the iteration |
Tag | Returns the Tag for this object. |
Type | Returns the type of the iteration |
Unit | Returns the units for the iteration value |
Value | Returns the iteration value |
ValueType | Returns the iteration value type |
Methods¶
Method | Description |
---|---|
Find | Returns a NXOpen.CAE.BaseResultType @return |
GetResultTypes | Returns the result types present in this iteration @return |
Enumerations¶
BaseIterationIterationType Enumeration | The Analysis type of a iteration object |
BaseIterationIterationValueType Enumeration | The type of value that is stored in a iteration object |
Property Detail¶
Name¶
-
BaseIteration.
Name
¶ Returns the name of the iteration
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Type¶
-
BaseIteration.
Type
¶ Returns the type of the iteration
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.CAE.BaseIterationIterationType
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Unit¶
-
BaseIteration.
Unit
¶ Returns the units for the iteration value
-------------------------------------
Getter Method
Signature
Unit()
Returns: Return type: NXOpen.Unit
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Value¶
-
BaseIteration.
Value
¶ Returns the iteration value
-------------------------------------
Getter Method
Signature
Value()
Returns: Return type: float New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ValueType¶
-
BaseIteration.
ValueType
¶ Returns the iteration value type
-------------------------------------
Getter Method
Signature
ValueType()
Returns: Return type: NXOpen.CAE.BaseIterationIterationValueType
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
Find¶
-
BaseIteration.
Find
¶ Returns a
NXOpen.CAE.BaseResultType
Signature
Find(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.TaggedObject
New in version NX7.5.0.
License requirements: None.
GetResultTypes¶
-
BaseIteration.
GetResultTypes
¶ Returns the result types present in this iteration
Signature
GetResultTypes()
Returns: Return type: list of NXOpen.CAE.BaseResultType
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)