FreeBodyResultsBuilderLocationMethod Enumeration¶
NXOpen.CAE.FreeBodyResultsBuilder.LocationMethod is an alias for NXOpen.CAE.FreeBodyResultsBuilderLocationMethod
-
class
NXOpen.CAE.
FreeBodyResultsBuilderLocationMethod
¶ Bases:
object
Location definition method
Enum Members
Enum Member Enum Member Description Id location is defined by node idCoords location is defined by coordinatesCsysorigin location is defined by coordinate system origin-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-