Solution Class¶
-
class
NXOpen.CAE.ResponseSimulation.
Solution
¶ Bases:
NXOpen.NXObject
Represents a meta solution providing response analysis functionalities in the .
sim file To create or edit an instance of this class, use
NXOpen.CAE.ResponseSimulation.SolutionBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ActiveEvent | Returns or sets the active event |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CheckObsoleteStatus | Checks status and updates solution properties for the solution which became obsolete because referenced modal shape file was changed. |
CloneEvent | Clones an event to the solution @return |
CloneSensor | Clones a sensor to the solution @return |
CloneStrainGage | Clones a strain gage to the solution @return |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
Destroy | Deletes a response simulation solution, including all events and excitations under it |
EvaluateFrf | Performs evaluation for FRF. |
EvaluateTransmissibility | Performs evaluation for transimissibility. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetEvaluationParameters | Returns the evaluation parameters of Response Analysis Meta solution @return |
GetEvents | Returns all the events of the solution @return |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetModalProperties | Returns the modal properties of Response Analysis Meta solution @return |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetResultFileName | Returns the result file name of solution @return |
GetSolutionName | Returns the response simulation solution name @return |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
ImportEvent | Imports an event to the solution @return |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetSolutionName | Sets the response simulation solution name |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
ActiveEvent¶
-
Solution.
ActiveEvent
¶ Returns or sets the active event
-------------------------------------
Getter Method
Signature
ActiveEvent()
Returns: Return type: NXOpen.CAE.ResponseSimulation.RSEvent
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ActiveEvent(activeEvent)
Parameters: activeEvent ( NXOpen.CAE.ResponseSimulation.RSEvent
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
IsOccurrence¶
-
Solution.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Solution.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
Solution.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Solution.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Solution.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
Solution.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
CheckObsoleteStatus¶
-
Solution.
CheckObsoleteStatus
¶ Checks status and updates solution properties for the solution which became obsolete because referenced modal shape file was changed.
The solution will be reactivated as normal state after status checking.
Signature
CheckObsoleteStatus()
New in version NX8.0.1.
License requirements: nx_response_anlys (“NX Response Analysis”)
CloneEvent¶
-
Solution.
CloneEvent
¶ Clones an event to the solution
Signature
CloneEvent(sourceEvent, suggestedName)
Parameters: - sourceEvent (
NXOpen.CAE.ResponseSimulation.RSEvent
) – - suggestedName (str) – NOTE: The full Unicode character set is not supported for this parameter.
Returns: Return type: New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
- sourceEvent (
CloneSensor¶
-
Solution.
CloneSensor
¶ Clones a sensor to the solution
Signature
CloneSensor(sourceSensor, suggestedName)
Parameters: - sourceSensor (
NXOpen.CAE.ResponseSimulation.Sensor
) – - suggestedName (str) – NOTE: The full Unicode character set is not supported for this parameter.
Returns: Return type: New in version NX5.0.1.
License requirements: nx_response_anlys (“NX Response Analysis”)
- sourceSensor (
CloneStrainGage¶
-
Solution.
CloneStrainGage
¶ Clones a strain gage to the solution
Signature
CloneStrainGage(sourceGage, suggestedName)
Parameters: - sourceGage (
NXOpen.CAE.ResponseSimulation.StrainGage
) – - suggestedName (str) – NOTE: The full Unicode character set is not supported for this parameter.
Returns: Return type: New in version NX5.0.1.
License requirements: nx_response_anlys (“NX Response Analysis”)
- sourceGage (
Destroy¶
-
Solution.
Destroy
¶ Deletes a response simulation solution, including all events and excitations under it
Signature
Destroy(deleteResultFile)
Parameters: deleteResultFile (bool) – delete the result files associated with the solution or not New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
EvaluateFrf¶
-
Solution.
EvaluateFrf
¶ Performs evaluation for FRF.
The evaluation results will be stored in an AFU file, which name could be returned by
NXOpen.CAE.ResponseSimulation.Solution.GetResultFileName
Signature
EvaluateFrf(evaluationSetting)
Parameters: evaluationSetting ( NXOpen.CAE.ResponseSimulation.FrfEvaluationSetting
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
EvaluateTransmissibility¶
-
Solution.
EvaluateTransmissibility
¶ Performs evaluation for transimissibility.
The evaluation results will be stored in an AFU file, which name could be returned by
NXOpen.CAE.ResponseSimulation.Solution.GetResultFileName
Signature
EvaluateTransmissibility(evaluationSetting)
Parameters: evaluationSetting ( NXOpen.CAE.ResponseSimulation.TransmissibilityEvaluationSetting
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
FindObject¶
-
Solution.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetEvaluationParameters¶
-
Solution.
GetEvaluationParameters
¶ Returns the evaluation parameters of Response Analysis Meta solution
Signature
GetEvaluationParameters()
Returns: Return type: NXOpen.CAE.ResponseSimulation.EvaluationParameters
New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
GetEvents¶
-
Solution.
GetEvents
¶ Returns all the events of the solution
Signature
GetEvents()
Returns: Return type: list of NXOpen.CAE.ResponseSimulation.RSEvent
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
GetModalProperties¶
-
Solution.
GetModalProperties
¶ Returns the modal properties of Response Analysis Meta solution
Signature
GetModalProperties()
Returns: Return type: NXOpen.CAE.ResponseSimulation.ModalProperties
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
GetResultFileName¶
-
Solution.
GetResultFileName
¶ Returns the result file name of solution
Signature
GetResultFileName()
Returns: Return type: str New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
GetSolutionName¶
-
Solution.
GetSolutionName
¶ Returns the response simulation solution name
Signature
GetSolutionName()
Returns: Return type: str New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ImportEvent¶
-
Solution.
ImportEvent
¶ Imports an event to the solution
Signature
ImportEvent(eventDefinitionFile, suggestedName)
Parameters: - eventDefinitionFile (str) – NOTE: The full Unicode character set is not supported for this parameter.
- suggestedName (str) – NOTE: The full Unicode character set is not supported for this parameter.
Returns: Return type: New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Print¶
-
Solution.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
Solution.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetSolutionName¶
-
Solution.
SetSolutionName
¶ Sets the response simulation solution name
Signature
SetSolutionName(solutionName, renameResultFile)
Parameters: - solutionName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- renameResultFile (bool) – if there are result files associated with the solution, rename the files or not
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)