EvaluationParameters Class¶
-
class
NXOpen.CAE.ResponseSimulation.
EvaluationParameters
¶ Bases:
NXOpen.TaggedObject
Represents the evaluation parameters for a response simulation meta solution
Not support KF.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
HypermatrixBufferSize | Returns or sets the buffer allocated for Hypermatrix files |
IntegrationMethod | Returns or sets the integration method used for transient analysis |
MaxArraySize | Returns or sets the dynamic storage array size allocated for RS evaluations |
MinDampingStatus | Returns or sets the minimum damping ratio status |
Tag | Returns the Tag for this object. |
ZeroMeanCorrection | Returns or sets the time-domain integration of acceleration excitations, used in evaluating time responses to acceleration loads. |
Methods¶
Enumerations¶
EvaluationParametersAnalysisIntegrationMethod Enumeration | the integration method used for transient analysis |
Property Detail¶
HypermatrixBufferSize¶
-
EvaluationParameters.
HypermatrixBufferSize
¶ Returns or sets the buffer allocated for Hypermatrix files
-------------------------------------
Getter Method
Signature
HypermatrixBufferSize()
Returns: Return type: int New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
HypermatrixBufferSize(bufferSize)
Parameters: bufferSize (int) – New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
IntegrationMethod¶
-
EvaluationParameters.
IntegrationMethod
¶ Returns or sets the integration method used for transient analysis
-------------------------------------
Getter Method
Signature
IntegrationMethod()
Returns: Return type: NXOpen.CAE.ResponseSimulation.EvaluationParametersAnalysisIntegrationMethod
New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
IntegrationMethod(method)
Parameters: method ( NXOpen.CAE.ResponseSimulation.EvaluationParametersAnalysisIntegrationMethod
) –New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
MaxArraySize¶
-
EvaluationParameters.
MaxArraySize
¶ Returns or sets the dynamic storage array size allocated for RS evaluations
-------------------------------------
Getter Method
Signature
MaxArraySize()
Returns: Return type: int New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
MaxArraySize(maxArraySize)
Parameters: maxArraySize (int) – New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
MinDampingStatus¶
-
EvaluationParameters.
MinDampingStatus
¶ Returns or sets the minimum damping ratio status
-------------------------------------
Getter Method
Signature
MinDampingStatus()
Returns: Return type: bool New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
MinDampingStatus(dampingStatus)
Parameters: dampingStatus (bool) – New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ZeroMeanCorrection¶
-
EvaluationParameters.
ZeroMeanCorrection
¶ Returns or sets the time-domain integration of acceleration excitations, used in evaluating time responses to acceleration loads.
false: no correction, meaning that “rigid drifting” shows in the displacement response when an acceleration excitation is applied; true: the software corrects for drifting by assuming a zero mean. Rigid drifting is filtered out based on a numerical integration that does not assume an initial condition.
-------------------------------------
Getter Method
Signature
ZeroMeanCorrection()
Returns: Return type: bool New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ZeroMeanCorrection(correctionValue)
Parameters: correctionValue (bool) – New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)