CreateJtBuilder Class¶
-
class
NXOpen.CAE.
CreateJtBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.CreateJtBuilder
To obtain an instance of this class use
NXOpen.Session.ResultManager
.New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetExportData | The result parameters |
SetOutputFile | The output file |
SetResult | The result |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CreateJtBuilderComponent Enumeration | This option is used to set the component for export |
Method Detail¶
SetExportData¶
-
CreateJtBuilder.
SetExportData
¶ The result parameters
Signature
SetExportData(parameters, templateIds, componentToExport)
Parameters: - parameters (list of
NXOpen.CAE.ResultParameters
) – set result parameters - templateIds (list of int) – set template Id per result parameter
- componentToExport (list of
NXOpen.CAE.CreateJtBuilderComponent
) – set template Id per result parameter
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- parameters (list of
SetOutputFile¶
-
CreateJtBuilder.
SetOutputFile
¶ The output file
Signature
SetOutputFile(outputFile)
Parameters: outputFile (str) – set output file NOTE: The full Unicode character set is not supported for this parameter. New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetResult¶
-
CreateJtBuilder.
SetResult
¶ The result
Signature
SetResult(result)
Parameters: result ( NXOpen.CAE.Result
) – set resultNew in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Validate¶
-
CreateJtBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.