ResultParameters Class¶
-
class
NXOpen.CAE.
ResultParameters
¶ Bases:
NXOpen.TaggedObject
This class is worked as a packet of information that can be either be used to change result state or pass around for information exchange between two
NXOpen.CAE.ResultAccess
objects.<br/>Use
NXOpen.CAE.ResultManager
to create anNXOpen.CAE.ResultParameters
<br/>You can modifiy these values but validation of correctness will only be perfomed when this object is set to a
NXOpen.CAE.ResultAccess
objectTo obtain an instance of this class use
NXOpen.Session.ResultManager
.New in version NX6.0.2.
Methods¶
Method | Description |
---|---|
AskSectionPlyLayer | Ask section, ply and layer @return |
DisplayMidnodeValue | This is display only command. |
GetAbsoluteValue | Ask whether all values are absolute values @return |
GetAveragingCriteria | Ask averaging criteria. |
GetBeamFilletRadius | Return the fillet radius @return |
GetBeamFillets | Return the fillets flag @return |
GetBeamResultsInLocalCoordinateSystem | Identifies whether beam results are presented in local coordinate system (if true) or in the same coordinate system as the rest of the model @return |
GetCalculateBeamStrResults | Ask if beam stresses and strains are calculated from element forces and section geometry @return |
GetComplexCriterion | If result is complex it returns which component is set(like real or imaginary) @return |
GetComputationType | Get computing type. |
GetCoordinateSystem | Ask result coordinate system @return |
GetElementValueCriterion | Ask how element the result is defined. |
GetExcludeElementsNotVisible | Ask whether elements which are not visible are consider for summation @return |
GetGenericResultType | Ask Result type @return |
GetIteration | Ask Current iteration number This method has been deprecated. |
GetLoadcase | Ask Current loadcase number This method has been deprecated. |
GetPhaseAngle | Ask phase angle. |
GetResultBeamSection | Ask section where beam results are defined @return |
GetResultComponent | Ask result component @return |
GetResultDataLocation | Ask FE entity where the result is defined This method has been deprecated. |
GetResultDataQuantity | Ask result type This method has been deprecated. |
GetResultDataSection | Ask section of a FE entity where the result is defined This method has been deprecated. |
GetResultShellSection | Ask section where shell results are defined @return |
GetResultType | Ask Result type This method has been deprecated. |
GetRotationAxisOfAbsoluteCyndricalCSYS | Get axis of rotation for axisyymettric results @return |
GetScale | Ask scale @return |
GetSelectedCoordinateSystem | Ask selected coordinate system in which results are to be presented |
GetTensorComponentAbsoluteValue | Get the method used when calculating the absolute values for the derived components of CAE.ResultDataType.Tensor like CAE.ResultComponent.MaximumPrincipal @return |
GetUnit | Ask result unit @return |
InitAveragingCriteria | Ask default averaging criteria @return |
IsForcedElementResult | Ask whether the result is converted as element result @return |
IsMidnodeValueDisplayed | Ask whether the result at mid nodes are ignored @return |
MakeElementResult | Make Nodal and Element-Nodal result to Element Result. |
SetAbsoluteValue | Set all values to absolute values. |
SetAveragingCriteria | Set averaging criteria |
SetBeamFilletRadius | Sets the fillet radius as a fraction of the adjacent dimensions |
SetBeamFillets | Sets the fillets flag |
SetBeamResultsInLocalCoordinateSystem | Presents beam results in local coordinate system (if flag is true) or in the same coordinate system as the rest of the model |
SetCalculateBeamStrResults | Sets a flag to calculate beam stresses and strains from element forces and section geometry (if available). |
SetComplexCriterion | Set complex criteria |
SetComputationType | Set computing type. |
SetCoordinateSystem | Set result coordinate system |
SetElementValueCriterion | Set how element the result is defined This option is only valid for nodal and elemen-nodal result; dose not do anything for element result. |
SetExcludeElementsNotVisible | Exclude or include elements which are not visible for computing with sum option. |
SetGenericResultType | Set Result type |
SetLoadcaseIteration | Set Current loadcase and iteration. |
SetPhaseAngle | Sets the phase angle at which result will be evaluated. |
SetResultBeamSection | Set section where beam results are defined |
SetResultComponent | Set result component |
SetResultDataLocation | Set FE entity where the result is defined This method has been deprecated. |
SetResultDataQuantity | Set result quantity This method has been deprecated. |
SetResultDataSection | Set section of a FE entity where the result is defined This method has been deprecated. |
SetResultShellSection | Set section where shell results are defined |
SetResultType | Set Result type This method has been deprecated. |
SetRotationAxisOfAbsoluteCyndricalCSYS | Set axis of rotation for axisymmetric results |
SetScale | Set scale. |
SetSectionPlyLayer | Set section, ply and layer |
SetSelectedCoordinateSystem | Set selected coordinate system in which results are to be presented Coordinate systems labels defined in a result file can be retrieved using CAE.Result.GetResultCoordinateSystems |
SetTensorComponentAbsoluteValue | Set the method used when calculating the absolute values for the derived components of CAE.ResultDataType.Tensor like CAE.ResultComponent.MaximumPrincipal |
SetUnit | Set result unit |
Method Detail¶
AskSectionPlyLayer¶
-
ResultParameters.
AskSectionPlyLayer
¶ Ask section, ply and layer
Signature
AskSectionPlyLayer()
Returns: a tuple Return type: A tuple consisting of (layer, section, ply). layer is a int. section is a int. ply is a int. New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DisplayMidnodeValue¶
-
ResultParameters.
DisplayMidnodeValue
¶ This is display only command.
Setting this value will not change modify ResultAccess queries. But Post view will ignore midnode values during display
Signature
DisplayMidnodeValue(display)
Parameters: display (bool) – New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetAbsoluteValue¶
-
ResultParameters.
GetAbsoluteValue
¶ Ask whether all values are absolute values
Signature
GetAbsoluteValue()
Returns: Return type: bool New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetAveragingCriteria¶
-
ResultParameters.
GetAveragingCriteria
¶ Ask averaging criteria.
Signature
GetAveragingCriteria()
Returns: Return type: NXOpen.CAE.ResultAveraging_Struct
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetBeamFilletRadius¶
-
ResultParameters.
GetBeamFilletRadius
¶ Return the fillet radius
Signature
GetBeamFilletRadius()
Returns: Return type: float New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetBeamFillets¶
-
ResultParameters.
GetBeamFillets
¶ Return the fillets flag
Signature
GetBeamFillets()
Returns: Return type: bool New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetBeamResultsInLocalCoordinateSystem¶
-
ResultParameters.
GetBeamResultsInLocalCoordinateSystem
¶ Identifies whether beam results are presented in local coordinate system (if true) or in the same coordinate system as the rest of the model
Signature
GetBeamResultsInLocalCoordinateSystem()
Returns: Return type: bool New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetCalculateBeamStrResults¶
-
ResultParameters.
GetCalculateBeamStrResults
¶ Ask if beam stresses and strains are calculated from element forces and section geometry
Signature
GetCalculateBeamStrResults()
Returns: Return type: bool New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetComplexCriterion¶
-
ResultParameters.
GetComplexCriterion
¶ If result is complex it returns which component is set(like real or imaginary)
Signature
GetComplexCriterion()
Returns: Return type: NXOpen.CAE.ResultComplex
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetComputationType¶
-
ResultParameters.
GetComputationType
¶ Get computing type.
Signature
GetComputationType()
Returns: Return type: NXOpen.CAE.ResultComputationType
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetCoordinateSystem¶
-
ResultParameters.
GetCoordinateSystem
¶ Ask result coordinate system
Signature
GetCoordinateSystem()
Returns: Return type: NXOpen.CAE.ResultCoordinateSystem
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetElementValueCriterion¶
-
ResultParameters.
GetElementValueCriterion
¶ Ask how element the result is defined.
This option is only valid for nodal and elemen-nodal result.
Signature
GetElementValueCriterion()
Returns: Return type: NXOpen.CAE.ResultElementValueCriterion
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetExcludeElementsNotVisible¶
-
ResultParameters.
GetExcludeElementsNotVisible
¶ Ask whether elements which are not visible are consider for summation
Signature
GetExcludeElementsNotVisible()
Returns: Return type: bool New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetGenericResultType¶
-
ResultParameters.
GetGenericResultType
¶ Ask Result type
Signature
GetGenericResultType()
Returns: Return type: NXOpen.CAE.BaseResultType
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetIteration¶
-
ResultParameters.
GetIteration
¶ Ask Current iteration number This method has been deprecated.
This functionality was moved to this class
NXOpen.CAE.BaseResultType
, which can be obtained by usingNXOpen.CAE.ResultParameters.GetGenericResultType
.Signature
GetIteration()
Returns: Return type: int New in version NX6.0.2.
Deprecated since version NX8.0.0: Use
NXOpen.CAE.ResultParameters.GetGenericResultType
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetLoadcase¶
-
ResultParameters.
GetLoadcase
¶ Ask Current loadcase number This method has been deprecated.
This functionality was moved to this class
NXOpen.CAE.BaseResultType
, which can be obtained by usingNXOpen.CAE.ResultParameters.GetGenericResultType
.Signature
GetLoadcase()
Returns: Return type: int New in version NX6.0.2.
Deprecated since version NX8.0.0: Use
NXOpen.CAE.ResultParameters.GetGenericResultType
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetPhaseAngle¶
-
ResultParameters.
GetPhaseAngle
¶ Ask phase angle.
If complex result is set to Phaseangle type then user can specify an angle at which result will be evaluated
Signature
GetPhaseAngle()
Returns: Return type: float New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetResultBeamSection¶
-
ResultParameters.
GetResultBeamSection
¶ Ask section where beam results are defined
Signature
GetResultBeamSection()
Returns: Return type: NXOpen.CAE.ResultSection
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetResultComponent¶
-
ResultParameters.
GetResultComponent
¶ Ask result component
Signature
GetResultComponent()
Returns: Return type: NXOpen.CAE.ResultComponent
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetResultDataLocation¶
-
ResultParameters.
GetResultDataLocation
¶ Ask FE entity where the result is defined This method has been deprecated.
This functionality was moved to this class
NXOpen.CAE.BaseResultType
, which can be obtained by usingNXOpen.CAE.ResultParameters.GetGenericResultType
.Signature
GetResultDataLocation()
Returns: Return type: NXOpen.CAE.ResultLocation
New in version NX6.0.2.
Deprecated since version NX8.0.0: Use
NXOpen.CAE.BaseResultType.Location
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetResultDataQuantity¶
-
ResultParameters.
GetResultDataQuantity
¶ Ask result type This method has been deprecated.
This functionality was moved to this class
NXOpen.CAE.BaseResultType
, which can be obtained by usingNXOpen.CAE.ResultParameters.GetGenericResultType
.Signature
GetResultDataQuantity()
Returns: Return type: NXOpen.CAE.ResultQuantity
New in version NX6.0.2.
Deprecated since version NX8.0.0: Use
NXOpen.CAE.ResultParameters.GetGenericResultType
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetResultDataSection¶
-
ResultParameters.
GetResultDataSection
¶ Ask section of a FE entity where the result is defined This method has been deprecated.
This functionality was moved to this class
NXOpen.CAE.BaseResultType
, which can be obtained by usingNXOpen.CAE.ResultParameters.GetGenericResultType
.Signature
GetResultDataSection()
Returns: Return type: NXOpen.CAE.ResultSection
New in version NX6.0.2.
Deprecated since version NX8.0.0: Use
NXOpen.CAE.ResultParameters.GetGenericResultType
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetResultShellSection¶
-
ResultParameters.
GetResultShellSection
¶ Ask section where shell results are defined
Signature
GetResultShellSection()
Returns: Return type: NXOpen.CAE.ResultSection
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetResultType¶
-
ResultParameters.
GetResultType
¶ Ask Result type This method has been deprecated.
This functionality was moved to this class
NXOpen.CAE.BaseResultType
, which can be obtained by usingNXOpen.CAE.ResultParameters.GetGenericResultType
.Signature
GetResultType()
Returns: Return type: NXOpen.CAE.ResultType_Struct
New in version NX6.0.2.
Deprecated since version NX8.0.0: Use
NXOpen.CAE.ResultParameters.GetGenericResultType
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetRotationAxisOfAbsoluteCyndricalCSYS¶
-
ResultParameters.
GetRotationAxisOfAbsoluteCyndricalCSYS
¶ Get axis of rotation for axisyymettric results
Signature
GetRotationAxisOfAbsoluteCyndricalCSYS()
Returns: Return type: NXOpen.CAE.PostAxisymetricAxis
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetScale¶
-
ResultParameters.
GetScale
¶ Ask scale
Signature
GetScale()
Returns: Return type: float New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetSelectedCoordinateSystem¶
-
ResultParameters.
GetSelectedCoordinateSystem
¶ Ask selected coordinate system in which results are to be presented
Signature
GetSelectedCoordinateSystem()
Returns: a tuple Return type: A tuple consisting of (source, id). source is a NXOpen.CAE.ResultCoordinateSystemSource
. id is a int.New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetTensorComponentAbsoluteValue¶
-
ResultParameters.
GetTensorComponentAbsoluteValue
¶ Get the method used when calculating the absolute values for the derived components of
CAE.ResultDataType.Tensor
likeCAE.ResultComponent.MaximumPrincipal
Signature
GetTensorComponentAbsoluteValue()
Returns: Return type: NXOpen.CAE.ResultTensorDerivedAbsolute
New in version NX8.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetUnit¶
-
ResultParameters.
GetUnit
¶ Ask result unit
Signature
GetUnit()
Returns: Return type: NXOpen.Unit
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
InitAveragingCriteria¶
-
ResultParameters.
InitAveragingCriteria
¶ Ask default averaging criteria
Signature
InitAveragingCriteria()
Returns: Return type: NXOpen.CAE.ResultAveraging_Struct
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsForcedElementResult¶
-
ResultParameters.
IsForcedElementResult
¶ Ask whether the result is converted as element result
Signature
IsForcedElementResult()
Returns: Return type: bool New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsMidnodeValueDisplayed¶
-
ResultParameters.
IsMidnodeValueDisplayed
¶ Ask whether the result at mid nodes are ignored
Signature
IsMidnodeValueDisplayed()
Returns: Return type: bool New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
MakeElementResult¶
-
ResultParameters.
MakeElementResult
¶ Make Nodal and Element-Nodal result to Element Result.
Does not do anything if the result is element result already. To define what value should be used to represent an element, use
NXOpen.CAE.ResultParameters.SetElementValueCriterion
Signature
MakeElementResult(elementResult)
Parameters: elementResult (bool) – New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetAbsoluteValue¶
-
ResultParameters.
SetAbsoluteValue
¶ Set all values to absolute values.
Warning: Once converted to absolute value it is not possible to revert to original values.
Signature
SetAbsoluteValue(absolute)
Parameters: absolute (bool) – New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetAveragingCriteria¶
-
ResultParameters.
SetAveragingCriteria
¶ Set averaging criteria
Signature
SetAveragingCriteria(average)
Parameters: average ( NXOpen.CAE.ResultAveraging_Struct
) –New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetBeamFilletRadius¶
-
ResultParameters.
SetBeamFilletRadius
¶ Sets the fillet radius as a fraction of the adjacent dimensions
Signature
SetBeamFilletRadius(beamFilletRadius)
Parameters: beamFilletRadius (float) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetBeamFillets¶
-
ResultParameters.
SetBeamFillets
¶ Sets the fillets flag
Signature
SetBeamFillets(beamFillets)
Parameters: beamFillets (bool) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetBeamResultsInLocalCoordinateSystem¶
-
ResultParameters.
SetBeamResultsInLocalCoordinateSystem
¶ Presents beam results in local coordinate system (if flag is true) or in the same coordinate system as the rest of the model
Signature
SetBeamResultsInLocalCoordinateSystem(local)
Parameters: local (bool) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetCalculateBeamStrResults¶
-
ResultParameters.
SetCalculateBeamStrResults
¶ Sets a flag to calculate beam stresses and strains from element forces and section geometry (if available).
Does not affect other result types and element types
Signature
SetCalculateBeamStrResults(calcBeamStrResults)
Parameters: calcBeamStrResults (bool) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetComplexCriterion¶
-
ResultParameters.
SetComplexCriterion
¶ Set complex criteria
Signature
SetComplexCriterion(complex)
Parameters: complex ( NXOpen.CAE.ResultComplex
) –New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetComputationType¶
-
ResultParameters.
SetComputationType
¶ Set computing type.
Signature
SetComputationType(computeType)
Parameters: computeType ( NXOpen.CAE.ResultComputationType
) –New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetCoordinateSystem¶
-
ResultParameters.
SetCoordinateSystem
¶ Set result coordinate system
Signature
SetCoordinateSystem(coordinate)
Parameters: coordinate ( NXOpen.CAE.ResultCoordinateSystem
) –New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetElementValueCriterion¶
-
ResultParameters.
SetElementValueCriterion
¶ Set how element the result is defined This option is only valid for nodal and elemen-nodal result; dose not do anything for element result.
Signature
SetElementValueCriterion(criteria)
Parameters: criteria ( NXOpen.CAE.ResultElementValueCriterion
) –New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetExcludeElementsNotVisible¶
-
ResultParameters.
SetExcludeElementsNotVisible
¶ Exclude or include elements which are not visible for computing with sum option.
Signature
SetExcludeElementsNotVisible(excludeElements)
Parameters: excludeElements (bool) – New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetGenericResultType¶
-
ResultParameters.
SetGenericResultType
¶ Set Result type
Signature
SetGenericResultType(type)
Parameters: type ( NXOpen.CAE.BaseResultType
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetLoadcaseIteration¶
-
ResultParameters.
SetLoadcaseIteration
¶ Set Current loadcase and iteration.
This method has been deprecated. This functionality was moved to this class
NXOpen.CAE.BaseResultType
, which can be obtained by usingNXOpen.CAE.ResultParameters.GetGenericResultType
.Signature
SetLoadcaseIteration(loadcase, iteration)
Parameters: - loadcase (int) – loadcase number varies from 0 to N-1
- iteration (int) – iteration number varies from 0 to N-1
New in version NX6.0.2.
Deprecated since version NX8.0.0: Use
NXOpen.CAE.ResultParameters.SetGenericResultType
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetPhaseAngle¶
-
ResultParameters.
SetPhaseAngle
¶ Sets the phase angle at which result will be evaluated.
This is only value if complex result is set to the PhaseAngle type
Signature
SetPhaseAngle(angle)
Parameters: angle (float) – New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetResultBeamSection¶
-
ResultParameters.
SetResultBeamSection
¶ Set section where beam results are defined
Signature
SetResultBeamSection(section)
Parameters: section ( NXOpen.CAE.ResultSection
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetResultComponent¶
-
ResultParameters.
SetResultComponent
¶ Set result component
Signature
SetResultComponent(component)
Parameters: component ( NXOpen.CAE.ResultComponent
) –New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetResultDataLocation¶
-
ResultParameters.
SetResultDataLocation
¶ Set FE entity where the result is defined This method has been deprecated.
This functionality was moved to this class
NXOpen.CAE.BaseResultType
, which can be obtained by usingNXOpen.CAE.ResultParameters.GetGenericResultType
.Signature
SetResultDataLocation(location)
Parameters: location ( NXOpen.CAE.ResultLocation
) –New in version NX6.0.2.
Deprecated since version NX8.0.0: Use
NXOpen.CAE.ResultParameters.GetGenericResultType
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetResultDataQuantity¶
-
ResultParameters.
SetResultDataQuantity
¶ Set result quantity This method has been deprecated.
This functionality was moved to this class
NXOpen.CAE.BaseResultType
, which can be obtained by usingNXOpen.CAE.ResultParameters.GetGenericResultType
.Signature
SetResultDataQuantity(quantity)
Parameters: quantity ( NXOpen.CAE.ResultQuantity
) –New in version NX6.0.2.
Deprecated since version NX8.0.0: Use
NXOpen.CAE.ResultParameters.GetGenericResultType
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetResultDataSection¶
-
ResultParameters.
SetResultDataSection
¶ Set section of a FE entity where the result is defined This method has been deprecated.
This functionality was moved to this class
NXOpen.CAE.BaseResultType
, which can be obtained by usingNXOpen.CAE.ResultParameters.GetGenericResultType
.Signature
SetResultDataSection(section)
Parameters: section ( NXOpen.CAE.ResultSection
) –New in version NX6.0.2.
Deprecated since version NX8.0.0: Use
NXOpen.CAE.ResultParameters.GetGenericResultType
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetResultShellSection¶
-
ResultParameters.
SetResultShellSection
¶ Set section where shell results are defined
Signature
SetResultShellSection(section)
Parameters: section ( NXOpen.CAE.ResultSection
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetResultType¶
-
ResultParameters.
SetResultType
¶ Set Result type This method has been deprecated.
This functionality was moved to this class
NXOpen.CAE.BaseResultType
, which can be obtained by usingNXOpen.CAE.ResultParameters.GetGenericResultType
.Signature
SetResultType(type)
Parameters: type ( NXOpen.CAE.ResultType_Struct
) –New in version NX6.0.2.
Deprecated since version NX8.0.0: Use
NXOpen.CAE.ResultParameters.GetGenericResultType
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetRotationAxisOfAbsoluteCyndricalCSYS¶
-
ResultParameters.
SetRotationAxisOfAbsoluteCyndricalCSYS
¶ Set axis of rotation for axisymmetric results
Signature
SetRotationAxisOfAbsoluteCyndricalCSYS(axis)
Parameters: axis ( NXOpen.CAE.PostAxisymetricAxis
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetScale¶
-
ResultParameters.
SetScale
¶ Set scale.
This will affect all subsequent result query.
Signature
SetScale(scale)
Parameters: scale (float) – New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetSectionPlyLayer¶
-
ResultParameters.
SetSectionPlyLayer
¶ Set section, ply and layer
Signature
SetSectionPlyLayer(section, ply, layer)
Parameters: - section (int) –
- ply (int) –
- layer (int) –
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetSelectedCoordinateSystem¶
-
ResultParameters.
SetSelectedCoordinateSystem
¶ Set selected coordinate system in which results are to be presented Coordinate systems labels defined in a result file can be retrieved using
CAE.Result.GetResultCoordinateSystems
Signature
SetSelectedCoordinateSystem(source, id)
Parameters: - source (
NXOpen.CAE.ResultCoordinateSystemSource
) – - id (int) –
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- source (
SetTensorComponentAbsoluteValue¶
-
ResultParameters.
SetTensorComponentAbsoluteValue
¶ Set the method used when calculating the absolute values for the derived components of
CAE.ResultDataType.Tensor
likeCAE.ResultComponent.MaximumPrincipal
Signature
SetTensorComponentAbsoluteValue(absolute)
Parameters: absolute ( NXOpen.CAE.ResultTensorDerivedAbsolute
) –New in version NX8.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetUnit¶
-
ResultParameters.
SetUnit
¶ Set result unit
Signature
SetUnit(unit)
Parameters: unit ( NXOpen.Unit
) –New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)