FieldTable Class¶
-
class
NXOpen.Fields.
FieldTable
¶ Bases:
NXOpen.Fields.Field
Represents the Field Table class.
A field (see
NXOpen.Fields.Field
) defined in terms of tabular data involving one or more look-up independent columns and one or more dependent variables (seeNXOpen.Fields.FieldVariable
) which depend on the look-up columns.To obtain a instance of this class use
NXOpen.Fields.FieldManager
.New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AnnTolerance | Returns or sets the approximate nearest neighbor (ANN) interpolation tolerance |
Color | Returns or sets the color of the object. |
Discontinuities | Returns a flag specifying if the table has discontinuites |
IndependentValueDivisor | Returns or sets the linear interpolation divisor for field independent value, the zero value represents no divisor used |
IndependentValueDivisorOption | Returns or sets a value indicating whether to set the linear interpolation divisor for field independent value |
IndependentValueShift | Returns or sets the linear interpolation shift for field independent value |
IndependentValueShiftOption | Returns or sets a value indicating whether to set the linear interpolation shift for field independent value |
InterpolationMethod | Returns or sets the interpolation method used when this table data is evaluated. |
IsBlanked | Returns the blank status of this object. |
IsLocked | Returns a value that indicates whether this field is locked against edits. |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsUserField | Returns a value that indicates whether this field is a user created/managed field. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
LinearLogOption | Returns or sets the linear/log option used when this table data is evaluated using the linear 1d interpolator. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PersistentInterpolator | Returns or sets a flag specifying if interpolator is persistent between session |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
ValuesOutsideTableInterpolation | Returns or sets the outside table values interpolation method for standard linear interpolation |
Methods¶
Method | Description |
---|---|
Blank | Blanks the object. |
CopyAsTableToPart | Create a new table field from this field (regardless of type). |
CopyToPart | Copy the field to the target part. |
CreateCopyInPart | Copy the field to the target part. |
CreateTableInPart | Create a new table field from this field (regardless of type). |
Delete | Delete this field; destroys the field and removes all references to it. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
EditFieldTable | Edit the table field. |
EditFieldTableComplexDisplay | Edit the table field complex display. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetData | Returns the values for the given NXOpen.Fields.FieldVariable in this NXOpen.Fields.FieldTable . |
GetDependentVariables | Returns the dependent variables for this NXOpen.Fields.Field @return dependent variables for this NXOpen.Fields.FieldVariable |
GetDescription | Returns the description of the field. |
GetFieldEvaluator | Returns a field evaluator which can be used to evaluate this field. |
GetIdLabel | Returns the ID/Label of the field. |
GetIdwOptions | Get the inverse distance weighting (IDW) interpolation options |
GetIndependentVariables | Returns the independent variables for this NXOpen.Fields.Field @return independent variables for this NXOpen.Fields.FieldVariable |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSpatialMap | Returns the spatial map for the formula field if one exists. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Highlight | Highlights the object. |
LoadFromFile | Populate the table from a file replacing or appending data |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveViewDependency | Remove dependency on all views from an object. |
Rename | Update the name of the field. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetDescription | Update the description of the field. |
SetIdLabel | Update the ID/Label of the field. |
SetIdwOptions | Set the inverse distance weighting (IDW) interpolation options |
SetInterpolation | Specified interpolation method, this method was deprecated in NX7. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetSpatialMap | Set the spatial map for the formula field. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
XYGraph | Creates displayed graphs of the Field’s specified independent variable versus all the Field’s dependent variables |
Enumerations¶
FieldTableInterpolationEnum Enumeration | Interpolation type This enumeration has been deprecated use NXOpen.Fields.FieldEvaluatorInterpolationEnum instead. |
FieldTableLoadFileOption Enumeration | Load file options |
Property Detail¶
AnnTolerance¶
-
FieldTable.
AnnTolerance
¶ Returns or sets the approximate nearest neighbor (ANN) interpolation tolerance
-------------------------------------
Getter Method
Signature
AnnTolerance()
Returns: approximate nearest neighbor (ANN) interpolation tolerance Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnnTolerance(annTolerance)
Parameters: annTolerance (float) – approximate nearest neighbor (ANN) interpolation tolerance New in version NX8.5.0.
License requirements: None.
Discontinuities¶
-
FieldTable.
Discontinuities
¶ Returns a flag specifying if the table has discontinuites
-------------------------------------
Getter Method
Signature
Discontinuities()
Returns: a flag specifying if the table has discontinuites Return type: bool New in version NX9.0.0.
License requirements: None.
IndependentValueDivisor¶
-
FieldTable.
IndependentValueDivisor
¶ Returns or sets the linear interpolation divisor for field independent value, the zero value represents no divisor used
-------------------------------------
Getter Method
Signature
IndependentValueDivisor()
Returns: the interpolation divisor for independent value Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IndependentValueDivisor(divisor)
Parameters: divisor (float) – the interpolation divisor for independent value New in version NX9.0.0.
License requirements: None.
IndependentValueDivisorOption¶
-
FieldTable.
IndependentValueDivisorOption
¶ Returns or sets a value indicating whether to set the linear interpolation divisor for field independent value
-------------------------------------
Getter Method
Signature
IndependentValueDivisorOption()
Returns: the interpolation divisor flag for independent value Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IndependentValueDivisorOption(divisorOption)
Parameters: divisorOption (bool) – the interpolation divisor flag for independent value New in version NX9.0.0.
License requirements: None.
IndependentValueShift¶
-
FieldTable.
IndependentValueShift
¶ Returns or sets the linear interpolation shift for field independent value
-------------------------------------
Getter Method
Signature
IndependentValueShift()
Returns: the interpolation shift for independent value Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IndependentValueShift(shift)
Parameters: shift (float) – the interpolation shift for independent value New in version NX9.0.0.
License requirements: None.
IndependentValueShiftOption¶
-
FieldTable.
IndependentValueShiftOption
¶ Returns or sets a value indicating whether to set the linear interpolation shift for field independent value
-------------------------------------
Getter Method
Signature
IndependentValueShiftOption()
Returns: the interpolation shift flag for independent value Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IndependentValueShiftOption(shiftOption)
Parameters: shiftOption (bool) – the interpolation shift flag for independent value New in version NX9.0.0.
License requirements: None.
InterpolationMethod¶
-
FieldTable.
InterpolationMethod
¶ Returns or sets the interpolation method used when this table data is evaluated.
-------------------------------------
Getter Method
Signature
InterpolationMethod()
Returns: the interpolation method Return type: NXOpen.Fields.FieldEvaluatorInterpolationEnum
New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
InterpolationMethod(interpolationMethod)
Parameters: interpolationMethod ( NXOpen.Fields.FieldEvaluatorInterpolationEnum
) – the interpolation methodNew in version NX7.5.2.
License requirements: None.
IsOccurrence¶
-
FieldTable.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
FieldTable.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
LinearLogOption¶
-
FieldTable.
LinearLogOption
¶ Returns or sets the linear/log option used when this table data is evaluated using the linear 1d interpolator.
-------------------------------------
Getter Method
Signature
LinearLogOption()
Returns: the log option Return type: NXOpen.Fields.FieldEvaluatorLinearLogOptionEnum
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinearLogOption(linearOption)
Parameters: linearOption ( NXOpen.Fields.FieldEvaluatorLinearLogOptionEnum
) – the log optionNew in version NX9.0.0.
License requirements: None.
Name¶
-
FieldTable.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
FieldTable.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
FieldTable.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
PersistentInterpolator¶
-
FieldTable.
PersistentInterpolator
¶ Returns or sets a flag specifying if interpolator is persistent between session
-------------------------------------
Getter Method
Signature
PersistentInterpolator()
Returns: persistent interpolator indicator Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PersistentInterpolator(persistentInterpolator)
Parameters: persistentInterpolator (bool) – persistent interpolator indicator New in version NX8.5.0.
License requirements: None.
Prototype¶
-
FieldTable.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
ValuesOutsideTableInterpolation¶
-
FieldTable.
ValuesOutsideTableInterpolation
¶ Returns or sets the outside table values interpolation method for standard linear interpolation
-------------------------------------
Getter Method
Signature
ValuesOutsideTableInterpolation()
Returns: the outside table values interpolation method Return type: NXOpen.Fields.FieldEvaluatorValuesOutsideTableInterpolationEnum
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValuesOutsideTableInterpolation(interpolationMethod)
Parameters: interpolationMethod ( NXOpen.Fields.FieldEvaluatorValuesOutsideTableInterpolationEnum
) – the outside table values interpolation methodNew in version NX9.0.0.
License requirements: None.
Method Detail¶
EditFieldTable¶
-
FieldTable.
EditFieldTable
¶ Edit the table field.
Specifies the new array of :py:class:`NXOpen.Fields.FieldVariable`s for independent and dependent variables, as well as the new double values.
Signature
EditFieldTable(indepVarArray, depVarArray, datapoints)
Parameters: - indepVarArray (list of
NXOpen.Fields.FieldVariable
) – independent variables to be associated with the field - depVarArray (list of
NXOpen.Fields.FieldVariable
) – dependent expression fields to be associated with the formula field - datapoints (list of float) – row based array of double values representing the table; then number of points should equal the number of independent variables * the number of dependent variables * the number of rows.
New in version NX6.0.0.
License requirements: None.
- indepVarArray (list of
EditFieldTableComplexDisplay¶
-
FieldTable.
EditFieldTableComplexDisplay
¶ Edit the table field complex display.
Specifies the new array of complex display flags for independent and dependent variables.
Signature
EditFieldTableComplexDisplay(indepVarArrayComplexDisplay, depVarArrayComplexDisplay)
Parameters: - indepVarArrayComplexDisplay (list of bool) – independent variable complex display flags to be associated with the field
- depVarArrayComplexDisplay (list of bool) – dependent variable complex display flags to be associated with the field
New in version NX10.0.0.
License requirements: None.
FindObject¶
-
FieldTable.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetData¶
-
FieldTable.
GetData
¶ Returns the values for the given
NXOpen.Fields.FieldVariable
in thisNXOpen.Fields.FieldTable
.The input
NXOpen.Fields.FieldVariable
should be retrieved from the field usingNXOpen.Fields.Field.GetIndependentVariables
orNXOpen.Fields.Field.GetDependentVariables
. The values are in the sameNXOpen.Unit
as specified on theNXOpen.Fields.FieldVariable
.Signature
GetData(variable)
Parameters: variable ( NXOpen.Fields.FieldVariable
) – variable whose table values are to be returnedReturns: the row values for this variable Return type: list of float New in version NX7.5.4.
License requirements: None.
GetIdwOptions¶
-
FieldTable.
GetIdwOptions
¶ Get the inverse distance weighting (IDW) interpolation options
Signature
GetIdwOptions()
Returns: a tuple Return type: A tuple consisting of (nearestOption, nearestFraction). nearestOption is a NXOpen.Fields.FieldEvaluatorInverseDistanceWeightingEnum
. nearest option nearestFraction is a float. fractionNew in version NX8.5.0.
License requirements: None.
LoadFromFile¶
-
FieldTable.
LoadFromFile
¶ Populate the table from a file replacing or appending data
Signature
LoadFromFile(filename, loadFileOption)
Parameters: - filename (str) – file to read rows from NOTE: The full Unicode character set is not supported for this parameter.
- loadFileOption (
NXOpen.Fields.FieldTableLoadFileOption
) – append or replace
New in version NX6.0.1.
License requirements: None.
Print¶
-
FieldTable.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetIdwOptions¶
-
FieldTable.
SetIdwOptions
¶ Set the inverse distance weighting (IDW) interpolation options
Signature
SetIdwOptions(nearestOption, nearestFraction)
Parameters: - nearestOption (
NXOpen.Fields.FieldEvaluatorInverseDistanceWeightingEnum
) – nearest option - nearestFraction (float) – fraction
New in version NX8.5.0.
License requirements: None.
- nearestOption (
SetInterpolation¶
-
FieldTable.
SetInterpolation
¶ Specified interpolation method, this method was deprecated in NX7.
5.2.
Signature
SetInterpolation(interpolationMethod)
Parameters: interpolationMethod (int) – specified interpolation method; NXOpen.Fields.FieldTable
interpolation enum values for builtin methods.New in version NX6.0.0.
Deprecated since version NX7.5.2: Use
NXOpen.Fields.FieldTable.InterpolationMethod`
instead.License requirements: None.
SetName¶
-
FieldTable.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.