DisplayableObject Class¶
-
class
NXOpen.
DisplayableObject
¶ Bases:
NXOpen.NXObject
,NXOpen.IFitTo
Base class for all objects that are displayable.
This is an abstract class, and cannot be instantiated.
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color of the object. |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Blank | Blanks the object. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Highlight | Highlights the object. |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveViewDependency | Remove dependency on all views from an object. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Enumerations¶
DisplayableObjectObjectFont Enumeration | specifies the object font for objects such as lines |
DisplayableObjectObjectWidth Enumeration | specifies object width for objects such as lines and text |
Property Detail¶
Color¶
-
DisplayableObject.
Color
¶ Returns or sets the color of the object.
After setting the color, you must call
RedisplayObject
in order for the change to take effect. There is a more efficient way to change the color, layer, line font or line width of a object. First callNXOpen.DisplayManager.NewDisplayModification
and then call any combination of set methods for the propertiesNXOpen.DisplayModification.NewColor`
,NXOpen.DisplayModification.NewWidth`
,NXOpen.DisplayModification.NewFont`
andNXOpen.DisplayModification.NewLayer`
. Finally callNXOpen.DisplayModification.Apply
andTransientObject.Dispose
. This eliminates the need to callRedisplayObject
.NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
Color()
Returns: Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Color(color)
Parameters: color (int) – New in version NX4.0.0.
License requirements: None.
IsBlanked¶
-
DisplayableObject.
IsBlanked
¶ Returns the blank status of this object.
-------------------------------------
Getter Method
Signature
IsBlanked()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
IsOccurrence¶
-
DisplayableObject.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
DisplayableObject.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Layer¶
-
DisplayableObject.
Layer
¶ Returns or sets the layer that the object is in.
After setting the layer, you must call
RedisplayObject
in order for the change to take effect, except see the comments forNXOpen.DisplayableObject.Color`
.NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
Layer()
Returns: Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Layer(layer)
Parameters: layer (int) – New in version NX4.0.0.
License requirements: None.
LineFont¶
-
DisplayableObject.
LineFont
¶ Returns or sets the line font of the object.
After setting the line font, you must call
RedisplayObject
in order for the change to take effect, except see the comments forNXOpen.DisplayableObject.Color`
.NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
LineFont()
Returns: Return type: NXOpen.DisplayableObjectObjectFont
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineFont(font)
Parameters: font ( NXOpen.DisplayableObjectObjectFont
) –New in version NX4.0.0.
License requirements: None.
LineWidth¶
-
DisplayableObject.
LineWidth
¶ Returns or sets the line width of the object.
After setting the line width, you must call
RedisplayObject
in order for the change to take effect, except see the comments forNXOpen.DisplayableObject.Color`
.NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
LineWidth()
Returns: Return type: NXOpen.DisplayableObjectObjectWidth
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineWidth(width)
Parameters: width ( NXOpen.DisplayableObjectObjectWidth
) –New in version NX4.0.0.
License requirements: None.
Name¶
-
DisplayableObject.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
NameLocation¶
-
DisplayableObject.
NameLocation
¶ Returns the location of the object’s name.
-------------------------------------
Getter Method
Signature
NameLocation()
Returns: Return type: NXOpen.Point3d
New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
DisplayableObject.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
DisplayableObject.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
DisplayableObject.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
Blank¶
-
DisplayableObject.
Blank
¶ Blanks the object.
Signature
Blank()
New in version NX3.0.0.
License requirements: None.
FindObject¶
-
DisplayableObject.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Highlight¶
-
DisplayableObject.
Highlight
¶ Highlights the object.
Signature
Highlight()
New in version NX3.0.0.
License requirements: None.
Print¶
-
DisplayableObject.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RedisplayObject¶
-
DisplayableObject.
RedisplayObject
¶ Redisplays the object in all views.
Typically this is used to display an object after its creation.
Signature
RedisplayObject()
New in version NX4.0.0.
License requirements: None.
RemoveViewDependency¶
-
DisplayableObject.
RemoveViewDependency
¶ Remove dependency on all views from an object.
Signature
RemoveViewDependency()
New in version NX10.0.0.
License requirements: None.
SetName¶
-
DisplayableObject.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetNameLocation¶
-
DisplayableObject.
SetNameLocation
¶ Sets the location of the object’s name.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetNameLocation(location)
Parameters: location ( NXOpen.Point3d
) –New in version NX3.0.0.
License requirements: None.