DisplayModification Class¶
-
class
NXOpen.
DisplayModification
¶ Bases:
NXOpen.TransientObject
Represents changes to the display characteristics of an object
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
ApplyToAllFaces | Returns or sets the apply to all faces flag. |
ApplyToOwningParts | Returns or sets the flag to apply display changes to Owning Parts. |
FaceAnalysisMode | Returns or sets the face analysis mode flag. |
KnotDisplayState | Returns or sets the flag for knot display. |
NewColor | Returns or sets a new color for objects which will be modified. |
NewFont | Returns or sets a new font (line style) for objects which will be modified |
NewLayer | Returns or sets a new layer for objects which will be modified. |
NewTranslucency | Returns or sets a new translucency value for objects which will be modified. |
NewWidth | Returns or sets a new line width for objects which will be modified |
PartiallyShaded | Returns or sets the partial shading flag. |
PoleDisplayState | Returns or sets the flag for pole display. |
Methods¶
Method | Description |
---|---|
Apply | Apply this display modification to a set of objects |
Dispose | Free resources associated with the instance. |
GetNewGrid | Get grid count for objects which will be modified. |
SetNewGrid | Set a new grid count for objects which will be modified. |
Property Detail¶
ApplyToAllFaces¶
-
DisplayModification.
ApplyToAllFaces
¶ Returns or sets the apply to all faces flag.
Specifies whether the modification should apply to all faces of any bodies to which this is applied.
-------------------------------------
Getter Method
Signature
ApplyToAllFaces()
Returns: true to apply the modification to all faces Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApplyToAllFaces(apply)
Parameters: apply (bool) – true to apply the modification to all faces New in version NX3.0.0.
License requirements: None.
ApplyToOwningParts¶
-
DisplayModification.
ApplyToOwningParts
¶ Returns or sets the flag to apply display changes to Owning Parts.
Specifies whether the display modifications should apply to the owning parts of the selected objects.
-------------------------------------
Getter Method
Signature
ApplyToOwningParts()
Returns: true to apply the display property changes to the owning parts Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApplyToOwningParts(apply)
Parameters: apply (bool) – true to apply the display property changes to the owning parts New in version NX7.5.0.
License requirements: None.
FaceAnalysisMode¶
-
DisplayModification.
FaceAnalysisMode
¶ Returns or sets the face analysis mode flag.
Only applies to faces.
-------------------------------------
Getter Method
Signature
FaceAnalysisMode()
Returns: true to enable face analysis mode Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceAnalysisMode(on)
Parameters: on (bool) – true to enable face analysis mode New in version NX3.0.0.
License requirements: None.
KnotDisplayState¶
-
DisplayModification.
KnotDisplayState
¶ Returns or sets the flag for knot display.
Only applies to b-spline.
-------------------------------------
Getter Method
Signature
KnotDisplayState()
Returns: true to enable knot display Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KnotDisplayState(on)
Parameters: on (bool) – true to enable knot display New in version NX5.0.0.
License requirements: None.
NewColor¶
-
DisplayModification.
NewColor
¶ Returns or sets a new color for objects which will be modified.
This is in the range from 1 to 216.
To convert an RGB value to an NX color index, use UF_DISP_ask_closest_color. To convert a color name to an NX color index, use UF_DISP_ask_closest_color_in_displayed_part or UF_DISP_ask_closest_color_in_part. For unmanaged C++, use these functions directly. Otherwise, use the corresponding wrapper methods of class NXOpen.UF.UFDisp.
-------------------------------------
Getter Method
Signature
NewColor()
Returns: new color value in the range 1-216 Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewColor(newColor)
Parameters: newColor (int) – new color value New in version NX3.0.0.
License requirements: None.
NewFont¶
-
DisplayModification.
NewFont
¶ Returns or sets a new font (line style) for objects which will be modified
-------------------------------------
Getter Method
Signature
NewFont()
Returns: new font Return type: NXOpen.DisplayableObjectObjectFont
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewFont(newFont)
Parameters: newFont ( NXOpen.DisplayableObjectObjectFont
) – new fontNew in version NX3.0.0.
License requirements: None.
NewLayer¶
-
DisplayModification.
NewLayer
¶ Returns or sets a new layer for objects which will be modified.
-------------------------------------
Getter Method
Signature
NewLayer()
Returns: new layer, must be a valid layer number Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewLayer(layer)
Parameters: layer (int) – new layer, must be a valid layer number New in version NX3.0.0.
License requirements: None.
NewTranslucency¶
-
DisplayModification.
NewTranslucency
¶ Returns or sets a new translucency value for objects which will be modified.
Only applies to faces.
-------------------------------------
Getter Method
Signature
NewTranslucency()
Returns: new translucency value in the range 0 to 100 Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewTranslucency(translucency)
Parameters: translucency (int) – new translucency value in the range 0 to 100 New in version NX3.0.0.
License requirements: None.
NewWidth¶
-
DisplayModification.
NewWidth
¶ Returns or sets a new line width for objects which will be modified
-------------------------------------
Getter Method
Signature
NewWidth()
Returns: new line width Return type: NXOpen.DisplayableObjectObjectWidth
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewWidth(newWidth)
Parameters: newWidth ( NXOpen.DisplayableObjectObjectWidth
) – new line widthNew in version NX3.0.0.
License requirements: None.
PartiallyShaded¶
-
DisplayModification.
PartiallyShaded
¶ Returns or sets the partial shading flag.
Only applies to faces.
-------------------------------------
Getter Method
Signature
PartiallyShaded()
Returns: true for partial shading on Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartiallyShaded(on)
Parameters: on (bool) – true for partial shading on New in version NX3.0.0.
License requirements: None.
PoleDisplayState¶
-
DisplayModification.
PoleDisplayState
¶ Returns or sets the flag for pole display.
Only applies to b-spline.
-------------------------------------
Getter Method
Signature
PoleDisplayState()
Returns: true to enable pole display Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PoleDisplayState(on)
Parameters: on (bool) – true to enable pole display New in version NX5.0.0.
License requirements: None.
Method Detail¶
Apply¶
-
DisplayModification.
Apply
¶ Apply this display modification to a set of objects
Signature
Apply(objects)
Parameters: objects (list of NXOpen.DisplayableObject
) – objects to be modifiedNew in version NX3.0.0.
License requirements: None.
Dispose¶
-
DisplayModification.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetNewGrid¶
-
DisplayModification.
GetNewGrid
¶ Get grid count for objects which will be modified.
Only applies to faces.
Signature
GetNewGrid()
Returns: a tuple Return type: A tuple consisting of (uGrid, vGrid). uGrid is a int. number of grid lines in the u direction vGrid is a int. number of grid lines in the v direction New in version NX3.0.0.
License requirements: None.
SetNewGrid¶
-
DisplayModification.
SetNewGrid
¶ Set a new grid count for objects which will be modified.
Signature
SetNewGrid(uGrid, vGrid)
Parameters: - uGrid (int) – number of grid lines in the u direction
- vGrid (int) – number of grid lines in the v direction
New in version NX3.0.0.
License requirements: None.