Post Class¶
-
class
NXOpen.CAE.
Post
¶ Bases:
object
Represents Post-Processing
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CompareDisplayFiles | Utility to compare post ascii files @return |
CreateAnnotation | Creates min/max annotation object @return |
CreateCrossSectionViewForResult | Create a new cross-section view with specified result on a loaded result id. |
CreateHistoryGraph | Create a graph by extracting data from the input postview id, at the input node label or point, for the input iterations. |
CreatePathFromElemIds | Create a path from an ordered set of element ids on the input postview id. |
CreatePathFromNodeIds | Create a path from an ordered set of node ids on the input postview id. |
CreatePathFromPoints | Create a path from an ordered set of points on the input postview id. |
CreatePostview | Create a new post view with default settings on a loaded result id. |
CreatePostviewForResult | Create a new post view with specified result on a loaded result id. |
CreatePostviewsForResultAndSE | Create a new post view with specified result on a loaded result id. |
CreateSpatialGraph | Create a graph by extracting data from the input postview id, along an input path id The input postview id is what was returned from CreatePostview or CreatePostviewForResult. |
CreateStreamlineSeedSet | Create a seed set that can be used to specify the start points for streamline extraction. |
CreateUserGroupFromEntityLabels | Create a User Group using element or node labels. |
CrossSectionViewSetLockRotation | Orients and disables all rotations in the input postview id. |
CrossSectionViewSetResult | Set the result for color display in the input cross-section view id. |
DeleteAllTemplates | Delete all loaded template xml files |
DeleteViewport | End all post processing activity in the input view port index |
Deletegraphs | Deletes NXOpen.CAE.PostGraph objects |
GetAnnotations | Gets all NXOpen.CAE.PostAnnotation in this post view |
GetPostviewIds | Returns the list of current Postview Ids @return the list of current Postview Ids |
GetResultForPostview | Returns the NXOpen.CAE.Result and a copy of the NXOpen.CAE.ResultParameters which define the input postview ID. |
GraphDelete | Delete the input graph specfied by graph_ids. |
LoadImportedResult | Load an existing result file that is not associated with a solution. |
LoadRaEventResult | Load results for a Response analysis event. |
LoadSolutionResult | Load results for a solution. |
LoadTemplate | Loads a template xml files from user specified location @return |
PathDelete | Delete the input path id. |
PlotGraph | Plot or Overlay the input graph specfied by graph_ids. |
Plotgraphs | Plot or overlay NXOpen.CAE.PostGraph objects as XY plot @return NXOpen.CAE.Xyplot.Plot object |
PostviewAnimationControl | Control animation for the input postview id The input postview id is what was returned from CreatePostview or CreatePostviewForResult This interface works only in interactive mode. |
PostviewAnimationControlStreamline | Control streamline animation for the input postview id The input postview id is what was returned from CreatePostview or CreatePostviewForResult. |
PostviewAnimationPlay | Play or Replay the animation for the input postview id with the input animation parameters. |
PostviewApplyCsysContainerVisibility | Set the visibility of a coordinate system container in the input postview id with immediate effect. |
PostviewApplyCsysVisibility | Set the visibility of a coordinate system (id) in the input postview id with immediate effect. |
PostviewApplyGroupContainerVisibility | Set the visibility of an element group container in the input postview id with immediate effect. |
PostviewApplyGroupVisibility | Set the visibility of an element group (index) within a container (1D, 2D, Connector etc) in the input postview id with immediate effect. |
PostviewApplyShowAll | Perform a Show All on the input postview id. |
PostviewApplyTemplate | Apply a loaded template on the input postview id. |
PostviewApplyTemplateFile | Apply a template file on the input postview id. |
PostviewApplyUserGroupVisibility | Control visibility of one or more usergroups with immediate effect. |
PostviewCaptureAnimatedGif | Capture an animated gif image for an input postview id is that is already animating. |
PostviewCreateClone | Creates a clone of a given postview. |
PostviewDelete | Delete a postview The input postview id is what was returned from CreatePostview, CreatePostviewForResult, or CreateCrossSectionViewForResult |
PostviewExportDisplay | Export the display of the input postview id to the specified format. |
PostviewExportTemplate | Save all the setting of the input postview id to a template xml file. |
PostviewMarkerOnOff | Set the min-max markers on-off for the input postview id. |
PostviewRename | Rename a postview. |
PostviewSaveTemplate | Save all the setting of the input postview id to a template xml file, capture image, and load template for future use. |
PostviewSetAnnotationBox | Set min-max marker box options in the input postview id. |
PostviewSetAxisymmetric | Set cutting-plane options in the input postview id. |
PostviewSetClipping | Set clipping options in the input postview id. |
PostviewSetColorDisplayDeformationSynchronization | Set synchronization of the color and deformed display in the input postview id. |
PostviewSetColorbar | Set colorbar options in the input postview id. |
PostviewSetCompression | Set compression option in the input postview id. |
PostviewSetCriticalLayerIdDisplay | Activate or deactivate the laminate layer ply id label display for a given post view. |
PostviewSetCriticalLoadIdDisplay | Activate or deactivate the laminate critical loadcase id label display for a given post view. |
PostviewSetCriticalPlyIdDisplay | Activate or deactivate the laminate critical ply id label display for a given post view. |
PostviewSetCurrentInOverlay | Set the input postview id as the current postview if it is one of several overlaid postviews The input postview id is what was returned from CreatePostview or CreatePostviewForResult |
PostviewSetDeformation | Set the result for deformed shape in the input postview id. |
PostviewSetDeformed | Set the primary display to be deformed/undeformed in the input postview id. |
PostviewSetDeformedUndeformedSynchronization | Set the primary display to be deformed/undeformed in the input postview id. |
PostviewSetEdgeFace | Set edge and face styles and colors for both primary and undeformed displays in the input postview id. |
PostviewSetFontSize | Set font size options in the input postview id. |
PostviewSetFormat | Set text formating used for legend and identify in the input postview id. |
PostviewSetGroupContainerVisibility | Set the visibility of an element group container in the input postview id. |
PostviewSetGroupVisibility | Set the visibility of an element group (index) within a container (1D, 2D, Connector etc) in the input postview id. |
PostviewSetHeaderlines | Set headerlines in the input postview id. |
PostviewSetLegend | Set legend options in the input postview id. |
PostviewSetLighting | Set lighted option in the input postview id. |
PostviewSetMark | Set the mark display options in the input postview id. |
PostviewSetMarker | Set min-max marker options in the input postview id. |
PostviewSetPosition | Set legend positioning in the input postview id. |
PostviewSetResult | Set the result for color display in the input postview id. |
PostviewSetResultWithProbe | Set the result for color display in the input for postview which is created with a probe NXOpen.CAE.Post.CreatePostview . |
PostviewSetShowHeader | Set show header option in the input postview id. |
PostviewSetStreamline | Set the streamline display options in the input postview id. |
PostviewSetStreamlineSeedSet | Set the seed set to use for streamline extraction in the input postview id. |
PostviewSetStreamlineVelocity | Set the velocity field for streamline extraction in the input postview id. |
PostviewSetStyle | Set the fringe style in the input postview id. |
PostviewSetTarget | Set the target operator in the input postview id. |
PostviewSetText | Set text color used for legend and identify in the input postview id. |
PostviewSetUndeformed | Set the undeformed display in the input postview id. |
PostviewUpdate | Make the input postview id up-to-date with all the settings made via PostviewSet* methods so far. |
ReloadTemplates | Search and load template xml files |
SetFactoryDefaultTemplate | Use factory defaults rather than a template for the default postview settings to be used in all subsequent PostviewCreate calls |
StreamlineSeedSetDelete | Delete a Seed Set. |
TemplateDelete | Delete a loaded template xml file specified by template_id. |
TemplateRename | Rename a loaded template xml file specified by template_id. |
TemplateSearch | Search for a template handle for loaded template xml file specified by its name. |
TemplateSetAsDefault | Set a loaded template as the default postview settings to be used for all subsequent PostviewCreate calls. |
UnloadResult | Unload the input result id. |
UnloadResultFile | Unload results that use the input file name |
UpdateUserGroupsFromSimPart | Synchronize the Groups in Post-Processing with those in the Simulation Part |
UserGroupDelete | Rename a User Group. |
UserGroupRename | Delete a User Group. |
Enumerations¶
PostAbcissa Enumeration | Abcissa types for graph |
PostAnimationControl Enumeration | Animation controls |
PostAnimationIterationTypes Enumeration | Animation styles |
PostAnimationStyle Enumeration | Animation styles |
PostAnimationType Enumeration | Animation types |
PostAxisymetricAxis Enumeration | Axis about which axis symmetric model rotates to create 3D display |
PostClipPlane Enumeration | Cutting plane options |
PostClipSide Enumeration | Clip hither-yon-cutplaneonly options |
PostEdgeStyle Enumeration | Edge display styles |
PostExport Enumeration | Export types for postview display |
PostFaceStyle Enumeration | Face display styles |
PostFormat Enumeration | Colorbar format |
PostGroupVisibility Enumeration | Show hide options for user group visibiliy control |
PostIntegrationScheme Enumeration | Intergration schemes for streamline extraction |
PostLegend Enumeration | legend display options |
PostLimitDisplay Enumeration | Drawing methods for overflow and under flor values |
PostMarkColor Enumeration | Mark color options |
PostMarkHide Enumeration | Mark hide options |
PostMarkLocation Enumeration | Mark locations |
PostMarkMaximumSize Enumeration | Maximum mark size options |
PostMarkRenderStyle Enumeration | Mark render styles |
PostMarkSize Enumeration | Mark size options |
PostMarkTensorStyle Enumeration | Mark styles for tensors |
PostMarker Enumeration | Min-Max marker display options |
PostNoDataTreatment Enumeration | NoData treatments for extracted data at a graph point |
PostNodeValueSharingCriterion Enumeration | Criteria for value sharing of extracted data at a graph point |
PostPosition Enumeration | Colorbar position |
PostScale Enumeration | Colorbar scales |
PostShowHeader Enumeration | Show header display options |
PostSpectrum Enumeration | colorbar spectrums |
PostStreamlineColor Enumeration | Streamline color options |
PostStreamlineDirection Enumeration | Direction options for streamline extraction |
PostStreamlineLineWeight Enumeration | Streamline line weight options |
PostStreamlineSize Enumeration | Streamline size options |
PostStreamlineStyle Enumeration | Streamline display styles |
PostStreamlineSynchronization Enumeration | Synchronization options for streamlines |
PostStyle Enumeration | Fringe styles |
PostTarget Enumeration | Target operators |
PostThreshold Enumeration | colorbar thresholds |
PostValueSharingCriterion Enumeration | Criteria for value sharing for extracted stream line data |
Structs¶
PostASCIIDiffTolerances_Struct Struct | Tolerances used for comparing postview ASCII display files |
PostAnimation_Struct Struct | Animation settings |
PostAnimationStreamline_Struct Struct | Animation settings for streamline animation |
PostAnnotationBox_Struct Struct | Annotation box display settings |
PostAxisymmetric_Struct Struct | 3D Axi-symmetric model display settings |
PostClipping_Struct Struct | Cutting-plane display settings |
PostColorbar_Struct Struct | Colorbar settings |
PostEdgeFace_Struct Struct | Edge and Face display settings |
PostGraphIds_Struct Struct | Graph handle |
PostGraphParameters_Struct Struct | Graph extraction parameters |
PostHeaderlines_Struct Struct | Headerlines |
PostMark_Struct Struct | Mark display settings |
PostStreamline_Struct Struct | Streamline display settings |
PostStreamlineData_Struct Struct | Streamline data extraction parameters |
PostStreamlineExtraction_Struct Struct | Streamline extraction parameters |
PostStreamlineSeed_Struct Struct | Streamline seed point definition |
PostText_Struct Struct | Annotation text settings |
Method Detail¶
CompareDisplayFiles¶
-
Post.
CompareDisplayFiles
¶ Utility to compare post ascii files
Signature
CompareDisplayFiles(benchmarkFileName, testFileName, tolerances)
Parameters: - benchmarkFileName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- testFileName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- tolerances (
NXOpen.CAE.PostASCIIDiffTolerances_Struct
) –
Returns: Return type: str
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateAnnotation¶
-
Post.
CreateAnnotation
¶ Overloaded method CreateAnnotation
CreateAnnotation(postviewId, name, num, max, usertext)
CreateAnnotation(postviewId, name, entities, subEntities, usertext)
CreateAnnotation(postviewId, name, elements, nodes, elmedgeface, usertext)
CreateAnnotation(postviewId, name, xcoord, ycoord, usertext)
-------------------------------------
Creates min/max annotation object
Signature
CreateAnnotation(postviewId, name, num, max, usertext)
Parameters: - postviewId (int) –
- name (str) – Annotation name NOTE: The full Unicode character set is not supported for this parameter.
- num (int) – Number of minimum or maximum
- max (bool) – true means maximum, false is minimum
- usertext (list of str) – Additional text in each box
Returns: Return type: New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Creates entity annotation object
Signature
CreateAnnotation(postviewId, name, entities, subEntities, usertext)
Parameters: - postviewId (int) –
- name (str) – Annotation name NOTE: The full Unicode character set is not supported for this parameter.
- entities (list of int) – List of node or elements
- subEntities (list of int) – List of nodes for element-nodal result
- usertext (list of str) – Additional text in each box
Returns: Return type: New in version NX8.5.0.
Deprecated since version NX9.0.0: use
NXOpen.CAE.Post.JA_SPP_create_annotation
with extra face parameter.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Creates entity annotation object
Signature
CreateAnnotation(postviewId, name, elements, nodes, elmedgeface, usertext)
Parameters: - postviewId (int) –
- name (str) – Annotation name NOTE: The full Unicode character set is not supported for this parameter.
- elements (list of int) – List of node or elements
- nodes (list of int) – List of nodes
- elmedgeface (list of int) – List of super entity(face/edge) for node and elements pick
- usertext (list of str) – Additional text in each box
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Creates user location box annotation object
Signature
CreateAnnotation(postviewId, name, xcoord, ycoord, usertext)
Parameters: - postviewId (int) –
- name (str) – Annotation name NOTE: The full Unicode character set is not supported for this parameter.
- xcoord (float) – Parametric x screen coordinate, varies from 0 to 1
- ycoord (float) – Parametric y screen coordinate, varies from 0 to 1
- usertext (list of str) – Additional text in each box
Returns: Return type: New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
CreateCrossSectionViewForResult¶
-
Post.
CreateCrossSectionViewForResult
¶ Create a new cross-section view with specified result on a loaded result id.
Signature
CreateCrossSectionViewForResult(viewIndex, resultId, result)
Parameters: - viewIndex (int) – 0 thru 8, viewport number to place cross-section view in
- resultId (int) –
- result (
NXOpen.CAE.CrossSectionParameters
) –
Returns: Return type: int
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateHistoryGraph¶
-
Post.
CreateHistoryGraph
¶ Create a graph by extracting data from the input postview id, at the input node label or point, for the input iterations.
Iterations specified as start, end and step. The input postview id is what was returned from CreatePostview or CreatePostviewForResult. The input path id is what was returned from CreatePathFromNodeIds or CreatePathFromPoints. Returns a graph handle that may be used in PlotGraph and Graph* calls
Signature
CreateHistoryGraph(postviewId, name, graph, startIteration, endIteration, iterationIncrement, nodeLabel, point)
Parameters: - postviewId (int) –
- name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- graph (
NXOpen.CAE.PostGraphParameters_Struct
) – - startIteration (int) –
- endIteration (int) –
- iterationIncrement (int) –
- nodeLabel (int) –
- point (list of float) –
Returns: Return type: New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreatePathFromElemIds¶
-
Post.
CreatePathFromElemIds
¶ Create a path from an ordered set of element ids on the input postview id.
The input postview id is what was returned from CreatePostview or CreatePostviewForResult. Returns a path handle that maye be used in CreateSpatialGraph and Path* calls
Signature
CreatePathFromElemIds(postviewId, name, elemIds)
Parameters: - postviewId (int) –
- name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- elemIds (list of int) –
Returns: Return type: int
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreatePathFromNodeIds¶
-
Post.
CreatePathFromNodeIds
¶ Create a path from an ordered set of node ids on the input postview id.
The input postview id is what was returned from CreatePostview or CreatePostviewForResult. Returns a path handle that maye be used in CreateSpatialGraph and Path* calls
Signature
CreatePathFromNodeIds(postviewId, name, nodeIds)
Parameters: - postviewId (int) –
- name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- nodeIds (list of int) –
Returns: Return type: int
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreatePathFromPoints¶
-
Post.
CreatePathFromPoints
¶ Create a path from an ordered set of points on the input postview id.
The input postview id is what was returned from CreatePostview or CreatePostviewForResult. Returns a path handle that maye be used in CreateSpatialGraph and Path* calls
Signature
CreatePathFromPoints(postviewId, name, points, numberOfInsertPointsPerSegment)
Parameters: - postviewId (int) –
- name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- points (list of float) –
- numberOfInsertPointsPerSegment (int) – greater than or equal to 0
Returns: Return type: int
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreatePostview¶
-
Post.
CreatePostview
¶ Overloaded method CreatePostview
CreatePostview(viewIndex, resultId, overlay)
CreatePostview(viewIndex, result, overlay)
CreatePostview(viewIndex, probeparams, overlay)
-------------------------------------
Create a new post view with default settings on a loaded result id. The result id is what was obtained from LoadImportedResult or LoadSolutionResult. Returns a postview handle that may be used in Postview*, CreatePath* and CreateGraph* calls
Signature
CreatePostview(viewIndex, resultId, overlay)
Parameters: - viewIndex (int) – 0 thru 8, viewport number to place postview in
- resultId (int) –
- overlay (bool) –
Returns: Return type: int
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Create a new post view with default settings on a loaded result id. The result id is what was obtained from LoadImportedResult or LoadSolutionResult. Returns a postview handle that may be used in Postview*, CreatePath* and CreateGraph* calls
Signature
CreatePostview(viewIndex, result, overlay)
Parameters: - viewIndex (int) – 0 thru 8, viewport number to place postview in
- result (
NXOpen.CAE.Result
) – - overlay (bool) –
Returns: Return type: int
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Create a new post view for a given probe. If Probe is loadcase/iteration varying, it will create postview of first available loadcase iteration. User can set new loadcase, iteration and update postview using
NXOpen.CAE.Post.PostviewUpdate
Returns a postview handle that may be used in Postview*, CreatePath* and CreateGraph* callsSignature
CreatePostview(viewIndex, probeparams, overlay)
Parameters: - viewIndex (int) – 0 thru 8, viewport number to place postview in
- probeparams (
NXOpen.CAE.ResultParametersWithProbe
) – - overlay (bool) –
Returns: Return type: int
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
CreatePostviewForResult¶
-
Post.
CreatePostviewForResult
¶ Overloaded method CreatePostviewForResult
CreatePostviewForResult(viewIndex, resultId, overlay, result)
CreatePostviewForResult(viewIndex, result, overlay, resultParamter)
-------------------------------------
Create a new post view with specified result on a loaded result id. The result id is what was obtained from LoadImportedResult or LoadSolutionResult. Returns a postview handle that may be used in Postview*, CreatePath* and CreateGraph* calls
NXOpen.CAE.ResultResultParameters_Struct
has been replaced byNXOpen.CAE.ResultParameters
This method is replaced byNXOpen.CAE.Post.CreatePostviewForResult
Signature
CreatePostviewForResult(viewIndex, resultId, overlay, result)
Parameters: - viewIndex (int) – 0 thru 8, viewport number to place postview in
- resultId (int) –
- overlay (bool) –
- result (
NXOpen.CAE.ResultResultParameters_Struct
) –
Returns: Return type: int
New in version NX5.0.0.
Deprecated since version NX7.5.1: Use
NXOpen.CAE.Post.CreatePostviewForResult
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Create a new post view with specified result on a loaded result id. The result id is what was obtained from LoadImportedResult or LoadSolutionResult. Returns a postview handle that may be used in Postview*, CreatePath* and CreateGraph* calls
Signature
CreatePostviewForResult(viewIndex, result, overlay, resultParamter)
Parameters: - viewIndex (int) – 0 thru 8, viewport number to place postview in
- result (
NXOpen.CAE.Result
) – - overlay (bool) –
- resultParamter (
NXOpen.CAE.ResultParameters
) –
Returns: Return type: int
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
CreatePostviewsForResultAndSE¶
-
Post.
CreatePostviewsForResultAndSE
¶ Create a new post view with specified result on a loaded result id.
Also create overlays of any loaded super element results associated with the result id and set the color bar ranges to the viewport displayed. Set the deformation scale to Absolute with a scale factor of 1. The result id is what was obtained from LoadImportedResult or LoadSolutionResult. Returns an array of postview handles that may be used in Postview*, CreatePath* and CreateGraph* calls
Signature
CreatePostviewsForResultAndSE(viewIndex, result, resultParamter)
Parameters: - viewIndex (int) – 0 thru 8, viewport number to place postview in
- result (
NXOpen.CAE.Result
) – - resultParamter (
NXOpen.CAE.ResultParameters
) –
Returns: Return type: list of int
New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateSpatialGraph¶
-
Post.
CreateSpatialGraph
¶ Create a graph by extracting data from the input postview id, along an input path id The input postview id is what was returned from CreatePostview or CreatePostviewForResult.
The input path id is what was returned from CreatePathFromNodeIds or CreatePathFromPoints. Returns a graph handle that may be used in PlotGraph and Graph* calls
Signature
CreateSpatialGraph(postviewId, name, graph, pathId)
Parameters: - postviewId (int) –
- name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- graph (
NXOpen.CAE.PostGraphParameters_Struct
) – - pathId (int) –
Returns: Return type: New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateStreamlineSeedSet¶
-
Post.
CreateStreamlineSeedSet
¶ Create a seed set that can be used to specify the start points for streamline extraction.
The input postview id is what was returned from CreatePostview or CreatePostviewForResult. Returns a seedset handle that maye be used in StreamlineSeedSet* calls and PostVeiwSetStreamlineSeedSet
Signature
CreateStreamlineSeedSet(postviewId, name, seeds)
Parameters: - postviewId (int) –
- name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- seeds (list of
NXOpen.CAE.PostStreamlineSeed_Struct
) –
Returns: Return type: int
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateUserGroupFromEntityLabels¶
-
Post.
CreateUserGroupFromEntityLabels
¶ Create a User Group using element or node labels.
Returns a usergroup handle that may be used in UserGroup* calls and in PostViewApplyUserGroupVisibility
Signature
CreateUserGroupFromEntityLabels(postviewId, entityType, labels)
Parameters: - postviewId (int) –
- entityType (
NXOpen.CAE.CaeGroupCollectionEntityType
) – - labels (list of int) –
Returns: Return type: int
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CrossSectionViewSetLockRotation¶
-
Post.
CrossSectionViewSetLockRotation
¶ Orients and disables all rotations in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreateCrossSectionViewForResult
Signature
CrossSectionViewSetLockRotation(postviewId, lockRotation)
Parameters: - postviewId (int) –
- lockRotation (bool) –
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CrossSectionViewSetResult¶
-
Post.
CrossSectionViewSetResult
¶ Set the result for color display in the input cross-section view id.
Needs a CrossSectionViewUpdate call to take effect. The input cross-section view id is what was returned from CreateCrossSectionViewForResult
Signature
CrossSectionViewSetResult(postviewId, result)
Parameters: - postviewId (int) –
- result (
NXOpen.CAE.CrossSectionParameters
) –
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteAllTemplates¶
-
Post.
DeleteAllTemplates
¶ Delete all loaded template xml files
Signature
DeleteAllTemplates()
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteViewport¶
-
Post.
DeleteViewport
¶ End all post processing activity in the input view port index
Signature
DeleteViewport(viewIndex)
Parameters: viewIndex (int) – 0 thru 8, viewport number to remove post displays New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Deletegraphs¶
-
Post.
Deletegraphs
¶ Deletes
NXOpen.CAE.PostGraph
objectsSignature
Deletegraphs(graphs)
Parameters: graphs (list of NXOpen.CAE.PostGraph
) –NXOpen.CAE.PostGraph
object listNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetAnnotations¶
-
Post.
GetAnnotations
¶ Gets all
NXOpen.CAE.PostAnnotation
in this post viewSignature
GetAnnotations(postviewId)
Parameters: postviewId (int) – Returns: Return type: list of NXOpen.CAE.PostAnnotation
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetPostviewIds¶
-
Post.
GetPostviewIds
¶ Returns the list of current Postview Ids
Signature
GetPostviewIds()
Returns: the list of current Postview Ids Return type: list of int New in version NX8.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetResultForPostview¶
-
Post.
GetResultForPostview
¶ Returns the
NXOpen.CAE.Result
and a copy of theNXOpen.CAE.ResultParameters
which define the input postview ID.Signature
GetResultForPostview(postviewId)
Parameters: postviewId (int) – postview ID Returns: a tuple Return type: A tuple consisting of (result, resultParamter). result is a NXOpen.CAE.Result
.NXOpen.CAE.Result
which defines input postview resultParamter is aNXOpen.CAE.ResultParameters
. a copy of theNXOpen.CAE.ResultParameters
which defines input postview, It is user’s responsibility to destroy the result parameters object once done usingNXOpen.CAE.ResultManager.DeleteResultParameters
, in order to free up system resourcesNew in version NX8.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GraphDelete¶
-
Post.
GraphDelete
¶ Delete the input graph specfied by graph_ids.
The input graph_ids is what was returned from CreateSpatialGraph or CreateHistoryGraph
Signature
GraphDelete(graphIds)
Parameters: graphIds ( NXOpen.CAE.PostGraphIds_Struct
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
LoadImportedResult¶
-
Post.
LoadImportedResult
¶ Load an existing result file that is not associated with a solution.
Returns a result handle that may be used in PostviewCreate* calls
Signature
LoadImportedResult(resultName, fileName, units)
Parameters: - resultName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- fileName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- units (list of
NXOpen.Unit
) –
Returns: Return type: int
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
LoadRaEventResult¶
-
Post.
LoadRaEventResult
¶ Load results for a Response analysis event.
Returns a result handle that may be used in PostviewCreate* calls
Signature
LoadRaEventResult(raEvent)
Parameters: raEvent ( NXOpen.CAE.ResponseSimulation.RSEvent
) –Returns: Return type: int New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
LoadSolutionResult¶
-
Post.
LoadSolutionResult
¶ Load results for a solution.
Returns a result handle that may be used in PostviewCreate* calls
Signature
LoadSolutionResult(solution)
Parameters: solution ( NXOpen.CAE.SimSolution
) –Returns: Return type: int New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
LoadTemplate¶
-
Post.
LoadTemplate
¶ Loads a template xml files from user specified location
Signature
LoadTemplate(filename, name)
Parameters: - filename (str) – NOTE: The full Unicode character set is not supported for this parameter.
- name (str) – NOTE: The full Unicode character set is not supported for this parameter.
Returns: a tuple
Return type: A tuple consisting of (imagefilename, templateId). imagefilename is a str. templateId is a int.
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PathDelete¶
-
Post.
PathDelete
¶ Delete the input path id.
The input path id is what was returned from CreatePathFromNodeIds or CreatePathFromPoints
Signature
PathDelete(pathId)
Parameters: pathId (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PlotGraph¶
-
Post.
PlotGraph
¶ Plot or Overlay the input graph specfied by graph_ids.
The input graph_ids is what was returned from CreateSpatialGraph or CreateHistoryGraph
Signature
PlotGraph(viewIndex, graphIds, overlay)
Parameters: - viewIndex (int) –
- graphIds (
NXOpen.CAE.PostGraphIds_Struct
) – - overlay (bool) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Plotgraphs¶
-
Post.
Plotgraphs
¶ Plot or overlay
NXOpen.CAE.PostGraph
objects as XY plotSignature
Plotgraphs(windowIndex, viewIndex, graphs, overlay)
Parameters: - windowIndex (int) – Window Index will be -1 for plotting it in main nx window
- viewIndex (int) – View Index
- graphs (list of
NXOpen.CAE.PostGraph
) –NXOpen.CAE.PostGraph
object list - overlay (bool) – overlay option
Returns: NXOpen.CAE.Xyplot.Plot
objectReturn type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewAnimationControl¶
-
Post.
PostviewAnimationControl
¶ Control animation for the input postview id The input postview id is what was returned from CreatePostview or CreatePostviewForResult This interface works only in interactive mode.
Signature
PostviewAnimationControl(postviewId, control, frame, fullCycle, delay)
Parameters: - postviewId (int) –
- control (
NXOpen.CAE.PostAnimationControl
) – - frame (int) – frame number to use with control = SetFrame
- fullCycle (bool) – to be used with control = FullCycle
- delay (int) – milliseconds, to use with control = Delay
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewAnimationControlStreamline¶
-
Post.
PostviewAnimationControlStreamline
¶ Control streamline animation for the input postview id The input postview id is what was returned from CreatePostview or CreatePostviewForResult.
This interface works only in interactive mode.
Signature
PostviewAnimationControlStreamline(postviewId, control)
Parameters: - postviewId (int) –
- control (
NXOpen.CAE.PostAnimationStreamline_Struct
) –
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PostviewAnimationPlay¶
-
Post.
PostviewAnimationPlay
¶ Play or Replay the animation for the input postview id with the input animation parameters.
The input postview id is what was returned from CreatePostview or CreatePostviewForResult This interface works only in interactive mode.
Signature
PostviewAnimationPlay(postviewId, animation)
Parameters: - postviewId (int) –
- animation (
NXOpen.CAE.PostAnimation_Struct
) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewApplyCsysContainerVisibility¶
-
Post.
PostviewApplyCsysContainerVisibility
¶ Set the visibility of a coordinate system container in the input postview id with immediate effect.
The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewApplyCsysContainerVisibility(postviewId, visibility)
Parameters: - postviewId (int) –
- visibility (bool) –
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewApplyCsysVisibility¶
-
Post.
PostviewApplyCsysVisibility
¶ Set the visibility of a coordinate system (id) in the input postview id with immediate effect.
The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewApplyCsysVisibility(postviewId, id, visibility)
Parameters: - postviewId (int) –
- id (int) – coordinate system id
- visibility (bool) –
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewApplyGroupContainerVisibility¶
-
Post.
PostviewApplyGroupContainerVisibility
¶ Overloaded method PostviewApplyGroupContainerVisibility
PostviewApplyGroupContainerVisibility(postviewId, container, visibility)
PostviewApplyGroupContainerVisibility(postviewId, container, visibility)
-------------------------------------
Set the visibility of an element group container in the input postview id with immediate effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewApplyGroupContainerVisibility(postviewId, container, visibility)
Parameters: - postviewId (int) –
- container (
NXOpen.CAE.ResultGroupContainer
) – - visibility (bool) –
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Set the visibility of an element group container(s) in the input postview id with immediate effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewApplyGroupContainerVisibility(postviewId, container, visibility)
Parameters: - postviewId (int) –
- container (list of
NXOpen.CAE.ResultGroupContainer
) – - visibility (bool) –
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
PostviewApplyGroupVisibility¶
-
Post.
PostviewApplyGroupVisibility
¶ Overloaded method PostviewApplyGroupVisibility
PostviewApplyGroupVisibility(postviewId, container, group, visibility)
PostviewApplyGroupVisibility(postviewId, container, group, visibility)
-------------------------------------
Set the visibility of an element group (index) within a container (1D, 2D, Connector etc) in the input postview id with immediate effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewApplyGroupVisibility(postviewId, container, group, visibility)
Parameters: - postviewId (int) –
- container (
NXOpen.CAE.ResultGroupContainer
) – - group (int) – 0 thru number of groups in container - 1
- visibility (bool) –
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Set the visibility of an element group(s) (index) within a container (1D, 2D, Connector etc) in the input postview id with immediate effect. The container and group id array are associated 1 to 1 with each other. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewApplyGroupVisibility(postviewId, container, group, visibility)
Parameters: - postviewId (int) –
- container (list of
NXOpen.CAE.ResultGroupContainer
) – - group (list of int) –
- visibility (bool) –
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
PostviewApplyShowAll¶
-
Post.
PostviewApplyShowAll
¶ Perform a Show All on the input postview id.
The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewApplyShowAll(postviewId)
Parameters: postviewId (int) – New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewApplyTemplate¶
-
Post.
PostviewApplyTemplate
¶ Apply a loaded template on the input postview id.
The input postview id is what was returned from CreatePostview, CreatePostviewForResult, or CreateCrossSectionViewForResult
Signature
PostviewApplyTemplate(postviewId, templateId)
Parameters: - postviewId (int) –
- templateId (int) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewApplyTemplateFile¶
-
Post.
PostviewApplyTemplateFile
¶ Apply a template file on the input postview id.
The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewApplyTemplateFile(postviewId, xmlFileName)
Parameters: - postviewId (int) –
- xmlFileName (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewApplyUserGroupVisibility¶
-
Post.
PostviewApplyUserGroupVisibility
¶ Control visibility of one or more usergroups with immediate effect.
The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewApplyUserGroupVisibility(postviewId, usergroupIds, visibility)
Parameters: - postviewId (int) –
- usergroupIds (list of int) –
- visibility (
NXOpen.CAE.PostGroupVisibility
) –
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PostviewCaptureAnimatedGif¶
-
Post.
PostviewCaptureAnimatedGif
¶ Capture an animated gif image for an input postview id is that is already animating.
The input postview id is what was returned from CreatePostview or CreatePostviewForResult This interface works only in interactive mode.
Signature
PostviewCaptureAnimatedGif(postviewId, fileName, includeOverlayedPostviews, whiteBackground)
Parameters: - postviewId (int) –
- fileName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- includeOverlayedPostviews (bool) –
- whiteBackground (bool) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewCreateClone¶
-
Post.
PostviewCreateClone
¶ Creates a clone of a given postview.
The clone postview has to be created in a different viewport than the source postview
Signature
PostviewCreateClone(postviewId, viewIndex)
Parameters: - postviewId (int) –
- viewIndex (int) –
Returns: Return type: int
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewDelete¶
-
Post.
PostviewDelete
¶ Delete a postview The input postview id is what was returned from CreatePostview, CreatePostviewForResult, or CreateCrossSectionViewForResult
Signature
PostviewDelete(postviewId)
Parameters: postviewId (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewExportDisplay¶
-
Post.
PostviewExportDisplay
¶ Export the display of the input postview id to the specified format.
VRML is not yet supported. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewExportDisplay(postviewId, fileName, format, ignoreClipping, ignoreVisibility)
Parameters: - postviewId (int) –
- fileName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- format (
NXOpen.CAE.PostExport
) – - ignoreClipping (bool) –
- ignoreVisibility (bool) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewExportTemplate¶
-
Post.
PostviewExportTemplate
¶ Save all the setting of the input postview id to a template xml file.
no image capture. xml file is not loaded, and can be reused only via PostviewApplyTemplateFile The input postview id is what was returned from CreatePostview, CreatePostviewForResult, or CreateCrossSectionViewForResult
Signature
PostviewExportTemplate(postviewId, xmlFileName)
Parameters: - postviewId (int) –
- xmlFileName (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewMarkerOnOff¶
-
Post.
PostviewMarkerOnOff
¶ Set the min-max markers on-off for the input postview id.
The input postview id is what was returned from CreatePostview, CreatePostviewForResult, or CreateCrossSectionViewForResult
Signature
PostviewMarkerOnOff(postviewId, showMarker)
Parameters: - postviewId (int) –
- showMarker (bool) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewRename¶
-
Post.
PostviewRename
¶ Rename a postview.
The input postview id is what was returned from CreatePostview, CreatePostviewForResult, or CreateCrossSectionViewForResult
Signature
PostviewRename(postviewId, newName)
Parameters: - postviewId (int) –
- newName (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSaveTemplate¶
-
Post.
PostviewSaveTemplate
¶ Save all the setting of the input postview id to a template xml file, capture image, and load template for future use.
The input postview id is what was returned from CreatePostview, CreatePostviewForResult, or CreateCrossSectionViewForResult. Returns a template handle that may be used in PostviewApplyTemplate and Template* calls
Signature
PostviewSaveTemplate(postviewId)
Parameters: postviewId (int) – Returns: Return type: int New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetAnnotationBox¶
-
Post.
PostviewSetAnnotationBox
¶ Set min-max marker box options in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview, CreatePostviewForResult, or CreateCrossSectionViewForResult
Signature
PostviewSetAnnotationBox(postviewId, annotationBox)
Parameters: - postviewId (int) –
- annotationBox (
NXOpen.CAE.PostAnnotationBox_Struct
) –
New in version NX5.0.0.
Deprecated since version NX9.0.0: Set
NXOpen.CAE.PostAnnotation
Display Attribute directly instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetAxisymmetric¶
-
Post.
PostviewSetAxisymmetric
¶ Set cutting-plane options in the input postview id.
Needs a PostviewUpdate call to take effect. In addition, needs to have
NXOpen.CAE.PostTarget
set toNXOpen.CAE.PostTarget.AxisSymmetry3D
The input postview id is what was returned from CreatePostview or CreatePostviewForResultSignature
PostviewSetAxisymmetric(postviewId, axisymmetric)
Parameters: - postviewId (int) –
- axisymmetric (
NXOpen.CAE.PostAxisymmetric_Struct
) –
New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetClipping¶
-
Post.
PostviewSetClipping
¶ Overloaded method PostviewSetClipping
PostviewSetClipping(postviewId, clipping)
PostviewSetClipping(postviewId, clipping)
-------------------------------------
Set clipping options in the input postview id. Needs a PostviewUpdate call to take effect. In addition, needs to have the
NXOpen.CAE.PostTarget
set toNXOpen.CAE.PostTarget.CuttingPlane
for the model to appear clipped.NXOpen.CAE.PostClipping_Struct
has been replaced byNXOpen.CAE.ClippingParameters
The input postview id is what was returned from CreatePostview or CreatePostviewForResultSignature
PostviewSetClipping(postviewId, clipping)
Parameters: - postviewId (int) –
- clipping (
NXOpen.CAE.PostClipping_Struct
) –
New in version NX5.0.0.
Deprecated since version NX7.5.1: Use
NXOpen.CAE.Post.PostviewSetClipping
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Set cutting-plane options in the input postview id. Needs a PostviewUpdate call to take effect. In addition, needs to have the Target set to CuttingPlane for the model to appear clipped. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetClipping(postviewId, clipping)
Parameters: - postviewId (int) –
- clipping (
NXOpen.CAE.ClippingParameters
) –
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
PostviewSetColorDisplayDeformationSynchronization¶
-
Post.
PostviewSetColorDisplayDeformationSynchronization
¶ Set synchronization of the color and deformed display in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetColorDisplayDeformationSynchronization(postviewId, synchronization)
Parameters: - postviewId (int) –
- synchronization (bool) –
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetColorbar¶
-
Post.
PostviewSetColorbar
¶ Overloaded method PostviewSetColorbar
PostviewSetColorbar(postviewId, colorbar)
PostviewSetColorbar(postviewId, colorbar, customOverwrite, rangeValue, rangeColors)
-------------------------------------
Set colorbar options in the input postview id. Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview, CreatePostviewForResult, or CreateCrossSectionViewForResult
Signature
PostviewSetColorbar(postviewId, colorbar)
Parameters: - postviewId (int) –
- colorbar (
NXOpen.CAE.PostColorbar_Struct
) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Set color bar options along with custom overwrite options in the input postview id.
Signature
PostviewSetColorbar(postviewId, colorbar, customOverwrite, rangeValue, rangeColors)
Parameters: - postviewId (int) – Post view id.
- colorbar (
NXOpen.CAE.PostColorbar_Struct
) – Color bar. - customOverwrite (bool) –
- rangeValue (list of float) – Range values.
- rangeColors (list of
NXOpen.NXColorRgb_Struct
) – Range colors.
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
PostviewSetCompression¶
-
Post.
PostviewSetCompression
¶ Set compression option in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetCompression(postviewId, compress, featureangle, banddifference)
Parameters: - postviewId (int) –
- compress (bool) – true - This option will compress the memory needed for displaying the model.Option will draw the model as one connected set. false - This option will draw the each element as separatly to improve the quality of the display
- featureangle (float) – Angle is used to determine if the element edge is feature edge or not. If angle between the elements under consideration is more than the given angle then separete element normal are used for drawing the faces
- banddifference (float) – Value is used check edge vertices result values comparision in case element-nodal and elemental display. If the value of the vertices are in same band then the differnce between those values should less than differnce of the banddifference mentioned. If the difference is more than this value then those will be considered as difference vertices
New in version NX8.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetCriticalLayerIdDisplay¶
-
Post.
PostviewSetCriticalLayerIdDisplay
¶ Activate or deactivate the laminate layer ply id label display for a given post view.
The critical layer id display is only supported for
NXOpen.CAE.LaminateGraphicalReport
results, for specific datasets.Signature
PostviewSetCriticalLayerIdDisplay(postviewId, displayCriticalLayers)
Parameters: - postviewId (int) – Id of the post view on which the display is to be (de)activated
- displayCriticalLayers (bool) – If true, the critical layer ids will be displayed on elements
New in version NX9.0.2.
License requirements: nx_lam_composites (“Laminate Composites”)
PostviewSetCriticalLoadIdDisplay¶
-
Post.
PostviewSetCriticalLoadIdDisplay
¶ Activate or deactivate the laminate critical loadcase id label display for a given post view.
The critical loadcase id display is only supported for
NXOpen.CAE.LaminateGraphicalReport
results, for specific datasets.Signature
PostviewSetCriticalLoadIdDisplay(postviewId, displayCriticalLoads)
Parameters: - postviewId (int) – Id of the post view on which the display is to be (de)activated
- displayCriticalLoads (bool) – If true, the critical loadcase ids will be displayed on elements
New in version NX9.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
PostviewSetCriticalPlyIdDisplay¶
-
Post.
PostviewSetCriticalPlyIdDisplay
¶ Activate or deactivate the laminate critical ply id label display for a given post view.
The critical ply id display is only supported for
NXOpen.CAE.LaminateGraphicalReport
results, for specific datasets.Signature
PostviewSetCriticalPlyIdDisplay(postviewId, displayCriticalPlies)
Parameters: - postviewId (int) – Id of the post view on which the display is to be (de)activated
- displayCriticalPlies (bool) – If true, the critical ply ids will be displayed on elements
New in version NX8.5.0.
License requirements: nx_lam_composites (“Laminate Composites”)
PostviewSetCurrentInOverlay¶
-
Post.
PostviewSetCurrentInOverlay
¶ Set the input postview id as the current postview if it is one of several overlaid postviews The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetCurrentInOverlay(postviewId)
Parameters: postviewId (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetDeformation¶
-
Post.
PostviewSetDeformation
¶ Overloaded method PostviewSetDeformation
PostviewSetDeformation(postviewId, deformation)
PostviewSetDeformation(postviewId, deformation)
-------------------------------------
Set the result for deformed shape in the input postview id. Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
NXOpen.CAE.ResultDeformationParameters_Struct
has been replaced byNXOpen.CAE.DeformationParameters
This method is replaced byNXOpen.CAE.Post.PostviewSetDeformation
Signature
PostviewSetDeformation(postviewId, deformation)
Parameters: - postviewId (int) –
- deformation (
NXOpen.CAE.ResultDeformationParameters_Struct
) –
New in version NX5.0.0.
Deprecated since version NX7.5.1: Use
NXOpen.CAE.Post.PostviewSetDeformation
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Set the result for deformed shape in the input postview id. Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetDeformation(postviewId, deformation)
Parameters: - postviewId (int) –
- deformation (
NXOpen.CAE.DeformationParameters
) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
PostviewSetDeformed¶
-
Post.
PostviewSetDeformed
¶ Set the primary display to be deformed/undeformed in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetDeformed(postviewId, deformed)
Parameters: - postviewId (int) –
- deformed (bool) –
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetDeformedUndeformedSynchronization¶
-
Post.
PostviewSetDeformedUndeformedSynchronization
¶ Set the primary display to be deformed/undeformed in the input postview id.
Specify any additional undeformed display and whether the load case and iteration are to sunchronized for the color display and deformed shape. Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetDeformedUndeformedSynchronization(postviewId, showDeformedPrimaryDisplay, showUndeformedModel, synchronizeLoadCaseAndIteration)
Parameters: - postviewId (int) –
- showDeformedPrimaryDisplay (bool) –
- showUndeformedModel (bool) –
- synchronizeLoadCaseAndIteration (bool) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetEdgeFace¶
-
Post.
PostviewSetEdgeFace
¶ Overloaded method PostviewSetEdgeFace
PostviewSetEdgeFace(postviewId, primaryEdgeface, undeformedEdgeface)
PostviewSetEdgeFace(postviewId, edgeface)
-------------------------------------
Set edge and face styles and colors for both primary and undeformed displays in the input postview id. Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetEdgeFace(postviewId, primaryEdgeface, undeformedEdgeface)
Parameters: - postviewId (int) –
- primaryEdgeface (
NXOpen.CAE.PostEdgeFace_Struct
) – - undeformedEdgeface (
NXOpen.CAE.PostEdgeFace_Struct
) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Set edge and face styles and colors for primary display in the input postview id. Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreateCrossSectionViewForResult
Signature
PostviewSetEdgeFace(postviewId, edgeface)
Parameters: - postviewId (int) –
- edgeface (
NXOpen.CAE.PostEdgeFace_Struct
) –
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
PostviewSetFontSize¶
-
Post.
PostviewSetFontSize
¶ Set font size options in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview, CreatePostviewForResult, or CreateCrossSectionViewForResult
Signature
PostviewSetFontSize(postviewId, autoFontSize, fontScale)
Parameters: - postviewId (int) –
- autoFontSize (bool) –
- fontScale (float) –
New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetFormat¶
-
Post.
PostviewSetFormat
¶ Set text formating used for legend and identify in the input postview id.
The other options are not yet supported. Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetFormat(postviewId, format, numdecimal)
Parameters: - postviewId (int) –
- format (
NXOpen.CAE.PostFormat
) – - numdecimal (int) –
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetGroupContainerVisibility¶
-
Post.
PostviewSetGroupContainerVisibility
¶ Set the visibility of an element group container in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetGroupContainerVisibility(postviewId, container, visibility)
Parameters: - postviewId (int) –
- container (
NXOpen.CAE.ResultGroupContainer
) – - visibility (bool) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetGroupVisibility¶
-
Post.
PostviewSetGroupVisibility
¶ Set the visibility of an element group (index) within a container (1D, 2D, Connector etc) in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetGroupVisibility(postviewId, container, group, visibility)
Parameters: - postviewId (int) –
- container (
NXOpen.CAE.ResultGroupContainer
) – - group (int) – 0 thru number of groups in container - 1
- visibility (bool) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetHeaderlines¶
-
Post.
PostviewSetHeaderlines
¶ Set headerlines in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview, CreatePostviewForResult, or CreateCrossSectionViewForResult
Signature
PostviewSetHeaderlines(postviewId, headerlines)
Parameters: - postviewId (int) –
- headerlines (list of
NXOpen.CAE.PostHeaderlines_Struct
) –
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetLegend¶
-
Post.
PostviewSetLegend
¶ Set legend options in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview, CreatePostviewForResult, or CreateCrossSectionViewForResult
Signature
PostviewSetLegend(postviewId, showLegend, legend)
Parameters: - postviewId (int) –
- showLegend (bool) –
- legend (
NXOpen.CAE.PostLegend
) –
New in version NX5.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.CAE.Post.PostviewSetShowHeader
andNXOpen.CAE.Post.PostviewSetColorbar
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetLighting¶
-
Post.
PostviewSetLighting
¶ Set lighted option in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetLighting(postviewId, lighted)
Parameters: - postviewId (int) –
- lighted (bool) – If true fringe display is drawn with the lighting setting provided in view setting if false fringe display drawn with the color set color without botherring about surface normal and view angle
New in version NX8.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetMark¶
-
Post.
PostviewSetMark
¶ Set the mark display options in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetMark(postviewId, mark)
Parameters: - postviewId (int) –
- mark (
NXOpen.CAE.PostMark_Struct
) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetMarker¶
-
Post.
PostviewSetMarker
¶ Set min-max marker options in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetMarker(postviewId, showMarker, marker)
Parameters: - postviewId (int) –
- showMarker (bool) –
- marker (
NXOpen.CAE.PostMarker
) –
New in version NX5.0.0.
Deprecated since version NX9.0.0: Set
NXOpen.CAE.PostAnnotation
show hide instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetPosition¶
-
Post.
PostviewSetPosition
¶ Set legend positioning in the input postview id.
The other options are not yet supported. Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetPosition(postviewId, position)
Parameters: - postviewId (int) –
- position (
NXOpen.CAE.PostPosition
) –
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetResult¶
-
Post.
PostviewSetResult
¶ Overloaded method PostviewSetResult
PostviewSetResult(postviewId, result)
PostviewSetResult(postviewId, resultParamter)
-------------------------------------
Set the result for color display in the input postview id. Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
NXOpen.CAE.ResultResultParameters_Struct
has been replaced byNXOpen.CAE.ResultParameters
This method is replaced byNXOpen.CAE.Post.PostviewSetResult
Signature
PostviewSetResult(postviewId, result)
Parameters: - postviewId (int) –
- result (
NXOpen.CAE.ResultResultParameters_Struct
) –
New in version NX5.0.0.
Deprecated since version NX7.5.1: Use
NXOpen.CAE.Post.PostviewSetResult
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Set the result for color display in the input postview id. Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetResult(postviewId, resultParamter)
Parameters: - postviewId (int) –
- resultParamter (
NXOpen.CAE.ResultParameters
) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
PostviewSetResultWithProbe¶
-
Post.
PostviewSetResultWithProbe
¶ Set the result for color display in the input for postview which is created with a probe
NXOpen.CAE.Post.CreatePostview
.Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetResultWithProbe(postviewId, probeparams)
Parameters: - postviewId (int) –
- probeparams (
NXOpen.CAE.ResultParametersWithProbe
) –
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetShowHeader¶
-
Post.
PostviewSetShowHeader
¶ Set show header option in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview, CreatePostviewForResult, or CreateCrossSectionViewForResult
Signature
PostviewSetShowHeader(postviewId, showHeader)
Parameters: - postviewId (int) –
- showHeader (
NXOpen.CAE.PostShowHeader
) –
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetStreamline¶
-
Post.
PostviewSetStreamline
¶ Set the streamline display options in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetStreamline(postviewId, streamline)
Parameters: - postviewId (int) –
- streamline (
NXOpen.CAE.PostStreamline_Struct
) –
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PostviewSetStreamlineSeedSet¶
-
Post.
PostviewSetStreamlineSeedSet
¶ Set the seed set to use for streamline extraction in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetStreamlineSeedSet(postviewId, seedsetId)
Parameters: - postviewId (int) –
- seedsetId (int) –
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PostviewSetStreamlineVelocity¶
-
Post.
PostviewSetStreamlineVelocity
¶ Overloaded method PostviewSetStreamlineVelocity
PostviewSetStreamlineVelocity(postviewId, velocity)
PostviewSetStreamlineVelocity(postviewId, velocity)
-------------------------------------
Set the velocity field for streamline extraction in the input postview id. Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
NXOpen.CAE.ResultVelocityParameters_Struct
is no longer been supported This method is replaced byNXOpen.CAE.Post.PostviewSetStreamlineVelocity
Signature
PostviewSetStreamlineVelocity(postviewId, velocity)
Parameters: - postviewId (int) –
- velocity (
NXOpen.CAE.ResultVelocityParameters_Struct
) –
New in version NX6.0.0.
Deprecated since version NX7.5.1: Use
NXOpen.CAE.Post.PostviewSetStreamlineVelocity
instead.License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Set the velocity field for streamline extraction in the input postview id. Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetStreamlineVelocity(postviewId, velocity)
Parameters: - postviewId (int) –
- velocity (
NXOpen.CAE.BaseResultType
) –
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
PostviewSetStyle¶
-
Post.
PostviewSetStyle
¶ Set the fringe style in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview, CreatePostviewForResult, or CreateCrossSectionViewForResult
Signature
PostviewSetStyle(postviewId, showStyle, style)
Parameters: - postviewId (int) –
- showStyle (int) –
- style (
NXOpen.CAE.PostStyle
) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetTarget¶
-
Post.
PostviewSetTarget
¶ Set the target operator in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetTarget(postviewId, target)
Parameters: - postviewId (int) –
- target (
NXOpen.CAE.PostTarget
) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetText¶
-
Post.
PostviewSetText
¶ Set text color used for legend and identify in the input postview id.
The other options are not yet supported. Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetText(postviewId, text)
Parameters: - postviewId (int) –
- text (
NXOpen.CAE.PostText_Struct
) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewSetUndeformed¶
-
Post.
PostviewSetUndeformed
¶ Set the undeformed display in the input postview id.
Needs a PostviewUpdate call to take effect. The input postview id is what was returned from CreatePostview or CreatePostviewForResult
Signature
PostviewSetUndeformed(postviewId, undeformed)
Parameters: - postviewId (int) –
- undeformed (bool) –
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PostviewUpdate¶
-
Post.
PostviewUpdate
¶ Make the input postview id up-to-date with all the settings made via PostviewSet* methods so far.
The input postview id is what was returned from CreatePostview, CreatePostviewForResult, or CreateCrossSectionViewForResult
Signature
PostviewUpdate(postviewId)
Parameters: postviewId (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ReloadTemplates¶
-
Post.
ReloadTemplates
¶ Search and load template xml files
Signature
ReloadTemplates()
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetFactoryDefaultTemplate¶
-
Post.
SetFactoryDefaultTemplate
¶ Use factory defaults rather than a template for the default postview settings to be used in all subsequent PostviewCreate calls
Signature
SetFactoryDefaultTemplate()
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
StreamlineSeedSetDelete¶
-
Post.
StreamlineSeedSetDelete
¶ Delete a Seed Set.
The input seedset id is what was returned from
NXOpen.CAE.Post.CreateStreamlineSeedSet
Signature
StreamlineSeedSetDelete(seedsetId)
Parameters: seedsetId (int) – New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
TemplateDelete¶
-
Post.
TemplateDelete
¶ Delete a loaded template xml file specified by template_id.
The input template_id is what was returned from PostviewSaveTemplate or TemplateSearch
Signature
TemplateDelete(templateId)
Parameters: templateId (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
TemplateRename¶
-
Post.
TemplateRename
¶ Rename a loaded template xml file specified by template_id.
The input template_id is what was returned from PostviewSaveTemplate or TemplateSearch
Signature
TemplateRename(templateId, newName)
Parameters: - templateId (int) –
- newName (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
TemplateSearch¶
-
Post.
TemplateSearch
¶ Search for a template handle for loaded template xml file specified by its name.
Returns a template handle that may be used in PostviewApplyTemplate and Template* calls
Signature
TemplateSearch(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: int New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
TemplateSetAsDefault¶
-
Post.
TemplateSetAsDefault
¶ Set a loaded template as the default postview settings to be used for all subsequent PostviewCreate calls.
The input template_id is what was returned from PostviewSaveTemplate or TemplateSearch
Signature
TemplateSetAsDefault(templateId)
Parameters: templateId (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
UnloadResult¶
-
Post.
UnloadResult
¶ Unload the input result id.
The result id is what was obtained from LoadImportedResult or LoadSolutionResult
Signature
UnloadResult(resultId)
Parameters: resultId (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
UnloadResultFile¶
-
Post.
UnloadResultFile
¶ Unload results that use the input file name
Signature
UnloadResultFile(fileName)
Parameters: fileName (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
UpdateUserGroupsFromSimPart¶
-
Post.
UpdateUserGroupsFromSimPart
¶ Synchronize the Groups in Post-Processing with those in the Simulation Part
Signature
UpdateUserGroupsFromSimPart(simpart)
Parameters: simpart ( NXOpen.CAE.SimPart
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
UserGroupDelete¶
-
Post.
UserGroupDelete
¶ Rename a User Group.
The input usergroup id is what was returned from CreateUserGroupFromEntityLabels
Signature
UserGroupDelete(usergroupId)
Parameters: usergroupId (int) – New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
UserGroupRename¶
-
Post.
UserGroupRename
¶ Delete a User Group.
The input usergroup id is what was returned from CreateUserGroupFromEntityLabels
Signature
UserGroupRename(usergroupId, newName)
Parameters: - usergroupId (int) –
- newName (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)