Plot Class¶
-
class
NXOpen.CAE.Xyplot.
Plot
¶ Bases:
NXOpen.NXObject
Manages the plot template
Not support KF.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PlotTemplate | Returns the plot template |
Prototype | Returns the prototype of this object if it is an occurrence. |
SubGraphCountInStack | Returns the sub-graph count in a stacked plot. |
Tag | Returns the Tag for this object. |
Template | Returns the plot template |
Methods¶
Method | Description |
---|---|
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
Find | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
FitAxisLimit | Update axis limits for an overlaying plot if current displayed axis limits in plot do not fit for all records. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDeviceAndViewIndex | Gets the window device and view index of the plot graph. |
GetGraphs | Gets all graphs on the plot. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetRecordCount | Returns the count of plotted records on the plot graph. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Prints a representation of this object to the system log file. | |
SaveRecord | Saves a plotted record on the plot graph to an afu file. |
SaveRecords | Saves plotted records on a graph to an afu file. |
SaveRecordsToCsv | Saves plotted records on a plot graph to a CSV file. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
IsOccurrence¶
-
Plot.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Plot.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
Plot.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Plot.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Plot.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
PlotTemplate¶
-
Plot.
PlotTemplate
¶ Returns the plot template
-------------------------------------
Getter Method
Signature
PlotTemplate()
Returns: Plot template Return type: NXOpen.CAE.Xyplot.PlotGraphTemplate
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
Prototype¶
-
Plot.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
SubGraphCountInStack¶
-
Plot.
SubGraphCountInStack
¶ Returns the sub-graph count in a stacked plot.
-------------------------------------
Getter Method
Signature
SubGraphCountInStack()
Returns: Sub-graph count Return type: int New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
Template¶
-
Plot.
Template
¶ Returns the plot template
-------------------------------------
Getter Method
Signature
Template()
Returns: Plot template Return type: NXOpen.CAE.Xyplot.BaseTemplate
New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.Xyplot.Plot.PlotTemplate
instead.License requirements: nx_ftk (“NX Advanced Graphing”)
Method Detail¶
Find¶
-
Plot.
Find
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
Find(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.TaggedObject
New in version NX10.0.0.
License requirements: None.
FindObject¶
-
Plot.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
FitAxisLimit¶
-
Plot.
FitAxisLimit
¶ Update axis limits for an overlaying plot if current displayed axis limits in plot do not fit for all records.
Signature
FitAxisLimit()
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
GetDeviceAndViewIndex¶
-
Plot.
GetDeviceAndViewIndex
¶ Gets the window device and view index of the plot graph.
Signature
GetDeviceAndViewIndex()
Returns: a tuple Return type: A tuple consisting of (windowDevice, viewIndex). windowDevice is a int. the device of window viewIndex is a int. the index of view New in version NX9.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
GetGraphs¶
-
Plot.
GetGraphs
¶ Gets all graphs on the plot.
Signature
GetGraphs()
Returns: Graph objects Return type: list of NXOpen.CAE.Xyplot.Graph
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
GetRecordCount¶
-
Plot.
GetRecordCount
¶ Returns the count of plotted records on the plot graph.
Signature
GetRecordCount()
Returns: Record count Return type: int New in version NX9.0.0.
License requirements: None.
Print¶
-
Plot.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SaveRecord¶
-
Plot.
SaveRecord
¶ Saves a plotted record on the plot graph to an afu file.
Use
NXOpen.CAE.AfuManager.CreateRecord
to create the record.Signature
SaveRecord(recordIndex, afuFileName, recordName)
Parameters: - recordIndex (int) – the index of record to be saved
- afuFileName (str) – Afu file name NOTE: The full Unicode character set is not supported for this parameter.
- recordName (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.Xyplot.Plot.SaveRecords
instead.License requirements: nx_ftk (“NX Advanced Graphing”)
SaveRecords¶
-
Plot.
SaveRecords
¶ Saves plotted records on a graph to an afu file.
The record index is between 0 and the value returned from
NXOpen.CAE.Xyplot.Plot.GetRecordCount
.Signature
SaveRecords(recordIndexes, recordNames, outputFileName, reportError)
Parameters: - recordIndexes (list of int) – The index of records to be saved
- recordNames (list of str) – The output record names NOTE: The full Unicode character set is not supported for this parameter.
- outputFileName (str) – The destination file with full file name. The file suffix must be ”.afu”. NOTE: The full Unicode character set is not supported for this parameter.
- reportError (bool) –
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
SaveRecordsToCsv¶
-
Plot.
SaveRecordsToCsv
¶ Saves plotted records on a plot graph to a CSV file.
Signature
SaveRecordsToCsv(recordIndex, recordNames, csvFileName, isWriteHeader)
Parameters: - recordIndex (list of int) – the indexes of records to be saved
- recordNames (list of str) – NOTE: The full Unicode character set is not supported for this parameter.
- csvFileName (str) – the destination CSV file name NOTE: The full Unicode character set is not supported for this parameter.
- isWriteHeader (bool) –
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
SetName¶
-
Plot.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.