ResultDeformationParameters_Struct Struct¶
NXOpen.CAE.Result.DeformationParameters is an alias for NXOpen.CAE.ResultDeformationParameters_Struct
-
class
NXOpen.CAE.
ResultDeformationParameters_Struct
¶ Bases:
object
Deformation parameter structure to specify complete result state for the deformed shape This structure has been replaced by
NXOpen.CAE.DeformationParameters
Deprecated since version NX7.5.1: This structure has been replaced by
NXOpen.CAE.DeformationParameters
Fields¶
Field | Description |
---|---|
LoadCaseIndex | load case number starting from 0 |
IterationIndex | iteration number starting from 0 |
Type | |
Complex | |
PhaseAngle | |
DeformationScale | |
AbsoluteScaleValue | |
ModelPercentScaleValue |
LoadCaseIndex¶
-
ResultDeformationParameters_Struct.
LoadCaseIndex
¶ load case number starting from 0
-------------------------------------
Getter Method Signature
LoadCaseIndex()
Returns: Return type: int -------------------------------------
Setter Method
Signature
LoadCaseIndex(value)
Parameters: value (int) –
IterationIndex¶
-
ResultDeformationParameters_Struct.
IterationIndex
¶ iteration number starting from 0
-------------------------------------
Getter Method Signature
IterationIndex()
Returns: Return type: int -------------------------------------
Setter Method
Signature
IterationIndex(value)
Parameters: value (int) –
Type¶
-
ResultDeformationParameters_Struct.
Type
¶ -------------------------------------
Getter Method Signature
Type()
Returns: Return type: NXOpen.CAE.ResultType_Struct
-------------------------------------
Setter Method
Signature
Type(value)
Parameters: value ( NXOpen.CAE.ResultType_Struct
) –
Complex¶
-
ResultDeformationParameters_Struct.
Complex
¶ -------------------------------------
Getter Method Signature
Complex()
Returns: Return type: NXOpen.CAE.ResultComplex
-------------------------------------
Setter Method
Signature
Complex(value)
Parameters: value ( NXOpen.CAE.ResultComplex
) –
PhaseAngle¶
-
ResultDeformationParameters_Struct.
PhaseAngle
¶ -------------------------------------
Getter Method Signature
PhaseAngle()
Returns: Return type: float -------------------------------------
Setter Method
Signature
PhaseAngle(value)
Parameters: value (float) –
DeformationScale¶
-
ResultDeformationParameters_Struct.
DeformationScale
¶ -------------------------------------
Getter Method Signature
DeformationScale()
Returns: Return type: NXOpen.CAE.ResultDeformationScale
-------------------------------------
Setter Method
Signature
DeformationScale(value)
Parameters: value ( NXOpen.CAE.ResultDeformationScale
) –
AbsoluteScaleValue¶
-
ResultDeformationParameters_Struct.
AbsoluteScaleValue
¶ -------------------------------------
Getter Method Signature
AbsoluteScaleValue()
Returns: Return type: float -------------------------------------
Setter Method
Signature
AbsoluteScaleValue(value)
Parameters: value (float) –
ModelPercentScaleValue¶
-
ResultDeformationParameters_Struct.
ModelPercentScaleValue
¶ -------------------------------------
Getter Method Signature
ModelPercentScaleValue()
Returns: Return type: float -------------------------------------
Setter Method
Signature
ModelPercentScaleValue(value)
Parameters: value (float) –