PostAnimationStreamline_Struct Struct¶
NXOpen.CAE.Post.AnimationStreamline is an alias for NXOpen.CAE.PostAnimationStreamline_Struct
-
class
NXOpen.CAE.
PostAnimationStreamline_Struct
¶ Bases:
object
Animation settings for streamline animation
Fields¶
Field | Description |
---|---|
ShowGuides | |
StreamSync | |
ActiveRegionStartFactor | between 0. |
ActiveRegionEndFactor | between 0. |
NumberOfIncrements | |
ContinuousPulse | |
NumberOfTimePeriods | |
FramesPerPulse | more than 2. |
PulseDutycycle | not yet supported |
ShowGuides¶
-
PostAnimationStreamline_Struct.
ShowGuides
¶ -------------------------------------
Getter Method Signature
ShowGuides()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
ShowGuides(value)
Parameters: value (bool) –
StreamSync¶
-
PostAnimationStreamline_Struct.
StreamSync
¶ -------------------------------------
Getter Method Signature
StreamSync()
Returns: Return type: NXOpen.CAE.PostStreamlineSynchronization
-------------------------------------
Setter Method
Signature
StreamSync(value)
Parameters: value ( NXOpen.CAE.PostStreamlineSynchronization
) –
ActiveRegionStartFactor¶
-
PostAnimationStreamline_Struct.
ActiveRegionStartFactor
¶ between 0.
0 and 1.0
-------------------------------------
Getter Method Signature
ActiveRegionStartFactor()
Returns: Return type: float -------------------------------------
Setter Method
Signature
ActiveRegionStartFactor(value)
Parameters: value (float) –
ActiveRegionEndFactor¶
-
PostAnimationStreamline_Struct.
ActiveRegionEndFactor
¶ between 0.
0 and 1.0
-------------------------------------
Getter Method Signature
ActiveRegionEndFactor()
Returns: Return type: float -------------------------------------
Setter Method
Signature
ActiveRegionEndFactor(value)
Parameters: value (float) –
NumberOfIncrements¶
-
PostAnimationStreamline_Struct.
NumberOfIncrements
¶ -------------------------------------
Getter Method Signature
NumberOfIncrements()
Returns: Return type: int -------------------------------------
Setter Method
Signature
NumberOfIncrements(value)
Parameters: value (int) –
ContinuousPulse¶
-
PostAnimationStreamline_Struct.
ContinuousPulse
¶ -------------------------------------
Getter Method Signature
ContinuousPulse()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
ContinuousPulse(value)
Parameters: value (bool) –
NumberOfTimePeriods¶
-
PostAnimationStreamline_Struct.
NumberOfTimePeriods
¶ -------------------------------------
Getter Method Signature
NumberOfTimePeriods()
Returns: Return type: int -------------------------------------
Setter Method
Signature
NumberOfTimePeriods(value)
Parameters: value (int) –