CAEConnectionCollection Class¶
-
class
NXOpen.CAE.
CAEConnectionCollection
¶ Bases:
object
Provides method for creating builder for connection operation commands in a fem/afem part
To obtain an instance of this class, refer to
NXOpen.CAE.BaseFEModel
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateConnectionBuilder | Creates a builder for Connection Command @return |
CreateWeldConnectionBuilder | Creates a builder for WeldConnection Command @return |
FindObject | Finds the NXOpen.CAE.CAEConnection with the given identifier as recorded in a journal. |
Method Detail¶
CreateConnectionBuilder¶
-
CAEConnectionCollection.
CreateConnectionBuilder
¶ Creates a builder for Connection Command
Signature
CreateConnectionBuilder(connection)
Parameters: connection ( NXOpen.CAE.CAEConnection
) –NXOpen.CAE.CAEConnection
to be edited, if None then create a new oneReturns: Return type: NXOpen.CAE.CAEConnectionBuilder
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateWeldConnectionBuilder¶
-
CAEConnectionCollection.
CreateWeldConnectionBuilder
¶ Creates a builder for WeldConnection Command
Signature
CreateWeldConnectionBuilder(weldconnection)
Parameters: weldconnection ( NXOpen.CAE.CAEWeldConnection
) – WeldConnection Recipe to be edited, if None then create a new oneReturns: Return type: NXOpen.CAE.CAEWeldConnectionBuilder
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
FindObject¶
-
CAEConnectionCollection.
FindObject
¶ Finds the
NXOpen.CAE.CAEConnection
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Connection name Returns: connection with this identifier Return type: NXOpen.CAE.CAEConnection
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)