CaeGroupCollectionAutoGroupTypes_Struct Struct¶
NXOpen.CAE.CaeGroupCollection.AutoGroupTypes is an alias for NXOpen.CAE.CaeGroupCollectionAutoGroupTypes_Struct
-
class
NXOpen.CAE.
CaeGroupCollectionAutoGroupTypes_Struct
¶ Bases:
object
Contains information about the types by which we do auto grouping
Fields¶
Field | Description |
---|---|
ByMaterial | true if meshes are to be grouped by material |
ByPpt | true if meshes are to be grouped by physical property table |
ByColor | true if meshes are to be grouped by color |
BySection | true if meshes are to be grouped by 1-D section |
ByLaminate | true if meshes are to be grouped by laminate |
ByDimension | true if meshes are to be grouped by dimension |
ByMeshcolltype | true if meshes are to be grouped by mesh collector type |
ByMeshsubtype | related to meshes_by_meshcolltype, true if we also want to group by mesh subtype |
ByMaterial¶
-
CaeGroupCollectionAutoGroupTypes_Struct.
ByMaterial
¶ true if meshes are to be grouped by material
-------------------------------------
Getter Method Signature
ByMaterial()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
ByMaterial(value)
Parameters: value (bool) –
ByPpt¶
-
CaeGroupCollectionAutoGroupTypes_Struct.
ByPpt
¶ true if meshes are to be grouped by physical property table
-------------------------------------
Getter Method Signature
ByPpt()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
ByPpt(value)
Parameters: value (bool) –
ByColor¶
-
CaeGroupCollectionAutoGroupTypes_Struct.
ByColor
¶ true if meshes are to be grouped by color
-------------------------------------
Getter Method Signature
ByColor()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
ByColor(value)
Parameters: value (bool) –
BySection¶
-
CaeGroupCollectionAutoGroupTypes_Struct.
BySection
¶ true if meshes are to be grouped by 1-D section
-------------------------------------
Getter Method Signature
BySection()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
BySection(value)
Parameters: value (bool) –
ByLaminate¶
-
CaeGroupCollectionAutoGroupTypes_Struct.
ByLaminate
¶ true if meshes are to be grouped by laminate
-------------------------------------
Getter Method Signature
ByLaminate()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
ByLaminate(value)
Parameters: value (bool) –
ByDimension¶
-
CaeGroupCollectionAutoGroupTypes_Struct.
ByDimension
¶ true if meshes are to be grouped by dimension
-------------------------------------
Getter Method Signature
ByDimension()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
ByDimension(value)
Parameters: value (bool) –
ByMeshcolltype¶
-
CaeGroupCollectionAutoGroupTypes_Struct.
ByMeshcolltype
¶ true if meshes are to be grouped by mesh collector type
-------------------------------------
Getter Method Signature
ByMeshcolltype()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
ByMeshcolltype(value)
Parameters: value (bool) –
ByMeshsubtype¶
-
CaeGroupCollectionAutoGroupTypes_Struct.
ByMeshsubtype
¶ related to meshes_by_meshcolltype, true if we also want to group by mesh subtype
-------------------------------------
Getter Method Signature
ByMeshsubtype()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
ByMeshsubtype(value)
Parameters: value (bool) –