NodeModifyLocationBuilder Class¶
-
class
NXOpen.CAE.
NodeModifyLocationBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.NodeModifyLocationBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateNodeModifyLocationBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Csys | Returns or sets the csys |
Node | Returns the node |
Phi | Returns the phi |
Tag | Returns the Tag for this object. |
Theta | Returns the theta |
NXOpen.CAE.NodeModifyLocationBuilder.X | Returns the x |
XOption | Returns or sets the x option |
NXOpen.CAE.NodeModifyLocationBuilder.Y | Returns the y |
YOption | Returns or sets the y option |
NXOpen.CAE.NodeModifyLocationBuilder.Z | Returns the z |
ZOption | Returns or sets the z option |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Csys¶
-
NodeModifyLocationBuilder.
Csys
¶ Returns or sets the csys
-------------------------------------
Getter Method
Signature
Csys()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Csys(csys)
Parameters: csys ( NXOpen.CoordinateSystem
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Node¶
-
NodeModifyLocationBuilder.
Node
¶ Returns the node
-------------------------------------
Getter Method
Signature
Node()
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX5.0.0.
License requirements: None.
Phi¶
-
NodeModifyLocationBuilder.
Phi
¶ Returns the phi
-------------------------------------
Getter Method
Signature
Phi()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
Theta¶
-
NodeModifyLocationBuilder.
Theta
¶ Returns the theta
-------------------------------------
Getter Method
Signature
Theta()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
X¶
-
NodeModifyLocationBuilder.
X
¶ Returns the x
-------------------------------------
Getter Method
Signature
X()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
XOption¶
-
NodeModifyLocationBuilder.
XOption
¶ Returns or sets the x option
-------------------------------------
Getter Method
Signature
XOption()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XOption(xOption)
Parameters: xOption (bool) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Y¶
-
NodeModifyLocationBuilder.
Y
¶ Returns the y
-------------------------------------
Getter Method
Signature
Y()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
YOption¶
-
NodeModifyLocationBuilder.
YOption
¶ Returns or sets the y option
-------------------------------------
Getter Method
Signature
YOption()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YOption(yOption)
Parameters: yOption (bool) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Z¶
-
NodeModifyLocationBuilder.
Z
¶ Returns the z
-------------------------------------
Getter Method
Signature
Z()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
ZOption¶
-
NodeModifyLocationBuilder.
ZOption
¶ Returns or sets the z option
-------------------------------------
Getter Method
Signature
ZOption()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZOption(zOption)
Parameters: zOption (bool) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
NodeModifyLocationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.