CorrelSolutionCollection Class¶
-
class
NXOpen.CAE.
CorrelSolutionCollection
¶ Bases:
object
Represents a collection of correl meta solution
To obtain an instance of this class, refer to
NXOpen.CAE.CorrelManager
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ActiveSolution | Returns or sets the active solution |
Methods¶
Method | Description |
---|---|
CloneSolution | Clones a correl meta solution @return the newly created NXOpen.CAE.CorrelSolution |
CreateComacViewerBuilder | Creates the builder object of correl comac matrix viewer @return |
CreateShapeMetricViewerBuilder | Creates the builder object of correl shape metric viewer @return |
CreateSolutionBuilder | Creates the builder object of correl meta solution @return |
FindObject | Finds a correl meta solution with specified solution name @return Correlation metasolution found |
GetValidSolutionName | Returns next valid correlation solution name @return a NXOpen.CAE.CorrelSolution valid name |
Property Detail¶
ActiveSolution¶
-
CorrelSolutionCollection.
ActiveSolution
¶ Returns or sets the active solution
-------------------------------------
Getter Method
Signature
ActiveSolution()
Returns: Return type: NXOpen.CAE.CorrelSolution
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActiveSolution(activeSolution)
Parameters: activeSolution ( NXOpen.CAE.CorrelSolution
) –New in version NX5.0.0.
License requirements: None.
Method Detail¶
CloneSolution¶
-
CorrelSolutionCollection.
CloneSolution
¶ Clones a correl meta solution
Signature
CloneSolution(oldSolution, suggestedName)
Parameters: - oldSolution (
NXOpen.CAE.CorrelSolution
) – theNXOpen.CAE.SimSolution
to be cloned - suggestedName (str) – name to use instead of default name (may be NULL)
Returns: the newly created
NXOpen.CAE.CorrelSolution
Return type: New in version NX5.0.0.
License requirements: None.
- oldSolution (
CreateComacViewerBuilder¶
-
CorrelSolutionCollection.
CreateComacViewerBuilder
¶ Creates the builder object of correl comac matrix viewer
Signature
CreateComacViewerBuilder()
Returns: Return type: NXOpen.CAE.ComacViewerBuilder
New in version NX6.0.0.
License requirements: nx_correl_base (“FE Correlation”)
CreateShapeMetricViewerBuilder¶
-
CorrelSolutionCollection.
CreateShapeMetricViewerBuilder
¶ Creates the builder object of correl shape metric viewer
Signature
CreateShapeMetricViewerBuilder(solution)
Parameters: solution ( NXOpen.CAE.CorrelSolution
) – Correlation setupReturns: Return type: NXOpen.CAE.ShapeMetricViewerBuilder
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
CreateSolutionBuilder¶
-
CorrelSolutionCollection.
CreateSolutionBuilder
¶ Creates the builder object of correl meta solution
Signature
CreateSolutionBuilder(solution)
Parameters: solution ( NXOpen.CAE.CorrelSolution
) –Returns: Return type: NXOpen.CAE.CorrelSolutionBuilder
New in version NX5.0.0.
License requirements: None.
FindObject¶
-
CorrelSolutionCollection.
FindObject
¶ Finds a correl meta solution with specified solution name
Signature
FindObject(solutionName)
Parameters: solutionName (str) – Solution to be found Returns: Correlation metasolution found Return type: NXOpen.CAE.CorrelSolution
New in version NX5.0.0.
License requirements: None.
GetValidSolutionName¶
-
CorrelSolutionCollection.
GetValidSolutionName
¶ Returns next valid correlation solution name
Signature
GetValidSolutionName()
Returns: a NXOpen.CAE.CorrelSolution
valid nameReturn type: str New in version NX5.0.0.
License requirements: None.