XyFunctionDataType Enumeration¶
-
class
NXOpen.CAE.
XyFunctionDataType
¶ Bases:
object
Defines the data type of a function in AFU file Enum Members
Enum Member Enum Member Description General Function is General Function.Time Function is Time HistoryCrossSpectrum Function is Cross SpectrumFrequencyResponseFunction Function is Frequency Response FunctionTransmissibility Function is TransmissibilityPowerSpectralDensity Function is Power Spectral DensitySpectrum Function is SpectrumShockResponseSpectrum Function is Shock Response SpectrumTemperature Function is TemperatureStressStrain Function is Stress/Strain FunctionLife Function is Fatigue LifeCampbellDiagram Function is Campbell DiagramTimingChart Function is Timing ChartStiffnessAndDamping Function is Stiffness and Damping-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-