ModelUpdateDesignVariablesRapidCreateBuilder Class¶
-
class
NXOpen.CAE.
ModelUpdateDesignVariablesRapidCreateBuilder
¶ Bases:
NXOpen.Builder
This class is the builder that is used for the rapid creation of design variables.
To create a new instance of this class, use
NXOpen.CAE.CorrelManager.CreateModelUpdateDesignVariablesRapidCreateBuilderBuilder
New in version NX8.0.1.
Properties¶
Property | Description |
---|---|
CardName | Returns or sets the card name |
DesignVariableType | Returns or sets the design variable type |
HasInitialValue | Returns or sets the has initial value |
HasLowerBound | Returns or sets the has lower bound |
HasUpperBound | Returns or sets the has upper bound |
InitialValue | Returns or sets the initial value |
LowerBound | Returns or sets the lower bound |
MaterialTypes | Returns or sets the material types |
NameSeed | Returns or sets the name seed |
PhysicalTypes | Returns or sets the physical types |
Tag | Returns the Tag for this object. |
UpperBound | Returns or sets the upper bound |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
DeselectAllEntities | This command deselects all the entities. |
DeselectAllFields | This command deselects all the fields. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SelectAllEntities | This command selects all the entities. |
SelectAllFields | This command selects all the fields. |
SelectEntity | This command selects one entity. |
SelectField | This command selects one field. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ModelUpdateDesignVariablesRapidCreateBuilderDesignVariableTypeEnum Enumeration | The enum for the design variable type. |
ModelUpdateDesignVariablesRapidCreateBuilderMaterialTypesEnum Enumeration | The enum for the material type. |
ModelUpdateDesignVariablesRapidCreateBuilderPhysicalTypesEnum Enumeration | The enum for the physical type. |
Property Detail¶
CardName¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
CardName
¶ Returns or sets the card name
-------------------------------------
Getter Method
Signature
CardName()
Returns: Return type: str New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CardName(cardName)
Parameters: cardName (str) – New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
DesignVariableType¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
DesignVariableType
¶ Returns or sets the design variable type
-------------------------------------
Getter Method
Signature
DesignVariableType()
Returns: Return type: NXOpen.CAE.ModelUpdateDesignVariablesRapidCreateBuilderDesignVariableTypeEnum
New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
DesignVariableType(designVariableType)
Parameters: designVariableType ( NXOpen.CAE.ModelUpdateDesignVariablesRapidCreateBuilderDesignVariableTypeEnum
) –New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
HasInitialValue¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
HasInitialValue
¶ Returns or sets the has initial value
-------------------------------------
Getter Method
Signature
HasInitialValue()
Returns: Return type: bool New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
HasInitialValue(initialValue)
Parameters: initialValue (bool) – New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
HasLowerBound¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
HasLowerBound
¶ Returns or sets the has lower bound
-------------------------------------
Getter Method
Signature
HasLowerBound()
Returns: Return type: bool New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
HasLowerBound(lowerBound)
Parameters: lowerBound (bool) – New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
HasUpperBound¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
HasUpperBound
¶ Returns or sets the has upper bound
-------------------------------------
Getter Method
Signature
HasUpperBound()
Returns: Return type: bool New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
HasUpperBound(upperBound)
Parameters: upperBound (bool) – New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
InitialValue¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
InitialValue
¶ Returns or sets the initial value
-------------------------------------
Getter Method
Signature
InitialValue()
Returns: Return type: float New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
InitialValue(initialValue)
Parameters: initialValue (float) – New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
LowerBound¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
LowerBound
¶ Returns or sets the lower bound
-------------------------------------
Getter Method
Signature
LowerBound()
Returns: Return type: float New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
LowerBound(lowerBound)
Parameters: lowerBound (float) – New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
MaterialTypes¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
MaterialTypes
¶ Returns or sets the material types
-------------------------------------
Getter Method
Signature
MaterialTypes()
Returns: Return type: NXOpen.CAE.ModelUpdateDesignVariablesRapidCreateBuilderMaterialTypesEnum
New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaterialTypes(materialTypes)
Parameters: materialTypes ( NXOpen.CAE.ModelUpdateDesignVariablesRapidCreateBuilderMaterialTypesEnum
) –New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
NameSeed¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
NameSeed
¶ Returns or sets the name seed
-------------------------------------
Getter Method
Signature
NameSeed()
Returns: Return type: str New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
NameSeed(title)
Parameters: title (str) – New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
PhysicalTypes¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
PhysicalTypes
¶ Returns or sets the physical types
-------------------------------------
Getter Method
Signature
PhysicalTypes()
Returns: Return type: NXOpen.CAE.ModelUpdateDesignVariablesRapidCreateBuilderPhysicalTypesEnum
New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
PhysicalTypes(physicalTypes)
Parameters: physicalTypes ( NXOpen.CAE.ModelUpdateDesignVariablesRapidCreateBuilderPhysicalTypesEnum
) –New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
UpperBound¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
UpperBound
¶ Returns or sets the upper bound
-------------------------------------
Getter Method
Signature
UpperBound()
Returns: Return type: float New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperBound(upperBound)
Parameters: upperBound (float) – New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
Method Detail¶
DeselectAllEntities¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
DeselectAllEntities
¶ This command deselects all the entities.
Signature
DeselectAllEntities()
New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
DeselectAllFields¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
DeselectAllFields
¶ This command deselects all the fields.
Signature
DeselectAllFields()
New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
SelectAllEntities¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
SelectAllEntities
¶ This command selects all the entities.
Signature
SelectAllEntities()
New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
SelectAllFields¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
SelectAllFields
¶ This command selects all the fields.
Signature
SelectAllFields()
New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
SelectEntity¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
SelectEntity
¶ This command selects one entity.
Signature
SelectEntity(entityName)
Parameters: entityName (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
SelectField¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
SelectField
¶ This command selects one field.
Signature
SelectField(field)
Parameters: field (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
Validate¶
-
ModelUpdateDesignVariablesRapidCreateBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.