DurabilityStressAxesBuilder Class¶
-
class
NXOpen.CAE.
DurabilityStressAxesBuilder
¶ Bases:
NXOpen.Builder
Represents a builder class for the event fatigue settings.
The fatigue settings help the user control the fatigue/durability parameters in the event. To create a new instance of this class, use
NXOpen.CAE.DurabilityAxisSearchCollection.CreateStressaxesBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
BeamStress | Returns or sets the beam stress. |
ElementFaceStressAxis | Returns or sets the element face stress axis. |
Name | Returns or sets the name. |
NodeElementOption | Returns or sets the node element option. |
SearchResolution | Returns the search resolution. |
ShellRegion | Returns or sets the shell region. |
StressAxisDirectionSearchMethod | Returns or sets the stress axis direction search method. |
StressAxisMethod | Returns or sets the stress axis method. |
StressDirection | Returns or sets the stress direction. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DurabilityStressAxesBuilderBeamStressEnum Enumeration | the Beam Stress Enum |
DurabilityStressAxesBuilderElementFaceStressAxisEnum Enumeration | the Element Face Stress Axis Enum. |
DurabilityStressAxesBuilderNodeElementOptionEnum Enumeration | the Node Element Option Enum. |
DurabilityStressAxesBuilderShellRegionEnum Enumeration | the Shell Region Enum. |
DurabilityStressAxesBuilderStressAxisDirectionSearchMethodEnum Enumeration | the Stress Axis Direction Method Search Enum. |
DurabilityStressAxesBuilderStressAxisMethodEnum Enumeration | the Stress Axis Method Enum. |
Property Detail¶
BeamStress¶
-
DurabilityStressAxesBuilder.
BeamStress
¶ Returns or sets the beam stress.
-------------------------------------
Getter Method
Signature
BeamStress()
Returns: Return type: NXOpen.CAE.DurabilityStressAxesBuilderBeamStressEnum
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BeamStress(beamStress)
Parameters: beamStress ( NXOpen.CAE.DurabilityStressAxesBuilderBeamStressEnum
) –New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
ElementFaceStressAxis¶
-
DurabilityStressAxesBuilder.
ElementFaceStressAxis
¶ Returns or sets the element face stress axis.
-------------------------------------
Getter Method
Signature
ElementFaceStressAxis()
Returns: Return type: NXOpen.CAE.DurabilityStressAxesBuilderElementFaceStressAxisEnum
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ElementFaceStressAxis(elementFaceStressAxis)
Parameters: elementFaceStressAxis ( NXOpen.CAE.DurabilityStressAxesBuilderElementFaceStressAxisEnum
) –New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Name¶
-
DurabilityStressAxesBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(title)
Parameters: title (str) – New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
NodeElementOption¶
-
DurabilityStressAxesBuilder.
NodeElementOption
¶ Returns or sets the node element option.
-------------------------------------
Getter Method
Signature
NodeElementOption()
Returns: Return type: NXOpen.CAE.DurabilityStressAxesBuilderNodeElementOptionEnum
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NodeElementOption(nodeElementOption)
Parameters: nodeElementOption ( NXOpen.CAE.DurabilityStressAxesBuilderNodeElementOptionEnum
) –New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
SearchResolution¶
-
DurabilityStressAxesBuilder.
SearchResolution
¶ Returns the search resolution.
-------------------------------------
Getter Method
Signature
SearchResolution()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
ShellRegion¶
-
DurabilityStressAxesBuilder.
ShellRegion
¶ Returns or sets the shell region.
-------------------------------------
Getter Method
Signature
ShellRegion()
Returns: Return type: NXOpen.CAE.DurabilityStressAxesBuilderShellRegionEnum
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShellRegion(shellRegion)
Parameters: shellRegion ( NXOpen.CAE.DurabilityStressAxesBuilderShellRegionEnum
) –New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
StressAxisDirectionSearchMethod¶
-
DurabilityStressAxesBuilder.
StressAxisDirectionSearchMethod
¶ Returns or sets the stress axis direction search method.
-------------------------------------
Getter Method
Signature
StressAxisDirectionSearchMethod()
Returns: Return type: NXOpen.CAE.DurabilityStressAxesBuilderStressAxisDirectionSearchMethodEnum
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StressAxisDirectionSearchMethod(stressAxisDirectionSearchMethod)
Parameters: stressAxisDirectionSearchMethod ( NXOpen.CAE.DurabilityStressAxesBuilderStressAxisDirectionSearchMethodEnum
) –New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
StressAxisMethod¶
-
DurabilityStressAxesBuilder.
StressAxisMethod
¶ Returns or sets the stress axis method.
-------------------------------------
Getter Method
Signature
StressAxisMethod()
Returns: Return type: NXOpen.CAE.DurabilityStressAxesBuilderStressAxisMethodEnum
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StressAxisMethod(stressAxisMethod)
Parameters: stressAxisMethod ( NXOpen.CAE.DurabilityStressAxesBuilderStressAxisMethodEnum
) –New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
StressDirection¶
-
DurabilityStressAxesBuilder.
StressDirection
¶ Returns or sets the stress direction.
-------------------------------------
Getter Method
Signature
StressDirection()
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StressDirection(stressDirection)
Parameters: stressDirection ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Method Detail¶
Validate¶
-
DurabilityStressAxesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.