FENodeLabelMap Class¶
-
class
NXOpen.CAE.
FENodeLabelMap
¶ Bases:
NXOpen.TransientObject
Represents a Nodel Label to an
CAE.FENode
map, it can be used to quickly convert aCAE.FENode
label, which is generally used in solver input files and results files, in the node object itselfCAE.FENode
This is an abstract class
New in version NX6.0.2.
Methods¶
Method | Description |
---|---|
AskNextNodeLabel | Returns the next CAE.FENode label from the input put label. |
Dispose | Destroys the object |
GetNode | Returns CAE.FENode given a CAE.FENode label @return CAE.FENode |
Property Detail¶
Method Detail¶
AskNextNodeLabel¶
-
FENodeLabelMap.
AskNextNodeLabel
¶ Returns the next
CAE.FENode
label from the input put label.Signature
AskNextNodeLabel(nodelabel)
Parameters: nodelabel (int) – CAE.FENode
Label, for first node label input 0Returns: next CAE.FENode
LabelReturn type: int New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
Dispose¶
-
FENodeLabelMap.
Dispose
¶ Destroys the object
Signature
Dispose()
New in version NX6.0.2.
License requirements: None.
GetNode¶
-
FENodeLabelMap.
GetNode
¶ Returns
CAE.FENode
given aCAE.FENode
labelSignature
GetNode(nodelabel)
Parameters: nodelabel (int) – CAE.FENode
LabelReturns: CAE.FENode
Return type: NXOpen.CAE.FENode
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)