LaminateDynamicEventCollection Class¶
-
class
NXOpen.CAE.
LaminateDynamicEventCollection
¶ Bases:
object
Represents a collection of laminate dynamic events
To obtain an instance of this class, refer to
NXOpen.CAE.LaminateDynamicSim
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
CloneDynamicEvent | Clones the laminate dynamic event |
CreateRandomEventBuilder | Creates a builder for the laminate random event. |
CreateSineEventBuilder | Creates a builder for the laminate sine event. |
Delete | Deletes the laminate dynamic event |
FindObject | Finds a laminate dynamic event with the specified name @return Laminate Dynamic Event found |
Method Detail¶
CloneDynamicEvent¶
-
LaminateDynamicEventCollection.
CloneDynamicEvent
¶ Clones the laminate dynamic event
Signature
CloneDynamicEvent(dynamicEvent)
Parameters: dynamicEvent ( NXOpen.CAE.LaminateDynamicEvent
) – Laminate dynamic event to be clonedNew in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
CreateRandomEventBuilder¶
-
LaminateDynamicEventCollection.
CreateRandomEventBuilder
¶ Creates a builder for the laminate random event.
Signature
CreateRandomEventBuilder(laminateRandomEventTag)
Parameters: laminateRandomEventTag ( NXOpen.CAE.LaminateRandomEvent
) – The event.Returns: Return type: NXOpen.CAE.LaminateRandomEventBuilder
New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
CreateSineEventBuilder¶
-
LaminateDynamicEventCollection.
CreateSineEventBuilder
¶ Creates a builder for the laminate sine event.
Signature
CreateSineEventBuilder(laminateSineEventTag)
Parameters: laminateSineEventTag ( NXOpen.CAE.LaminateSineEvent
) – The event.Returns: Return type: NXOpen.CAE.LaminateSineEventBuilder
New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Delete¶
-
LaminateDynamicEventCollection.
Delete
¶ Deletes the laminate dynamic event
Signature
Delete(dynamicEvent)
Parameters: dynamicEvent ( NXOpen.CAE.LaminateDynamicEvent
) – Laminate dynamic event to be deletedNew in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
FindObject¶
-
LaminateDynamicEventCollection.
FindObject
¶ Finds a laminate dynamic event with the specified name
Signature
FindObject(name)
Parameters: name (str) – Laminate Dynamic Event name to be found Returns: Laminate Dynamic Event found Return type: NXOpen.CAE.LaminateDynamicEvent
New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)