LaminateRandomEventBuilder Class¶
-
class
NXOpen.CAE.
LaminateRandomEventBuilder
¶ Bases:
NXOpen.CAE.LaminateDynamicEventBuilder
Represents a
NXOpen.CAE.LaminateRandomEvent
builderTo create a new instance of this class, use
NXOpen.CAE.LaminateDynamicEventCollection.CreateRandomEventBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ConfidenceLevel | Returns or sets the confidence level (in %) |
ConfidenceLevelOption | Returns or sets the confidence level option |
DynamicEventName | Returns or sets the event name |
EventName | Returns or sets the event name |
ExcitationAxis | Returns or sets the excitation axis |
ExcitationCoordinateSystem | Returns or sets the excitation coordinate system |
ExcitationCsys | Returns or sets the excitation coordinate system |
ExcitationSelectedAxis | Returns or sets the excitation axis |
Function | Returns or sets the function. |
LowerBoundFreq | Returns or sets the lower bound freq |
LowerBoundFrequency | Returns or sets the lower bound freq |
NastranBasic | Returns or sets the nastran basic |
NastranBasicCsys | Returns or sets the nastran basic |
Reference | Returns or sets the reference |
ReferenceType | Returns or sets the reference type |
StandardDeviation | Returns or sets the number of standard deviations used to calculate the confidence level |
Tag | Returns the Tag for this object. |
UpperBoundFreq | Returns or sets the upper bound freq |
UpperBoundFrequency | Returns or sets the upper bound freq |
UserFunction | Returns or sets the function. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOutputRequest | Get the output request. |
GetOutputRequestObject | Get the output request. |
SetOutputRequest | Set the output request. |
SetOutputRequestObject | Set the output request. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LaminateRandomEventBuilderConfidenceLevelOptionEnum Enumeration | The confidence level option. |
LaminateRandomEventBuilderExcitationAxisEnum Enumeration | The excitation axis enum. |
LaminateRandomEventBuilderReferenceEnum Enumeration | The reference enum. |
Property Detail¶
ConfidenceLevel¶
-
LaminateRandomEventBuilder.
ConfidenceLevel
¶ Returns or sets the confidence level (in %)
-------------------------------------
Getter Method
Signature
ConfidenceLevel()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConfidenceLevel(confidenceLevel)
Parameters: confidenceLevel (float) – New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ConfidenceLevelOption¶
-
LaminateRandomEventBuilder.
ConfidenceLevelOption
¶ Returns or sets the confidence level option
-------------------------------------
Getter Method
Signature
ConfidenceLevelOption()
Returns: Return type: NXOpen.CAE.LaminateRandomEventBuilderConfidenceLevelOptionEnum
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConfidenceLevelOption(confidenceLevelOption)
Parameters: confidenceLevelOption ( NXOpen.CAE.LaminateRandomEventBuilderConfidenceLevelOptionEnum
) –New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
EventName¶
-
LaminateRandomEventBuilder.
EventName
¶ Returns or sets the event name
-------------------------------------
Getter Method
Signature
EventName()
Returns: Return type: str New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.DynamicEventName
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
EventName(eventName)
Parameters: eventName (str) – New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetDynamicEventName
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ExcitationAxis¶
-
LaminateRandomEventBuilder.
ExcitationAxis
¶ Returns or sets the excitation axis
-------------------------------------
Getter Method
Signature
ExcitationAxis()
Returns: Return type: NXOpen.CAE.LaminateRandomEventBuilderExcitationAxisEnum
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.ExcitationSelectedAxis
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ExcitationAxis(excitationAxis)
Parameters: excitationAxis ( NXOpen.CAE.LaminateRandomEventBuilderExcitationAxisEnum
) –New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetExcitationSelectedAxis
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ExcitationCoordinateSystem¶
-
LaminateRandomEventBuilder.
ExcitationCoordinateSystem
¶ Returns or sets the excitation coordinate system
-------------------------------------
Getter Method
Signature
ExcitationCoordinateSystem()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.ExcitationCsys
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ExcitationCoordinateSystem(excitationCoordinateSystem)
Parameters: excitationCoordinateSystem ( NXOpen.CoordinateSystem
) –New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetExcitationCsys
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Function¶
-
LaminateRandomEventBuilder.
Function
¶ Returns or sets the function.
-------------------------------------
Getter Method
Signature
Function()
Returns: Return type: NXOpen.TaggedObject
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.UserFunction
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Function(functionTag)
Parameters: functionTag ( NXOpen.TaggedObject
) –New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetUserFunction
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
LowerBoundFreq¶
-
LaminateRandomEventBuilder.
LowerBoundFreq
¶ Returns or sets the lower bound freq
-------------------------------------
Getter Method
Signature
LowerBoundFreq()
Returns: Return type: float New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.LowerBoundFrequency
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
LowerBoundFreq(lowerBoundFreq)
Parameters: lowerBoundFreq (float) – New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetLowerBoundFrequency
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
NastranBasic¶
-
LaminateRandomEventBuilder.
NastranBasic
¶ Returns or sets the nastran basic
-------------------------------------
Getter Method
Signature
NastranBasic()
Returns: Return type: bool New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.NastranBasicCsys
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
NastranBasic(nastranBasic)
Parameters: nastranBasic (bool) – New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetNastranBasicCsys
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Reference¶
-
LaminateRandomEventBuilder.
Reference
¶ Returns or sets the reference
-------------------------------------
Getter Method
Signature
Reference()
Returns: Return type: NXOpen.CAE.LaminateRandomEventBuilderReferenceEnum
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.ReferenceType
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Reference(reference)
Parameters: reference ( NXOpen.CAE.LaminateRandomEventBuilderReferenceEnum
) –New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetReferenceType
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
StandardDeviation¶
-
LaminateRandomEventBuilder.
StandardDeviation
¶ Returns or sets the number of standard deviations used to calculate the confidence level
-------------------------------------
Getter Method
Signature
StandardDeviation()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StandardDeviation(standardDeviation)
Parameters: standardDeviation (float) – New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
UpperBoundFreq¶
-
LaminateRandomEventBuilder.
UpperBoundFreq
¶ Returns or sets the upper bound freq
-------------------------------------
Getter Method
Signature
UpperBoundFreq()
Returns: Return type: float New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.UpperBoundFrequency
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
UpperBoundFreq(upperBoundFreq)
Parameters: upperBoundFreq (float) – New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetUpperBoundFrequency
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Method Detail¶
GetOutputRequest¶
-
LaminateRandomEventBuilder.
GetOutputRequest
¶ Get the output request.
Signature
GetOutputRequest()
Returns: Return type: NXOpen.CAE.ModelingObjectPropertyTable
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.GetOutputRequestObject
instead.License requirements: None.
SetOutputRequest¶
-
LaminateRandomEventBuilder.
SetOutputRequest
¶ Set the output request.
Signature
SetOutputRequest(ssmo)
Parameters: ssmo ( NXOpen.CAE.ModelingObjectPropertyTable
) –New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetOutputRequestObject
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Validate¶
-
LaminateRandomEventBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.