LaminateRandomEventBuilderReferenceEnum Enumeration¶
NXOpen.CAE.LaminateRandomEventBuilder.ReferenceEnum is an alias for NXOpen.CAE.LaminateRandomEventBuilderReferenceEnum
-
class
NXOpen.CAE.
LaminateRandomEventBuilderReferenceEnum
¶ Bases:
object
The reference enum.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilderReferenceTypeEnum
instead.Enum Members
Enum Member Enum Member Description Relative Absolute -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-