PreTestExportUnvBuilderFileUnitsOption Enumeration¶
NXOpen.CAE.PreTestExportUnvBuilder.FileUnitsOption is an alias for NXOpen.CAE.PreTestExportUnvBuilderFileUnitsOption
-
class
NXOpen.CAE.
PreTestExportUnvBuilderFileUnitsOption
¶ Bases:
object
The unit type enum
Enum Members
Enum Member Enum Member Description Si SI: Meter (newton)Bg BG: Foot (pound f)Mg MG: Meter (kilogram f)Ba BA: Foot (poundal)Mm MM: mm (milli newton)Cm CM: cm (centi newton)In IN: Inch (pound f)Gm GM: mm (kilogram f)Mn MN: mm (newton)-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-