ElementSplitBuilderTypes Enumeration¶
NXOpen.CAE.ElementSplitBuilder.Types is an alias for NXOpen.CAE.ElementSplitBuilderTypes
-
class
NXOpen.CAE.
ElementSplitBuilderTypes
¶ Bases:
object
the element split types
Enum Members
Enum Member Enum Member Description QuadTo2Tria Quad to 2 Tria QuadTo2Quad Quad to 2 Quad QuadTo4Quad Quad to 4 Quad QuadTo3Quad Quad to 3 Quad QuadTo3Tria Quad to 3 Tria TriaTo4Tria Tria to 4 Tria SplitByLine Split by line TriaTo2Tria Tria to 2 Tria -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-