DurabilityStrengthCollection Class¶
-
class
NXOpen.CAE.
DurabilityStrengthCollection
¶ Bases:
object
Represents a collection of event strength settings.
To obtain an instance of this class, refer to
NXOpen.CAE.DurabilityManager
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
CloneStrength | Clones a durability event strength settings. |
CreateEventstrengthsettingsBuilder | Creates the builder object of durability event strength settings. |
DeleteStrength | Delete a durability event strength settings. |
FindObject | Finds an event strength settings with a specified name. |
Method Detail¶
CloneStrength¶
-
DurabilityStrengthCollection.
CloneStrength
¶ Clones a durability event strength settings.
Signature
CloneStrength(source)
Parameters: source ( NXOpen.CAE.DurabilityStrength
) – Source event strength settingssReturns: Cloned event strength settingss Return type: NXOpen.CAE.DurabilityStrength
New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
CreateEventstrengthsettingsBuilder¶
-
DurabilityStrengthCollection.
CreateEventstrengthsettingsBuilder
¶ Creates the builder object of durability event strength settings.
Signature
CreateEventstrengthsettingsBuilder(eventstrengthsettings)
Parameters: eventstrengthsettings ( NXOpen.CAE.DurabilityStrength
) –Returns: Return type: NXOpen.CAE.DurabilityEventStrengthSettingsBuilder
New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
DeleteStrength¶
-
DurabilityStrengthCollection.
DeleteStrength
¶ Delete a durability event strength settings.
Signature
DeleteStrength(eventstrengthsettings)
Parameters: eventstrengthsettings ( NXOpen.CAE.DurabilityStrength
) – The durability event strength settings to be deletedNew in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
FindObject¶
-
DurabilityStrengthCollection.
FindObject
¶ Finds an event strength settings with a specified name.
Signature
FindObject(name)
Parameters: name (str) – name of the durability event strength settings Returns: The durability event strength settings Return type: NXOpen.CAE.DurabilityStrength
New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)