UserDefinedSolidBeamSectionBuilder Class¶
-
class
NXOpen.CAE.
UserDefinedSolidBeamSectionBuilder
¶ Bases:
NXOpen.CAE.IBeamSectionBuilder
Represents a
NXOpen.CAE.UserDefinedSolidBeamSectionBuilder
To create a new instance of this class, use
NXOpen.CAE.BeamSectionCollection.CreateUserDefinedSolidBeamSectionBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
DescriptorName | Returns or sets the section descriptor name |
DirectionType | Returns or sets the option to define reference vector |
PropertyTable | Returns the section builder’s NXOpen.CAE.PropertyTable |
ReferenceVector | Returns or sets the reference vector |
SectionName | Returns or sets the section name |
SolidFace | Returns the solid face |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetUserDefinedStressRecoveryPoints | Gets the user-defined stress recovery points. |
SetUserDefinedStressRecoveryPoints | Sets the user-defined stress recovery points. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DescriptorName¶
-
UserDefinedSolidBeamSectionBuilder.
DescriptorName
¶ Returns or sets the section descriptor name
-------------------------------------
Getter Method
Signature
DescriptorName()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DescriptorName(descriptorName)
Parameters: descriptorName (str) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DirectionType¶
-
UserDefinedSolidBeamSectionBuilder.
DirectionType
¶ Returns or sets the option to define reference vector
-------------------------------------
Getter Method
Signature
DirectionType()
Returns: Return type: NXOpen.CAE.BeamSectionDirectionOption
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DirectionType(directionType)
Parameters: directionType ( NXOpen.CAE.BeamSectionDirectionOption
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ReferenceVector¶
-
UserDefinedSolidBeamSectionBuilder.
ReferenceVector
¶ Returns or sets the reference vector
-------------------------------------
Getter Method
Signature
ReferenceVector()
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceVector(referenceVector)
Parameters: referenceVector ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SolidFace¶
-
UserDefinedSolidBeamSectionBuilder.
SolidFace
¶ Returns the solid face
-------------------------------------
Getter Method
Signature
SolidFace()
Returns: Return type: NXOpen.CAE.SelectCAEFace
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
UserDefinedSolidBeamSectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.