IBeamSectionBuilder Class¶
-
class
NXOpen.CAE.
IBeamSectionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.IBeamSectionBuilder
This is an abstract class
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
PropertyTable | Returns the section builder’s NXOpen.CAE.PropertyTable |
SectionName | Returns or sets the section name |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetUserDefinedStressRecoveryPoints | Gets the user-defined stress recovery points. |
SetUserDefinedStressRecoveryPoints | Sets the user-defined stress recovery points. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
PropertyTable¶
-
IBeamSectionBuilder.
PropertyTable
¶ Returns the section builder’s
NXOpen.CAE.PropertyTable
-------------------------------------
Getter Method
Signature
PropertyTable()
Returns: Return type: NXOpen.CAE.PropertyTable
New in version NX7.5.0.
License requirements: None.
SectionName¶
-
IBeamSectionBuilder.
SectionName
¶ Returns or sets the section name
-------------------------------------
Getter Method
Signature
SectionName()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionName(sectionName)
Parameters: sectionName (str) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
GetUserDefinedStressRecoveryPoints¶
-
IBeamSectionBuilder.
GetUserDefinedStressRecoveryPoints
¶ Gets the user-defined stress recovery points.
Signature
GetUserDefinedStressRecoveryPoints()
Returns: Return type: list of NXOpen.Point2d
New in version NX7.5.0.
License requirements: None.
SetUserDefinedStressRecoveryPoints¶
-
IBeamSectionBuilder.
SetUserDefinedStressRecoveryPoints
¶ Sets the user-defined stress recovery points.
Signature
SetUserDefinedStressRecoveryPoints(points)
Parameters: points (list of NXOpen.Point2d
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Validate¶
-
IBeamSectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.