SuppressHoleBuilder Class¶
-
class
NXOpen.CAE.
SuppressHoleBuilder
¶ Bases:
NXOpen.Builder
Builder for creating Hole Suppression Hole
To create a new instance of this class, use
NXOpen.CAE.AbstractionManager.CreateSuppressHoleBuilder
Default values.
Property Value Choice Automatic HoleDiameter.Value 0 (millimeters part), 0 (inches part) PointCreate None New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
BodySelect | Returns the bodyselect |
Choice | Returns or sets the type Automatic or Manual |
EdgeSelect | Returns the edgeselect |
HoleDiameter | Returns the holedia |
PointCreate | Returns or sets the pointcreate |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SuppressHoleBuilderOptionChoice Enumeration | the enum for method |
SuppressHoleBuilderOptionPointCreate Enumeration | the enum for point creation |
Property Detail¶
BodySelect¶
-
SuppressHoleBuilder.
BodySelect
¶ Returns the bodyselect
-------------------------------------
Getter Method
Signature
BodySelect()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Choice¶
-
SuppressHoleBuilder.
Choice
¶ Returns or sets the type Automatic or Manual
-------------------------------------
Getter Method
Signature
Choice()
Returns: Return type: NXOpen.CAE.SuppressHoleBuilderOptionChoice
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Choice(type)
Parameters: type ( NXOpen.CAE.SuppressHoleBuilderOptionChoice
) –New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EdgeSelect¶
-
SuppressHoleBuilder.
EdgeSelect
¶ Returns the edgeselect
-------------------------------------
Getter Method
Signature
EdgeSelect()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
HoleDiameter¶
-
SuppressHoleBuilder.
HoleDiameter
¶ Returns the holedia
-------------------------------------
Getter Method
Signature
HoleDiameter()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
PointCreate¶
-
SuppressHoleBuilder.
PointCreate
¶ Returns or sets the pointcreate
-------------------------------------
Getter Method
Signature
PointCreate()
Returns: Return type: NXOpen.CAE.SuppressHoleBuilderOptionPointCreate
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointCreate(pointCreate)
Parameters: pointCreate ( NXOpen.CAE.SuppressHoleBuilderOptionPointCreate
) –New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SuppressHoleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.