LaminatePly Class¶
-
class
NXOpen.CAE.
LaminatePly
¶ Bases:
NXOpen.NXObject
Represents one ply in a laminate layup
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AngleExpression | Returns the ply angle expression, relative to local material orientation |
Color | Returns or sets the ply color |
Description | Returns or sets the ply description |
DrapingExtension | Returns or sets the draping extension selection |
DrapingInput | Returns or sets the draping data (draping settings) |
GlobalId | Returns or sets the ply global id |
InterLaminarFailureTheory | Returns or sets the inter laminar failure theory used in a solid laminate nastran analysis (PCOMPS) |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
Orientation | Returns or sets the ply orientation angle in degrees, relative to local material orientation |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PlyFailureTheory | Returns or sets the ply failure theory used in a solid laminate nastran analysis (PCOMPS) |
Prototype | Returns the prototype of this object if it is an occurrence. |
SolidProperty | Returns or sets the ply solid property |
Tag | Returns the Tag for this object. |
Thickness | Returns or sets the ply thickness, in part units (inches or millimeters) |
ThicknessExpression | Returns the ply thickness expression |
UserDefinedInterLaminarFailureTheory | Returns or sets the user defined interlaminar failure theory name used in a solid laminate nastran analysis (PCOMPS) |
UserDefinedPlyFailureTheory | Returns or sets the user defined ply failure theory name used in a solid laminate nastran analysis (PCOMPS) |
Methods¶
Method | Description |
---|---|
AssignAngleExpression | Assigns a value to the ply angle expression |
AssignThicknessExpression | Assigns a value to the ply thickness expression |
ComputeDraping | Launch the draping algorithm, overriding previous results |
CopyDrapingResults | Copy draping results. |
CreateDrapingDataBuilder | Creates a NXOpen.CAE.LaminateDrapingDataBuilder @return |
CreateDrapingExtensionBuilder | Creates a NXOpen.CAE.LaminateDrapingExtensionBuilder @return |
CreateLaminatePlyMaxThicknessVarBuilder | Creates a NXOpen.CAE.LaminatePlyMaxThicknessVarBuilder @return |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
ExportDrapingDomainAsGroup | Exports draping domain to a group |
ExportDrapingResults | Exports draping results to a csv file. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetMaterialName | Gets the material name @return |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Information | Display global ply information |
Prints a representation of this object to the system log file. | |
ResetExtensionTarget | For global link ply subtype, resets the ply link target |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetMaterialByName | Sets the material by name. |
SetName | Sets the custom name of the object. |
SetPlyMaterialByName | Sets the ply material by name. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
LaminatePlyInterLaminarFailureTheoryType Enumeration | Inter-Laminar failure theory types |
LaminatePlyPlyFailureTheoryType Enumeration | Ply failure theory types |
LaminatePlySolidPropertyType Enumeration | Solid property type for laminate extrusion |
Property Detail¶
AngleExpression¶
-
LaminatePly.
AngleExpression
¶ Returns the ply angle expression, relative to local material orientation
-------------------------------------
Getter Method
Signature
AngleExpression()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Color¶
-
LaminatePly.
Color
¶ Returns or sets the ply color
-------------------------------------
Getter Method
Signature
Color()
Returns: ply color Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Color(orientation)
Parameters: orientation (int) – ply color New in version NX5.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
Description¶
-
LaminatePly.
Description
¶ Returns or sets the ply description
-------------------------------------
Getter Method
Signature
Description()
Returns: ply description Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Description(description)
Parameters: description (str) – ply description New in version NX7.5.0.
License requirements: nx_lam_composites (“Laminate Composites”)
DrapingExtension¶
-
LaminatePly.
DrapingExtension
¶ Returns or sets the draping extension selection
-------------------------------------
Getter Method
Signature
DrapingExtension()
Returns: draping extension Return type: NXOpen.CAE.LaminateDrapingExtension
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DrapingExtension(drapingExtension)
Parameters: drapingExtension ( NXOpen.CAE.LaminateDrapingExtension
) – draping extensionNew in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
DrapingInput¶
-
LaminatePly.
DrapingInput
¶ Returns or sets the draping data (draping settings)
-------------------------------------
Getter Method
Signature
DrapingInput()
Returns: draping algorithm input Return type: NXOpen.CAE.LaminateDrapingData
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DrapingInput(drapingInput)
Parameters: drapingInput ( NXOpen.CAE.LaminateDrapingData
) – draping algorithm inputNew in version NX7.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
GlobalId¶
-
LaminatePly.
GlobalId
¶ Returns or sets the ply global id
-------------------------------------
Getter Method
Signature
GlobalId()
Returns: ply color Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GlobalId(globalId)
Parameters: globalId (int) – ply color New in version NX6.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
InterLaminarFailureTheory¶
-
LaminatePly.
InterLaminarFailureTheory
¶ Returns or sets the inter laminar failure theory used in a solid laminate nastran analysis (PCOMPS)
-------------------------------------
Getter Method
Signature
InterLaminarFailureTheory()
Returns: Return type: NXOpen.CAE.LaminatePlyInterLaminarFailureTheoryType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InterLaminarFailureTheory(interLaminarFailureTheory)
Parameters: interLaminarFailureTheory ( NXOpen.CAE.LaminatePlyInterLaminarFailureTheoryType
) –New in version NX8.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
IsOccurrence¶
-
LaminatePly.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
LaminatePly.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
LaminatePly.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Orientation¶
-
LaminatePly.
Orientation
¶ Returns or sets the ply orientation angle in degrees, relative to local material orientation
-------------------------------------
Getter Method
Signature
Orientation()
Returns: ply orientation Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Orientation(orientation)
Parameters: orientation (float) – ply orientation New in version NX5.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
OwningComponent¶
-
LaminatePly.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
LaminatePly.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
PlyFailureTheory¶
-
LaminatePly.
PlyFailureTheory
¶ Returns or sets the ply failure theory used in a solid laminate nastran analysis (PCOMPS)
-------------------------------------
Getter Method
Signature
PlyFailureTheory()
Returns: Return type: NXOpen.CAE.LaminatePlyPlyFailureTheoryType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlyFailureTheory(plyFailureTheory)
Parameters: plyFailureTheory ( NXOpen.CAE.LaminatePlyPlyFailureTheoryType
) –New in version NX8.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Prototype¶
-
LaminatePly.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
SolidProperty¶
-
LaminatePly.
SolidProperty
¶ Returns or sets the ply solid property
-------------------------------------
Getter Method
Signature
SolidProperty()
Returns: ply solid property Return type: NXOpen.CAE.LaminatePlySolidPropertyType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SolidProperty(solidProp)
Parameters: solidProp ( NXOpen.CAE.LaminatePlySolidPropertyType
) – ply solid propertyNew in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Thickness¶
-
LaminatePly.
Thickness
¶ Returns or sets the ply thickness, in part units (inches or millimeters)
-------------------------------------
Getter Method
Signature
Thickness()
Returns: ply thickness Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Thickness(thickness)
Parameters: thickness (float) – ply thickness New in version NX5.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
ThicknessExpression¶
-
LaminatePly.
ThicknessExpression
¶ Returns the ply thickness expression
-------------------------------------
Getter Method
Signature
ThicknessExpression()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
UserDefinedInterLaminarFailureTheory¶
-
LaminatePly.
UserDefinedInterLaminarFailureTheory
¶ Returns or sets the user defined interlaminar failure theory name used in a solid laminate nastran analysis (PCOMPS)
-------------------------------------
Getter Method
Signature
UserDefinedInterLaminarFailureTheory()
Returns: the user defined interlaminar failure theory name Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserDefinedInterLaminarFailureTheory(name)
Parameters: name (str) – the user defined interlaminar failure theory name New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
UserDefinedPlyFailureTheory¶
-
LaminatePly.
UserDefinedPlyFailureTheory
¶ Returns or sets the user defined ply failure theory name used in a solid laminate nastran analysis (PCOMPS)
-------------------------------------
Getter Method
Signature
UserDefinedPlyFailureTheory()
Returns: the user defined ply failure theory name Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserDefinedPlyFailureTheory(name)
Parameters: name (str) – the user defined ply failure theory name New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Method Detail¶
AssignAngleExpression¶
-
LaminatePly.
AssignAngleExpression
¶ Assigns a value to the ply angle expression
Signature
AssignAngleExpression(angleExp)
Parameters: angleExp (str) – The angle expression string New in version NX10.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
AssignThicknessExpression¶
-
LaminatePly.
AssignThicknessExpression
¶ Assigns a value to the ply thickness expression
Signature
AssignThicknessExpression(thickExp)
Parameters: thickExp (str) – The thickness expression string New in version NX10.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
ComputeDraping¶
-
LaminatePly.
ComputeDraping
¶ Launch the draping algorithm, overriding previous results
Signature
ComputeDraping()
New in version NX7.5.1.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
CopyDrapingResults¶
-
LaminatePly.
CopyDrapingResults
¶ Copy draping results.
Signature
CopyDrapingResults(drapingResults)
Parameters: drapingResults ( NXOpen.CAE.LaminateDrapingOrientation
) – draping resultsNew in version NX7.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
CreateDrapingDataBuilder¶
-
LaminatePly.
CreateDrapingDataBuilder
¶ Creates a
NXOpen.CAE.LaminateDrapingDataBuilder
Signature
CreateDrapingDataBuilder()
Returns: Return type: NXOpen.CAE.LaminateDrapingDataBuilder
New in version NX7.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
CreateDrapingExtensionBuilder¶
-
LaminatePly.
CreateDrapingExtensionBuilder
¶ Creates a
NXOpen.CAE.LaminateDrapingExtensionBuilder
Signature
CreateDrapingExtensionBuilder()
Returns: Return type: NXOpen.CAE.LaminateDrapingExtensionBuilder
New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
CreateLaminatePlyMaxThicknessVarBuilder¶
-
LaminatePly.
CreateLaminatePlyMaxThicknessVarBuilder
¶ Creates a
NXOpen.CAE.LaminatePlyMaxThicknessVarBuilder
Signature
CreateLaminatePlyMaxThicknessVarBuilder()
Returns: Return type: NXOpen.CAE.LaminatePlyMaxThicknessVarBuilder
New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ExportDrapingDomainAsGroup¶
-
LaminatePly.
ExportDrapingDomainAsGroup
¶ Exports draping domain to a group
Signature
ExportDrapingDomainAsGroup()
New in version NX7.5.2.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ExportDrapingResults¶
-
LaminatePly.
ExportDrapingResults
¶ Exports draping results to a csv file.
Signature
ExportDrapingResults(csvFilename, showShearAngle, showYarnAngle, showPrimaryDirection, showSecondaryDirection, showNormalDirection)
Parameters: - csvFilename (str) – NOTE: The full Unicode character set is not supported for this parameter.
- showShearAngle (bool) –
- showYarnAngle (bool) –
- showPrimaryDirection (bool) –
- showSecondaryDirection (bool) –
- showNormalDirection (bool) –
New in version NX7.5.1.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
FindObject¶
-
LaminatePly.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetMaterialName¶
-
LaminatePly.
GetMaterialName
¶ Gets the material name
Signature
GetMaterialName()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
Information¶
-
LaminatePly.
Information
¶ Display global ply information
Signature
Information(detailed)
Parameters: detailed (bool) – New in version NX7.5.1.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Print¶
-
LaminatePly.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
ResetExtensionTarget¶
-
LaminatePly.
ResetExtensionTarget
¶ For global link ply subtype, resets the ply link target
Signature
ResetExtensionTarget(targetPly)
Parameters: targetPly ( NXOpen.CAE.LaminatePly
) – The new extension targetNew in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SetMaterialByName¶
-
LaminatePly.
SetMaterialByName
¶ Sets the material by name.
Signature
SetMaterialByName(name)
Parameters: name (str) – material name NOTE: The full Unicode character set is not supported for this parameter. New in version NX7.5.0.
License requirements: nx_lam_composites (“Laminate Composites”)
SetName¶
-
LaminatePly.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetPlyMaterialByName¶
-
LaminatePly.
SetPlyMaterialByName
¶ Sets the ply material by name.
Signature
SetPlyMaterialByName(name)
Parameters: name (str) – ply material name NOTE: The full Unicode character set is not supported for this parameter. New in version NX7.5.0.
License requirements: nx_lam_composites (“Laminate Composites”)