LaminatePlyMaxThicknessVarBuilder Class¶
-
class
NXOpen.CAE.
LaminatePlyMaxThicknessVarBuilder
¶ Bases:
NXOpen.Builder
Builder used to modify the ply maximum accepted thickness variation for laminate fill
To create a new instance of this class, use
NXOpen.CAE.LaminatePly.CreateLaminatePlyMaxThicknessVarBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
ThicknessOverride | Returns or sets the layup thickness variation limit override option |
ThicknessVariationDownLimit | Returns or sets the maximum allowed relative thickness reduction variation, in percentage, for the ply |
ThicknessVariationUpLimit | Returns or sets the maximum allowed relative thickness increase variation, in percentage, for the ply |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ThicknessOverride¶
-
LaminatePlyMaxThicknessVarBuilder.
ThicknessOverride
¶ Returns or sets the layup thickness variation limit override option
-------------------------------------
Getter Method
Signature
ThicknessOverride()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThicknessOverride(thicknessOverride)
Parameters: thicknessOverride (bool) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ThicknessVariationDownLimit¶
-
LaminatePlyMaxThicknessVarBuilder.
ThicknessVariationDownLimit
¶ Returns or sets the maximum allowed relative thickness reduction variation, in percentage, for the ply
-------------------------------------
Getter Method
Signature
ThicknessVariationDownLimit()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThicknessVariationDownLimit(thicknessVariationDownLimit)
Parameters: thicknessVariationDownLimit (float) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ThicknessVariationUpLimit¶
-
LaminatePlyMaxThicknessVarBuilder.
ThicknessVariationUpLimit
¶ Returns or sets the maximum allowed relative thickness increase variation, in percentage, for the ply
-------------------------------------
Getter Method
Signature
ThicknessVariationUpLimit()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThicknessVariationUpLimit(thicknessVariationUpLimit)
Parameters: thicknessVariationUpLimit (float) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Method Detail¶
Validate¶
-
LaminatePlyMaxThicknessVarBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.